<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Seriesのトピック[T1042 Ramdisk] Kernel panic - not syncing: No working init found.  Try passing init= option to kernel.</title>
    <link>https://community.nxp.com/t5/T-Series/T1042-Ramdisk-Kernel-panic-not-syncing-No-working-init-found-Try/m-p/1036542#M3543</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;I want to boot with ramdisk using commands below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;tftp 1000000 uImage--4.19-r0-t1042d4rdb-64b-20200217054545.bin&lt;BR /&gt;tftp 2000000 t1042d4rdb--4.19-r0-t1042d4rdb-64b-20200217054545.dtb&lt;BR /&gt;tftp 3000000 asd2.rootfs.ext2.gz.u-boot&lt;BR /&gt;bootm 1000000 3000000 2000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can successfully boot on bank0 with these commands. But when I switch to BANK 4 ( alternate bank ), It gives me error. Error logs are here;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Freeing unused kernel memory: 524K&lt;BR /&gt;This architecture does not have kernel memory protection.&lt;BR /&gt;Run /sbin/init as init process&lt;BR /&gt;EXT4-fs warning (device ram0): dx_probe:794: inode #3225: comm swapper/0: dx entry: limit 0 != root limit 125&lt;BR /&gt;EXT4-fs warning (device ram0): dx_probe:866: inode #3225: comm swapper/0: Corrupt directory, running e2fsck is recommended&lt;BR /&gt;Run /etc/init as init process&lt;BR /&gt;EXT4-fs warning (device ram0): dx_probe:794: inode #3361: comm swapper/0: dx entry: limit 0 != root limit 125&lt;BR /&gt;EXT4-fs warning (device ram0): dx_probe:866: inode #3361: comm swapper/0: Corrupt directory, running e2fsck is recommended&lt;BR /&gt;Run /bin/init as init process&lt;BR /&gt;Run /bin/sh as init process&lt;BR /&gt;Kernel panic - not syncing: No working init found.&amp;nbsp; Try passing init= option to kernel. See Linux Documentation/admin-guide/init.rst for guidance.&lt;BR /&gt;CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.19.26+gc0c2141 #1&lt;BR /&gt;Call Trace:&lt;BR /&gt;[c0000001f3107c70] [c000000000a810e4] .dump_stack+0xa8/0xec (unreliable)&lt;BR /&gt;[c0000001f3107d00] [c00000000004b580] .panic+0x12c/0x2e8&lt;BR /&gt;[c0000001f3107db0] [c000000000002464] .kernel_init+0x10c/0x128&lt;BR /&gt;[c0000001f3107e30] [c0000000000009f4] .ret_from_kernel_thread+0x58/0x64&lt;BR /&gt;Rebooting in 180 seconds..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attached full logs from BANK0 booting and BANK4 booting. They both have same U-boot environment variables. I am suspecting that this is a QMan problem but I am unable to reach QMAN memory from U-boot console.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I try to protect off QMan memory on flash&lt;/P&gt;&lt;P&gt;=&amp;gt; protect off 0xEFF10000 +$filesize &amp;nbsp;&lt;BR /&gt;Error: start address not on sector boundary&lt;/P&gt;&lt;P&gt;I had this error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help ? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Feb 2020 14:17:13 GMT</pubDate>
    <dc:creator>yusufalti333</dc:creator>
    <dc:date>2020-02-17T14:17:13Z</dc:date>
    <item>
      <title>[T1042 Ramdisk] Kernel panic - not syncing: No working init found.  Try passing init= option to kernel.</title>
      <link>https://community.nxp.com/t5/T-Series/T1042-Ramdisk-Kernel-panic-not-syncing-No-working-init-found-Try/m-p/1036542#M3543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;I want to boot with ramdisk using commands below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;tftp 1000000 uImage--4.19-r0-t1042d4rdb-64b-20200217054545.bin&lt;BR /&gt;tftp 2000000 t1042d4rdb--4.19-r0-t1042d4rdb-64b-20200217054545.dtb&lt;BR /&gt;tftp 3000000 asd2.rootfs.ext2.gz.u-boot&lt;BR /&gt;bootm 1000000 3000000 2000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can successfully boot on bank0 with these commands. But when I switch to BANK 4 ( alternate bank ), It gives me error. Error logs are here;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Freeing unused kernel memory: 524K&lt;BR /&gt;This architecture does not have kernel memory protection.&lt;BR /&gt;Run /sbin/init as init process&lt;BR /&gt;EXT4-fs warning (device ram0): dx_probe:794: inode #3225: comm swapper/0: dx entry: limit 0 != root limit 125&lt;BR /&gt;EXT4-fs warning (device ram0): dx_probe:866: inode #3225: comm swapper/0: Corrupt directory, running e2fsck is recommended&lt;BR /&gt;Run /etc/init as init process&lt;BR /&gt;EXT4-fs warning (device ram0): dx_probe:794: inode #3361: comm swapper/0: dx entry: limit 0 != root limit 125&lt;BR /&gt;EXT4-fs warning (device ram0): dx_probe:866: inode #3361: comm swapper/0: Corrupt directory, running e2fsck is recommended&lt;BR /&gt;Run /bin/init as init process&lt;BR /&gt;Run /bin/sh as init process&lt;BR /&gt;Kernel panic - not syncing: No working init found.&amp;nbsp; Try passing init= option to kernel. See Linux Documentation/admin-guide/init.rst for guidance.&lt;BR /&gt;CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.19.26+gc0c2141 #1&lt;BR /&gt;Call Trace:&lt;BR /&gt;[c0000001f3107c70] [c000000000a810e4] .dump_stack+0xa8/0xec (unreliable)&lt;BR /&gt;[c0000001f3107d00] [c00000000004b580] .panic+0x12c/0x2e8&lt;BR /&gt;[c0000001f3107db0] [c000000000002464] .kernel_init+0x10c/0x128&lt;BR /&gt;[c0000001f3107e30] [c0000000000009f4] .ret_from_kernel_thread+0x58/0x64&lt;BR /&gt;Rebooting in 180 seconds..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attached full logs from BANK0 booting and BANK4 booting. They both have same U-boot environment variables. I am suspecting that this is a QMan problem but I am unable to reach QMAN memory from U-boot console.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I try to protect off QMan memory on flash&lt;/P&gt;&lt;P&gt;=&amp;gt; protect off 0xEFF10000 +$filesize &amp;nbsp;&lt;BR /&gt;Error: start address not on sector boundary&lt;/P&gt;&lt;P&gt;I had this error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help ? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2020 14:17:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1042-Ramdisk-Kernel-panic-not-syncing-No-working-init-found-Try/m-p/1036542#M3543</guid>
      <dc:creator>yusufalti333</dc:creator>
      <dc:date>2020-02-17T14:17:13Z</dc:date>
    </item>
    <item>
      <title>Re: [T1042 Ramdisk] Kernel panic - not syncing: No working init found.  Try passing init= option to kernel.</title>
      <link>https://community.nxp.com/t5/T-Series/T1042-Ramdisk-Kernel-panic-not-syncing-No-working-init-found-Try/m-p/1036543#M3544</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="345379" data-username="yusufalti333@gmail.com" href="https://community.nxp.com/people/yusufalti333@gmail.com" style="color: #3d9ce7; background-color: #ffffff; border: 0px; font-weight: 600; text-decoration: none; font-size: 11.9994px;"&gt;Yusuf Altıparmak&lt;/A&gt;&lt;SPAN style="background-color: #ffffff; color: #646464; "&gt;,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please add "ramdisk_size=10000000" in bootargs.&lt;/P&gt;&lt;P&gt;In u-boot:&lt;/P&gt;&lt;P&gt;=&amp;gt;setenv bootargs "root=/dev/ram rw console=ttyS0,115200&amp;nbsp;&lt;SPAN&gt;r&lt;/SPAN&gt;&lt;SPAN&gt;amdisk_size=10000000"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;=&amp;gt;saveenv&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Yiping&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2020 06:19:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1042-Ramdisk-Kernel-panic-not-syncing-No-working-init-found-Try/m-p/1036543#M3544</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-02-18T06:19:27Z</dc:date>
    </item>
  </channel>
</rss>