<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic T4160 SD card interface in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T4160-SD-card-interface/m-p/955886#M3262</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a T4160 based board, in which i am testing the SD card interface. In the uboot shell, when i type mmc info command it is giving the response as "Card did not respond to voltage select!" . SD card I am using is Sandisk micro SD HC class1 16GB card. In my board i have used a voltage translator to convert 1.8V to 3.3V (card side) . When I probed the SD clock, it is at 400Khz.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What could be the issue? Is there a provision at uboot to disable voltage selection?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Jun 2019 13:10:39 GMT</pubDate>
    <dc:creator>logifrancis</dc:creator>
    <dc:date>2019-06-21T13:10:39Z</dc:date>
    <item>
      <title>T4160 SD card interface</title>
      <link>https://community.nxp.com/t5/T-Series/T4160-SD-card-interface/m-p/955886#M3262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a T4160 based board, in which i am testing the SD card interface. In the uboot shell, when i type mmc info command it is giving the response as "Card did not respond to voltage select!" . SD card I am using is Sandisk micro SD HC class1 16GB card. In my board i have used a voltage translator to convert 1.8V to 3.3V (card side) . When I probed the SD clock, it is at 400Khz.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What could be the issue? Is there a provision at uboot to disable voltage selection?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2019 13:10:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4160-SD-card-interface/m-p/955886#M3262</guid>
      <dc:creator>logifrancis</dc:creator>
      <dc:date>2019-06-21T13:10:39Z</dc:date>
    </item>
    <item>
      <title>Re: T4160 SD card interface</title>
      <link>https://community.nxp.com/t5/T-Series/T4160-SD-card-interface/m-p/955887#M3263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Hello &lt;STRONG&gt;&lt;A _jive_internal="true" data-avatarid="-1" data-content-finding="Community" data-userid="305827" data-username="logifrancis" href="https://community.nxp.com/people/logifrancis"&gt;Logi Francis&lt;/A&gt;&lt;/STRONG&gt;,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-size: 10.0pt; "&gt;"Card did not respond to voltage select" is caused by failure of the ACMD41, which means that the voltage selection settings by the host does not match with eMMC device.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-size: 10.0pt; "&gt;Please check RCW configuration. &lt;BR /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-size: 10.0pt; "&gt;SDHC_BASE (371): 0; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-size: 10.0pt; "&gt;SPI_BASE (382-383): 01 to use 8-bit eMMC support;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-size: 10.0pt; "&gt; &lt;BR /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-size: 10.0pt; "&gt;Please refer to the attached schematics on T2080QDS. &lt;BR /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-size: 10.0pt; "&gt;Please try increase your timeout value SYSCTL[DTOCV] to be E.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-size: 10.0pt; "&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-size: 10.0pt; "&gt;Yiping&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Jun 2019 13:57:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4160-SD-card-interface/m-p/955887#M3263</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2019-06-29T13:57:04Z</dc:date>
    </item>
  </channel>
</rss>