<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックT2080 Linux.uImage binary</title>
    <link>https://community.nxp.com/t5/T-Series/T2080-Linux-uImage-binary/m-p/952401#M3234</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How can I get a Linux.uImage for a T2080qds system? The image resides at flash address E8020000 and EC020000 and is approximately 7 MB. The flash there was inadvertently erased. If I can get a binary image that I can re-load that would be great. Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Sep 2019 16:53:56 GMT</pubDate>
    <dc:creator>clay_s_brice</dc:creator>
    <dc:date>2019-09-20T16:53:56Z</dc:date>
    <item>
      <title>T2080 Linux.uImage binary</title>
      <link>https://community.nxp.com/t5/T-Series/T2080-Linux-uImage-binary/m-p/952401#M3234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How can I get a Linux.uImage for a T2080qds system? The image resides at flash address E8020000 and EC020000 and is approximately 7 MB. The flash there was inadvertently erased. If I can get a binary image that I can re-load that would be great. Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Sep 2019 16:53:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2080-Linux-uImage-binary/m-p/952401#M3234</guid>
      <dc:creator>clay_s_brice</dc:creator>
      <dc:date>2019-09-20T16:53:56Z</dc:date>
    </item>
    <item>
      <title>Re: T2080 Linux.uImage binary</title>
      <link>https://community.nxp.com/t5/T-Series/T2080-Linux-uImage-binary/m-p/952402#M3235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Pre-built images (including uImage) are provided on the QorIQ Linux SDK v2.0 PPC64E6500 IMAGE.iso and QorIQ Linux SDK v2.0 PPCE6500 IMAGE.iso which can be downloaded from:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/linux-sdk-for-qoriq-processors:SDKLINUX?&amp;amp;code=SDKLINUX&amp;amp;nodeId=0152109D3F8624&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#nogo" title="https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/linux-sdk-for-qoriq-processors:SDKLINUX?&amp;amp;code=SDKLINUX&amp;amp;nodeId=0152109D3F8624&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#nogo"&gt;Linux® SDK for QorIQ® Processors | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also the ISOs contain complete NOR Flash images.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Sep 2019 09:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2080-Linux-uImage-binary/m-p/952402#M3235</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-09-21T09:38:55Z</dc:date>
    </item>
  </channel>
</rss>