<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Series中的主题 LCD Interface with 1042RDB</title>
    <link>https://community.nxp.com/t5/T-Series/LCD-Interface-with-1042RDB/m-p/931454#M3182</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How to interface TFT LCD(LQ150X1LW71N) that is shown in reference schematic with T1042RDB? The brightness control connectors of the LCD panel are two pin connector and there is 3 pin connector on board(J16, J17) . Similarly there are two connectors(J16,J17) on board relevant to LCD's brightness whereas there are four connectors(CN2,3,4,5) on LCD panel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Sep 2019 12:11:37 GMT</pubDate>
    <dc:creator>athershehzad</dc:creator>
    <dc:date>2019-09-30T12:11:37Z</dc:date>
    <item>
      <title>LCD Interface with 1042RDB</title>
      <link>https://community.nxp.com/t5/T-Series/LCD-Interface-with-1042RDB/m-p/931454#M3182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How to interface TFT LCD(LQ150X1LW71N) that is shown in reference schematic with T1042RDB? The brightness control connectors of the LCD panel are two pin connector and there is 3 pin connector on board(J16, J17) . Similarly there are two connectors(J16,J17) on board relevant to LCD's brightness whereas there are four connectors(CN2,3,4,5) on LCD panel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Sep 2019 12:11:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/LCD-Interface-with-1042RDB/m-p/931454#M3182</guid>
      <dc:creator>athershehzad</dc:creator>
      <dc:date>2019-09-30T12:11:37Z</dc:date>
    </item>
    <item>
      <title>Re: LCD Interface with 1042RDB</title>
      <link>https://community.nxp.com/t5/T-Series/LCD-Interface-with-1042RDB/m-p/931455#M3183</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is required to use DC to AC inverter.&lt;/P&gt;&lt;P&gt;For example, DMD43246:&lt;/P&gt;&lt;P&gt;&lt;A class="jivelink1" href="http://www.ergpower.com/pdf30/DmD43246.pdf" title="http://www.ergpower.com/pdf30/DmD43246.pdf"&gt;http://www.ergpower.com/pdf30/DmD43246.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The RDB 16-2 provides 12V for the inverter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To control ON/OFF and brightness it is needed to connect:&lt;/P&gt;&lt;P&gt;RDB&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Inverter&lt;/P&gt;&lt;P&gt;J17-1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;J1-5&lt;/P&gt;&lt;P&gt;J17-3&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; J1-6&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Sep 2019 15:29:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/LCD-Interface-with-1042RDB/m-p/931455#M3183</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-09-30T15:29:23Z</dc:date>
    </item>
    <item>
      <title>Re: LCD Interface with 1042RDB</title>
      <link>https://community.nxp.com/t5/T-Series/LCD-Interface-with-1042RDB/m-p/931456#M3184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Then how the brightness is controlled of the LCD.&lt;BR /&gt;What is will be connected to J17 ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Oct 2019 06:41:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/LCD-Interface-with-1042RDB/m-p/931456#M3184</guid>
      <dc:creator>athershehzad</dc:creator>
      <dc:date>2019-10-01T06:41:33Z</dc:date>
    </item>
  </channel>
</rss>