<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: T2080 USB control signals in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T2080-USB-control-signals/m-p/910561#M3127</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is possible to not use the signals in question, but the board designer still has to take precautions to eliminate possible hardware damage in case of USB device power failure.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Aug 2019 13:32:42 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2019-08-27T13:32:42Z</dc:date>
    <item>
      <title>T2080 USB control signals</title>
      <link>https://community.nxp.com/t5/T-Series/T2080-USB-control-signals/m-p/910560#M3126</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If I don't use the USB power fault and usb power enable signals, would I have any problem with this interface?&lt;/P&gt;&lt;P&gt;I don't want to use them since I am using the same 5V regulator to supply USB and other devices, so I don't want USB controller to controls also those other devices.&lt;/P&gt;&lt;P&gt;Should I use a specific 5V source to USB so I can control it with the above mentioned signals or it is not necessary?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 07:14:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2080-USB-control-signals/m-p/910560#M3126</guid>
      <dc:creator>paulagarcía-mor</dc:creator>
      <dc:date>2019-08-27T07:14:20Z</dc:date>
    </item>
    <item>
      <title>Re: T2080 USB control signals</title>
      <link>https://community.nxp.com/t5/T-Series/T2080-USB-control-signals/m-p/910561#M3127</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is possible to not use the signals in question, but the board designer still has to take precautions to eliminate possible hardware damage in case of USB device power failure.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 13:32:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2080-USB-control-signals/m-p/910561#M3127</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2019-08-27T13:32:42Z</dc:date>
    </item>
  </channel>
</rss>