<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: T2080 SerDes Clock Signals in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T2080-SerDes-Clock-Signals/m-p/899941#M3104</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;According to the datasheet of the microprocessor, the input voltage range of every SerDes signal, including clocks, is GND to SVDD (which is 1V).&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Please look T2080 device datasheet, Section 3.19.2.2 "SerDes reference clock receiver characteristics". There are 50 Ohm on-chip termination and AC decoupling. Actual voltage amplitude depends on how clock driver is coupled with clock input.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;But, in the reference design board, the serdes clock signals that go to the T2080 inputs (SD1_REFCLK1_P, SD_REFCLK1_N...) have a higher voltage level (2V5/3V3).&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The chip U23 (PI3PCIE3212), which is powered from 3.3V, is only switch chip, and the fact that this switch is powered from 3.3V does not mean output signals are 3.3V. The chip U48 (IDT9FGV0641) is powered from 1.8V, and there is also output termination.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 May 2019 16:49:26 GMT</pubDate>
    <dc:creator>alexander_yakov</dc:creator>
    <dc:date>2019-05-03T16:49:26Z</dc:date>
    <item>
      <title>T2080 SerDes Clock Signals</title>
      <link>https://community.nxp.com/t5/T-Series/T2080-SerDes-Clock-Signals/m-p/899940#M3103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with a T2080 device and I need some help to understand the voltage level of some signals.&lt;/P&gt;&lt;P&gt;According to the datasheet of the microprocessor, the input voltage range of every SerDes signal, including clocks, is GND to SVDD (which is 1V).&lt;/P&gt;&lt;P&gt;But, in the reference design board, the serdes clock signals that go to the T2080 inputs (SD1_REFCLK1_P, SD_REFCLK1_N...) have a higher voltage level (2V5/3V3).&lt;/P&gt;&lt;P&gt;How can it be possible?&amp;nbsp; Is the input voltage range higher for clock signals than for the rest of the serdes signals?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Paula&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 May 2019 09:17:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2080-SerDes-Clock-Signals/m-p/899940#M3103</guid>
      <dc:creator>paulagarcía-mor</dc:creator>
      <dc:date>2019-05-03T09:17:44Z</dc:date>
    </item>
    <item>
      <title>Re: T2080 SerDes Clock Signals</title>
      <link>https://community.nxp.com/t5/T-Series/T2080-SerDes-Clock-Signals/m-p/899941#M3104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;According to the datasheet of the microprocessor, the input voltage range of every SerDes signal, including clocks, is GND to SVDD (which is 1V).&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Please look T2080 device datasheet, Section 3.19.2.2 "SerDes reference clock receiver characteristics". There are 50 Ohm on-chip termination and AC decoupling. Actual voltage amplitude depends on how clock driver is coupled with clock input.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;But, in the reference design board, the serdes clock signals that go to the T2080 inputs (SD1_REFCLK1_P, SD_REFCLK1_N...) have a higher voltage level (2V5/3V3).&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The chip U23 (PI3PCIE3212), which is powered from 3.3V, is only switch chip, and the fact that this switch is powered from 3.3V does not mean output signals are 3.3V. The chip U48 (IDT9FGV0641) is powered from 1.8V, and there is also output termination.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 May 2019 16:49:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2080-SerDes-Clock-Signals/m-p/899941#M3104</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2019-05-03T16:49:26Z</dc:date>
    </item>
  </channel>
</rss>