<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックT4240 usb boot</title>
    <link>https://community.nxp.com/t5/T-Series/T4240-usb-boot/m-p/429859#M287</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;how to boot full rootfs image using the usb boot&lt;/P&gt;&lt;P&gt;at the uboot prompt iam getting the following error i have partitioned the usb and copied the full rootfs image on to the file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="Standard"&gt;usb start - start (scan) USB controller&lt;/P&gt;&lt;P class="Standard"&gt;usb reset - reset (rescan) USB controller&lt;/P&gt;&lt;P class="Standard"&gt;usb stop [f] - stop USB [f]=force stop&lt;/P&gt;&lt;P class="Standard"&gt;usb tree - show USB device tree&lt;/P&gt;&lt;P class="Standard"&gt;usb info [dev] - show available USB devices&lt;/P&gt;&lt;P class="Standard"&gt;usb test [dev] [port] [mode] - set USB 2.0 test mode&lt;/P&gt;&lt;P class="Standard"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; (specify port 0 to indicate the device's upstream port)&lt;/P&gt;&lt;P class="Standard"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Available modes: J, K, S[E0_NAK], P[acket], F[orce_Enable]&lt;/P&gt;&lt;P class="Standard"&gt;usb storage - show details of USB storage devices&lt;/P&gt;&lt;P class="Standard"&gt;usb dev [dev] - show or set current USB storage device&lt;/P&gt;&lt;P class="Standard"&gt;usb part [dev] - print partition table of one or all USB storage&amp;nbsp;&amp;nbsp;&amp;nbsp; devices&lt;/P&gt;&lt;P class="Standard"&gt;usb read addr blk# cnt - read `cnt' blocks starting at block `blk#'&lt;/P&gt;&lt;P class="Standard"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; to memory address `addr'&lt;/P&gt;&lt;P class="Standard"&gt;usb write addr blk# cnt - write `cnt' blocks starting at block `blk#'&lt;/P&gt;&lt;P class="Standard"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; from memory address `addr'&lt;/P&gt;&lt;P class="Standard"&gt;=&amp;gt; usb dev&lt;/P&gt;&lt;P class="Standard"&gt;&lt;/P&gt;&lt;P class="Standard"&gt;USB device 0: Vendor: hp&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Rev: 1100 Prod: v210w&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P class="Standard"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Type: Removable Hard Disk&lt;/P&gt;&lt;P class="Standard"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Capacity: 7680.0 MB = 7.5 GB (15728640 x 512)&lt;/P&gt;&lt;P class="Standard"&gt;=&amp;gt; usb dev device 0&lt;/P&gt;&lt;P class="Standard"&gt;&lt;/P&gt;&lt;P class="Standard"&gt;USB device 0: Vendor: hp&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Rev: 1100 Prod: v210w&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P class="Standard"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Type: Removable Hard Disk&lt;/P&gt;&lt;P class="Standard"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Capacity: 7680.0 MB = 7.5 GB (15728640 x 512)&lt;/P&gt;&lt;P class="Standard"&gt;=&amp;gt; usbboot device 0&lt;/P&gt;&lt;P class="Standard"&gt;&lt;/P&gt;&lt;P class="Standard"&gt;Loading from usb device 0, partition 1: Name: usbda1&amp;nbsp; Type: U-Boot&lt;/P&gt;&lt;P class="Standard"&gt;** Unknown image type&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Oct 2015 14:58:07 GMT</pubDate>
    <dc:creator>varunkjayan</dc:creator>
    <dc:date>2015-10-26T14:58:07Z</dc:date>
    <item>
      <title>T4240 usb boot</title>
      <link>https://community.nxp.com/t5/T-Series/T4240-usb-boot/m-p/429859#M287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;how to boot full rootfs image using the usb boot&lt;/P&gt;&lt;P&gt;at the uboot prompt iam getting the following error i have partitioned the usb and copied the full rootfs image on to the file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="Standard"&gt;usb start - start (scan) USB controller&lt;/P&gt;&lt;P class="Standard"&gt;usb reset - reset (rescan) USB controller&lt;/P&gt;&lt;P class="Standard"&gt;usb stop [f] - stop USB [f]=force stop&lt;/P&gt;&lt;P class="Standard"&gt;usb tree - show USB device tree&lt;/P&gt;&lt;P class="Standard"&gt;usb info [dev] - show available USB devices&lt;/P&gt;&lt;P class="Standard"&gt;usb test [dev] [port] [mode] - set USB 2.0 test mode&lt;/P&gt;&lt;P class="Standard"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; (specify port 0 to indicate the device's upstream port)&lt;/P&gt;&lt;P class="Standard"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Available modes: J, K, S[E0_NAK], P[acket], F[orce_Enable]&lt;/P&gt;&lt;P class="Standard"&gt;usb storage - show details of USB storage devices&lt;/P&gt;&lt;P class="Standard"&gt;usb dev [dev] - show or set current USB storage device&lt;/P&gt;&lt;P class="Standard"&gt;usb part [dev] - print partition table of one or all USB storage&amp;nbsp;&amp;nbsp;&amp;nbsp; devices&lt;/P&gt;&lt;P class="Standard"&gt;usb read addr blk# cnt - read `cnt' blocks starting at block `blk#'&lt;/P&gt;&lt;P class="Standard"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; to memory address `addr'&lt;/P&gt;&lt;P class="Standard"&gt;usb write addr blk# cnt - write `cnt' blocks starting at block `blk#'&lt;/P&gt;&lt;P class="Standard"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; from memory address `addr'&lt;/P&gt;&lt;P class="Standard"&gt;=&amp;gt; usb dev&lt;/P&gt;&lt;P class="Standard"&gt;&lt;/P&gt;&lt;P class="Standard"&gt;USB device 0: Vendor: hp&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Rev: 1100 Prod: v210w&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P class="Standard"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Type: Removable Hard Disk&lt;/P&gt;&lt;P class="Standard"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Capacity: 7680.0 MB = 7.5 GB (15728640 x 512)&lt;/P&gt;&lt;P class="Standard"&gt;=&amp;gt; usb dev device 0&lt;/P&gt;&lt;P class="Standard"&gt;&lt;/P&gt;&lt;P class="Standard"&gt;USB device 0: Vendor: hp&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Rev: 1100 Prod: v210w&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P class="Standard"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Type: Removable Hard Disk&lt;/P&gt;&lt;P class="Standard"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Capacity: 7680.0 MB = 7.5 GB (15728640 x 512)&lt;/P&gt;&lt;P class="Standard"&gt;=&amp;gt; usbboot device 0&lt;/P&gt;&lt;P class="Standard"&gt;&lt;/P&gt;&lt;P class="Standard"&gt;Loading from usb device 0, partition 1: Name: usbda1&amp;nbsp; Type: U-Boot&lt;/P&gt;&lt;P class="Standard"&gt;** Unknown image type&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Oct 2015 14:58:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4240-usb-boot/m-p/429859#M287</guid>
      <dc:creator>varunkjayan</dc:creator>
      <dc:date>2015-10-26T14:58:07Z</dc:date>
    </item>
  </channel>
</rss>