<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Series中的主题 Multicore Application</title>
    <link>https://community.nxp.com/t5/T-Series/Multicore-Application/m-p/826181#M2761</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Any sample application code is available to teset T4241 Multiple core.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Avinash N&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Jul 2018 08:43:32 GMT</pubDate>
    <dc:creator>avinashneethi</dc:creator>
    <dc:date>2018-07-18T08:43:32Z</dc:date>
    <item>
      <title>Multicore Application</title>
      <link>https://community.nxp.com/t5/T-Series/Multicore-Application/m-p/826181#M2761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Any sample application code is available to teset T4241 Multiple core.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Avinash N&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 08:43:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Multicore-Application/m-p/826181#M2761</guid>
      <dc:creator>avinashneethi</dc:creator>
      <dc:date>2018-07-18T08:43:32Z</dc:date>
    </item>
    <item>
      <title>Re: Multicore Application</title>
      <link>https://community.nxp.com/t5/T-Series/Multicore-Application/m-p/826182#M2762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Avinash N,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could create a bareboard project for T4240 in CodeWarrior IDE following new project wizards, in the Configurations panel, please select SMP and select Core index for all cores. Then connect CodeWarrior to the target board to execute the sample program at all cores.&lt;/P&gt;&lt;P&gt;In addition, in Debug Target Settings panel, please select "Download SRAM" or "Connect SRAM" Launch configuration to avoid DDR controller configuration trouble.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Aug 2018 06:34:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Multicore-Application/m-p/826182#M2762</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2018-08-03T06:34:14Z</dc:date>
    </item>
  </channel>
</rss>