<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックRe: T2081 interface with F-RAM</title>
    <link>https://community.nxp.com/t5/T-Series/T2081-interface-with-F-RAM/m-p/801279#M2686</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pavel Chubakov,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the reply.&lt;/P&gt;&lt;P&gt;i have one more doubt,&lt;/P&gt;&lt;P&gt;where to do pin muxing and input output mapping in case to T2080 RDB board,&lt;/P&gt;&lt;P&gt;as in case of IMX6UL we are specifically having pin muxing related header file present in U-boot and kernel,&lt;/P&gt;&lt;P&gt;i am trying to find the same for t2080RDB which i am not getting.&lt;/P&gt;&lt;P&gt;to configure the IO mapping as per the our custom board.&lt;/P&gt;&lt;P&gt;Any suggestion would be appreciated,kindly help to solve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reagrds,&lt;/P&gt;&lt;P&gt;Anshul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Oct 2018 10:03:26 GMT</pubDate>
    <dc:creator>anshulkhare</dc:creator>
    <dc:date>2018-10-26T10:03:26Z</dc:date>
    <item>
      <title>T2081 interface with F-RAM</title>
      <link>https://community.nxp.com/t5/T-Series/T2081-interface-with-F-RAM/m-p/801276#M2683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;we have T2081 custom board based on T2080RDB-PC,&lt;/P&gt;&lt;P&gt;in the custom board we have connected F-RAM(CY15B102Q-SXE) via SPI bus,&lt;/P&gt;&lt;P&gt;For connecting the F-RAM peripheral via SPI, what changes we have to do,&lt;/P&gt;&lt;P&gt;or do we have to write a new driver program for the interfacing T2081 and F-RAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestion would be appreciated,kindly help to solve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Anshul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2018 06:40:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2081-interface-with-F-RAM/m-p/801276#M2683</guid>
      <dc:creator>anshulkhare</dc:creator>
      <dc:date>2018-10-17T06:40:12Z</dc:date>
    </item>
    <item>
      <title>Re: T2081 interface with F-RAM</title>
      <link>https://community.nxp.com/t5/T-Series/T2081-interface-with-F-RAM/m-p/801277#M2684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;i did the changes as per this link &lt;A class="link-titled" href="https://community.cypress.com/docs/DOC-14647" title="https://community.cypress.com/docs/DOC-14647"&gt;F-RAM Support under Linux – KBA223028 | Cypress Developer Community&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;after modification&amp;nbsp; i have a doubt as we have added device support in the drivers/mtd/spi-nor/spi-nor.c&lt;/P&gt;&lt;P&gt;do we require to modify my board.c file and dts ???&lt;/P&gt;&lt;P&gt;Any suggestion would be appreciated,kindly help to solve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Anshul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Oct 2018 13:09:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2081-interface-with-F-RAM/m-p/801277#M2684</guid>
      <dc:creator>anshulkhare</dc:creator>
      <dc:date>2018-10-23T13:09:22Z</dc:date>
    </item>
    <item>
      <title>Re: T2081 interface with F-RAM</title>
      <link>https://community.nxp.com/t5/T-Series/T2081-interface-with-F-RAM/m-p/801278#M2685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;The T2080RDB Linux supports SPI-NOR Flash&lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt; Micron n25q512a&lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;. See attached .dts file&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;This &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;F-RAM uses similar commands as the n25q512a&lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;It looks like that driver for the &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;n25q512a can be used for CY15B102Q.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Oct 2018 11:09:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2081-interface-with-F-RAM/m-p/801278#M2685</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2018-10-25T11:09:37Z</dc:date>
    </item>
    <item>
      <title>Re: T2081 interface with F-RAM</title>
      <link>https://community.nxp.com/t5/T-Series/T2081-interface-with-F-RAM/m-p/801279#M2686</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pavel Chubakov,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the reply.&lt;/P&gt;&lt;P&gt;i have one more doubt,&lt;/P&gt;&lt;P&gt;where to do pin muxing and input output mapping in case to T2080 RDB board,&lt;/P&gt;&lt;P&gt;as in case of IMX6UL we are specifically having pin muxing related header file present in U-boot and kernel,&lt;/P&gt;&lt;P&gt;i am trying to find the same for t2080RDB which i am not getting.&lt;/P&gt;&lt;P&gt;to configure the IO mapping as per the our custom board.&lt;/P&gt;&lt;P&gt;Any suggestion would be appreciated,kindly help to solve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reagrds,&lt;/P&gt;&lt;P&gt;Anshul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Oct 2018 10:03:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2081-interface-with-F-RAM/m-p/801279#M2686</guid>
      <dc:creator>anshulkhare</dc:creator>
      <dc:date>2018-10-26T10:03:26Z</dc:date>
    </item>
  </channel>
</rss>