<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: T4240 XAUI configuration in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T4240-XAUI-configuration/m-p/781998#M2640</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Platon,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; we have not connected PHY, we have connected an transceiver to sfp+ (XAUI &amp;lt;---&amp;gt;TLK10232 &amp;lt;----&amp;gt; SFP+). In U-Boot we can able to access the device. But in linux It is showing error message as,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fsl_dpaa_mac ffe4f2000.ethernet fm1-mac9: init_phy() failed&lt;BR /&gt;ifconfig: SIOCSIFFLAGS: No such device&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can be the issue. Any handelings has to be done in DTS ?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Avinash N&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Oct 2018 11:10:00 GMT</pubDate>
    <dc:creator>avinashneethi</dc:creator>
    <dc:date>2018-10-30T11:10:00Z</dc:date>
    <item>
      <title>T4240 XAUI configuration</title>
      <link>https://community.nxp.com/t5/T-Series/T4240-XAUI-configuration/m-p/781996#M2638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; We are facing a serious issue with respect to &lt;A data-saferedirecturl="https://www.google.com/url?hl=en&amp;amp;q=http://www.ti.com/product/TLK10232&amp;amp;source=gmail&amp;amp;ust=1536150335306000&amp;amp;usg=AFQjCNEofXKgeQseSy-dNEPqd-PMQ-ZH1Q" href="http://www.ti.com/product/TLK10232" target="_blank" title="Link to Product Folder"&gt;TLK10232&lt;/A&gt;. We made a customized design with T4240 Processor along with the &lt;A data-saferedirecturl="https://www.google.com/url?hl=en&amp;amp;q=http://www.ti.com/product/TLK10232&amp;amp;source=gmail&amp;amp;ust=1536150335306000&amp;amp;usg=AFQjCNEofXKgeQseSy-dNEPqd-PMQ-ZH1Q" href="http://www.ti.com/product/TLK10232" target="_blank" title="Link to Product Folder"&gt;TLK10232&lt;/A&gt;. We are using U-Boot version - 2016.01 and kernel version - 4.1.8 .&amp;nbsp; &lt;A data-saferedirecturl="https://www.google.com/url?hl=en&amp;amp;q=http://www.ti.com/product/TLK10232&amp;amp;source=gmail&amp;amp;ust=1536150335306000&amp;amp;usg=AFQjCNEofXKgeQseSy-dNEPqd-PMQ-ZH1Q" href="http://www.ti.com/product/TLK10232" target="_blank" title="Link to Product Folder"&gt;TLK10232&lt;/A&gt; mdc and mdio are connected to the T4240 Processor.&amp;nbsp; Input reference clock is 156.25MHz. Pins That are hardwired,&lt;/P&gt;&lt;P&gt;PRTAD[4:0] - 11010,&lt;/P&gt;&lt;P&gt;ST - 0 and&lt;/P&gt;&lt;P&gt;MODE_SEL - 0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="DSC_0014.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67990i3B41105F4E9DAF28/image-size/large?v=v2&amp;amp;px=999" role="button" title="DSC_0014.JPG" alt="DSC_0014.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can we able to perform the read and write operation on the MDIO register space in uboot?&lt;/P&gt;&lt;P&gt;so that the path from T4240 to TLK10232 is clear ?&lt;/P&gt;&lt;P&gt;&lt;A data-saferedirecturl="https://www.google.com/url?hl=en&amp;amp;q=http://www.ti.com/product/TLK10232&amp;amp;source=gmail&amp;amp;ust=1536150335307000&amp;amp;usg=AFQjCNGmNWUfxXtwcgWnKzoGDgDiVM6f1g" href="http://www.ti.com/product/TLK10232" target="_blank" title="Link to Product Folder"&gt;http://www.ti.com/product/TLK10232&lt;/A&gt; Bulk Production is on hold due to this issue. Kindly Provide some idea to resolve this issue.&lt;/P&gt;&lt;P&gt;Thanks in Advance.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Avinash N&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Sep 2018 10:25:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4240-XAUI-configuration/m-p/781996#M2638</guid>
      <dc:creator>avinashneethi</dc:creator>
      <dc:date>2018-09-20T10:25:05Z</dc:date>
    </item>
    <item>
      <title>Re: T4240 XAUI configuration</title>
      <link>https://community.nxp.com/t5/T-Series/T4240-XAUI-configuration/m-p/781997#M2639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;NXP QorIQ SDK u-Boot does have provisions for communication with MDIO-&lt;BR /&gt;attached PHYs. If it is a custom board, make sure&amp;nbsp; your board-specific&lt;BR /&gt;code properly registers the MDIO controller your PHY connects to by&lt;BR /&gt;calling fm_memac_mdio_init() and sets your PHYs management addresses&lt;BR /&gt;by fm_info_set_phy_address(). If your board code does everything properly,&lt;BR /&gt;you should be able to communicate to your PHY using 'mii' CLI command.&lt;BR /&gt;See&amp;nbsp; board_eth_init() function defined in board/freescale/t4rdb/eth.c &lt;BR /&gt;procedure for a reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note,&amp;nbsp; the above functions and files may not be implemented, or may look differently&lt;/P&gt;&lt;P&gt;if you are working with a non-SDK version of u-Boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Oct 2018 09:07:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4240-XAUI-configuration/m-p/781997#M2639</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2018-10-24T09:07:31Z</dc:date>
    </item>
    <item>
      <title>Re: T4240 XAUI configuration</title>
      <link>https://community.nxp.com/t5/T-Series/T4240-XAUI-configuration/m-p/781998#M2640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Platon,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; we have not connected PHY, we have connected an transceiver to sfp+ (XAUI &amp;lt;---&amp;gt;TLK10232 &amp;lt;----&amp;gt; SFP+). In U-Boot we can able to access the device. But in linux It is showing error message as,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fsl_dpaa_mac ffe4f2000.ethernet fm1-mac9: init_phy() failed&lt;BR /&gt;ifconfig: SIOCSIFFLAGS: No such device&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can be the issue. Any handelings has to be done in DTS ?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Avinash N&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Oct 2018 11:10:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4240-XAUI-configuration/m-p/781998#M2640</guid>
      <dc:creator>avinashneethi</dc:creator>
      <dc:date>2018-10-30T11:10:00Z</dc:date>
    </item>
  </channel>
</rss>