<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: T1024 Second Core Bootup in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T1024-Second-Core-Bootup/m-p/781704#M2637</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="321286" data-username="kushshah" href="https://community.nxp.com/people/kushshah"&gt;Kush Shah&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When each core comes out of reset, its MMU has one 4KB page defined at 0x0_FFFF_Fnnn. Each core begins execution with the instruction at the effective address 0x0_FFFF_FFFC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To boot space translation mechanism allows translation of this window(in physical address space) to one specified by BSTRH, BSTRL and BSTAR. Processor will fetch first instruction from effective address 0xFFFF_FFFC as usual, the boot space translation mechanism will translate the physical address to the specific address such as 0x6_0000_0FFC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Each core has its own default 4K TLB entry, the boot space translation affects transactions initiated by all cores in the same manner.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Oct 2018 05:38:27 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2018-10-29T05:38:27Z</dc:date>
    <item>
      <title>T1024 Second Core Bootup</title>
      <link>https://community.nxp.com/t5/T-Series/T1024-Second-Core-Bootup/m-p/781703#M2636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does MMU for core-1 has default 4 KB page defined at&amp;nbsp; &lt;SPAN&gt;0x0_FFFF_Fnnn even w&lt;/SPAN&gt;hen boot space translation is enabled? or Does MMU provides access for the page which is set it up by the&amp;nbsp;Boot space translation register low (LCC_BSTRL)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can we set up TLB entry for the page defined in&amp;nbsp;&lt;SPAN&gt;LCC_BSTRL for core-1 from core-0 before releasing the core-1?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have referred u-boot code (mp.c), in that they are disabling the default reset page TLB and set it up that TLB with the page which will set up by&amp;nbsp;LCC_BSTRL. Does default TLB entry is global for both cores?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Oct 2018 13:47:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1024-Second-Core-Bootup/m-p/781703#M2636</guid>
      <dc:creator>kushshah</dc:creator>
      <dc:date>2018-10-11T13:47:27Z</dc:date>
    </item>
    <item>
      <title>Re: T1024 Second Core Bootup</title>
      <link>https://community.nxp.com/t5/T-Series/T1024-Second-Core-Bootup/m-p/781704#M2637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="321286" data-username="kushshah" href="https://community.nxp.com/people/kushshah"&gt;Kush Shah&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When each core comes out of reset, its MMU has one 4KB page defined at 0x0_FFFF_Fnnn. Each core begins execution with the instruction at the effective address 0x0_FFFF_FFFC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To boot space translation mechanism allows translation of this window(in physical address space) to one specified by BSTRH, BSTRL and BSTAR. Processor will fetch first instruction from effective address 0xFFFF_FFFC as usual, the boot space translation mechanism will translate the physical address to the specific address such as 0x6_0000_0FFC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Each core has its own default 4K TLB entry, the boot space translation affects transactions initiated by all cores in the same manner.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Oct 2018 05:38:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1024-Second-Core-Bootup/m-p/781704#M2637</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2018-10-29T05:38:27Z</dc:date>
    </item>
  </channel>
</rss>