<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックRe: IFC Flash Timing Register</title>
    <link>https://community.nxp.com/t5/T-Series/IFC-Flash-Timing-Register/m-p/778656#M2600</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;The ip_clk is the IFC module input clock. Frequency of the ip_clk is 1/2 platform Clock – refer to the QorIQ T1040 Reference Manual, 4.6.7.2 IP Logic Clock Distribution and Configuration.&lt;/P&gt;&lt;P&gt;How fields of the timing registers define NOR read/write timing you can see on Figure 24-38. Read cycle timing and Figure 24-40. Write cycle timing in the manual. F.e. let platform clock is 500 MHz (i.e. ip_clk cycle tIP = 2/500MHz = 4 ns). According to the datasheets the MT28EW01GABA1LPC has (OE# LOW to output valid) tOE=25 ns; the T1042 IFC input has 2* tIP setup time. So from Figure 24-38 we can conclude that TRAD*tIP should cover tOE+tSetup i.e. TRAD should be &amp;gt;= (floor(25ns/4)+1) +2 = (6+1)+2 = 9.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Nov 2017 10:08:17 GMT</pubDate>
    <dc:creator>r8070z</dc:creator>
    <dc:date>2017-11-16T10:08:17Z</dc:date>
    <item>
      <title>IFC Flash Timing Register</title>
      <link>https://community.nxp.com/t5/T-Series/IFC-Flash-Timing-Register/m-p/778655#M2599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;I am using T1042 and interfacing NOR Flash (part no :&amp;nbsp;MT28EW01GABA1LPC-1SIT ) to IFC.&lt;/P&gt;&lt;P&gt;I have done most of its setting but now i am confused in &lt;STRONG&gt;Flash Timing Registers&lt;/STRONG&gt;. I have read the reference manual but i cannot decide that what values should i set in all timing registers and what is frequency of &lt;STRONG&gt;ip_clk&lt;/STRONG&gt; that is used in diagrams of reference manual.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Nov 2017 07:31:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/IFC-Flash-Timing-Register/m-p/778655#M2599</guid>
      <dc:creator>faizmajeed</dc:creator>
      <dc:date>2017-11-15T07:31:08Z</dc:date>
    </item>
    <item>
      <title>Re: IFC Flash Timing Register</title>
      <link>https://community.nxp.com/t5/T-Series/IFC-Flash-Timing-Register/m-p/778656#M2600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;The ip_clk is the IFC module input clock. Frequency of the ip_clk is 1/2 platform Clock – refer to the QorIQ T1040 Reference Manual, 4.6.7.2 IP Logic Clock Distribution and Configuration.&lt;/P&gt;&lt;P&gt;How fields of the timing registers define NOR read/write timing you can see on Figure 24-38. Read cycle timing and Figure 24-40. Write cycle timing in the manual. F.e. let platform clock is 500 MHz (i.e. ip_clk cycle tIP = 2/500MHz = 4 ns). According to the datasheets the MT28EW01GABA1LPC has (OE# LOW to output valid) tOE=25 ns; the T1042 IFC input has 2* tIP setup time. So from Figure 24-38 we can conclude that TRAD*tIP should cover tOE+tSetup i.e. TRAD should be &amp;gt;= (floor(25ns/4)+1) +2 = (6+1)+2 = 9.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Nov 2017 10:08:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/IFC-Flash-Timing-Register/m-p/778656#M2600</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2017-11-16T10:08:17Z</dc:date>
    </item>
    <item>
      <title>Re: IFC Flash Timing Register</title>
      <link>https://community.nxp.com/t5/T-Series/IFC-Flash-Timing-Register/m-p/778657#M2601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got your point, But i have read in T1042 Manual that we can set IFC max clock 100MHZ . How can i set it 500MHZ&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33592i21271927A626857C/image-size/large?v=v2&amp;amp;px=999" title="Capture.PNG" alt="Capture.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Nov 2017 10:34:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/IFC-Flash-Timing-Register/m-p/778657#M2601</guid>
      <dc:creator>faizmajeed</dc:creator>
      <dc:date>2017-11-16T10:34:25Z</dc:date>
    </item>
    <item>
      <title>Re: IFC Flash Timing Register</title>
      <link>https://community.nxp.com/t5/T-Series/IFC-Flash-Timing-Register/m-p/778658#M2602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: #51626f; background: white;"&gt;I wrote let “&lt;STRONG&gt;platform &lt;/STRONG&gt;clock is 500 MHz” and “The &lt;STRONG&gt;ip_clk&lt;/STRONG&gt; is the IFC module input clock”. It is not output clock on the IFC_CLK pin which they name as &lt;STRONG&gt;IFC clock frequency&lt;/STRONG&gt;.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Nov 2017 14:19:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/IFC-Flash-Timing-Register/m-p/778658#M2602</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2017-11-20T14:19:37Z</dc:date>
    </item>
  </channel>
</rss>