<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PCIe in End Point mode in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/PCIe-in-End-Point-mode/m-p/770083#M2560</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the attached document.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Jan 2018 09:54:41 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2018-01-31T09:54:41Z</dc:date>
    <item>
      <title>PCIe in End Point mode</title>
      <link>https://community.nxp.com/t5/T-Series/PCIe-in-End-Point-mode/m-p/770082#M2559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to use QorIQ T1024 processor's PCIe port in End Point mode. My aim is to configure T1024 behave as a Memory Controller device on pci bus.&lt;/P&gt;&lt;P&gt;From reference manual, I understood that I need to set the pcie port to End Point mode in RCW to configure hardware. What else should I do to configure Software side?&amp;nbsp;I need Bars and set MSI interrupts to communicate with Host. Is it the same way as in RC mode? Can anybody share a sample code?&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jan 2018 05:27:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/PCIe-in-End-Point-mode/m-p/770082#M2559</guid>
      <dc:creator>leventkarakaya</dc:creator>
      <dc:date>2018-01-30T05:27:16Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe in End Point mode</title>
      <link>https://community.nxp.com/t5/T-Series/PCIe-in-End-Point-mode/m-p/770083#M2560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the attached document.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Jan 2018 09:54:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/PCIe-in-End-Point-mode/m-p/770083#M2560</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2018-01-31T09:54:41Z</dc:date>
    </item>
  </channel>
</rss>