<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Network ramdisk deployment from TFTP T2080RDB-PC in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/Network-ramdisk-deployment-from-TFTP-T2080RDB-PC/m-p/767475#M2545</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="315795" data-username="sandratrujillogarcía" href="https://community.nxp.com/people/sandratrujillogarcía"&gt;Sandra Trujillo García&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check whether you were using USDPAA dtb file to boot up the target board, if so please use the dtb file uImage-t2080rdb.dtb rather than uImage-t2080rdb-usdpaa*.dtb, because in USDPAA dtb file, all Ethernet interfaces have been assigned to USDPAA, so you cannot see any Ethernet interface in Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If your problem remains, please provide your the whole Linux booting up console log.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 May 2018 10:27:32 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2018-05-03T10:27:32Z</dc:date>
    <item>
      <title>Network ramdisk deployment from TFTP T2080RDB-PC</title>
      <link>https://community.nxp.com/t5/T-Series/Network-ramdisk-deployment-from-TFTP-T2080RDB-PC/m-p/767474#M2544</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;I have several questions about the configuration of the network on the T2080RDB-PC board when I load the image from RamDisk.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I load from ramdisk (TFTP) the image that I have built with yocto project I can't see the ethernet interfaces.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I turn on the board and let the SDK version (fsl-image-mfgtool) that was pre-installed start. With the ifconfig -a command I can see 6 network interfaces, these are all the interfaces that the T2080RDB-PC board has. The problem is when I want to load any of the images generated with yocto project (I have tried with the images fsl-image-minimal, fsl-image-mfgtool and fsl-image-full). In this case when I use the ifconfig -a command I can not see all these interfaces. How can I see all the ethernet interfaces when I use a loaded image on RamDisk with TFTP? How do I configure the interfaces to work with them?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for the help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2018 07:43:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Network-ramdisk-deployment-from-TFTP-T2080RDB-PC/m-p/767474#M2544</guid>
      <dc:creator>sandratrujillog</dc:creator>
      <dc:date>2018-04-25T07:43:07Z</dc:date>
    </item>
    <item>
      <title>Re: Network ramdisk deployment from TFTP T2080RDB-PC</title>
      <link>https://community.nxp.com/t5/T-Series/Network-ramdisk-deployment-from-TFTP-T2080RDB-PC/m-p/767475#M2545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="315795" data-username="sandratrujillogarcía" href="https://community.nxp.com/people/sandratrujillogarcía"&gt;Sandra Trujillo García&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check whether you were using USDPAA dtb file to boot up the target board, if so please use the dtb file uImage-t2080rdb.dtb rather than uImage-t2080rdb-usdpaa*.dtb, because in USDPAA dtb file, all Ethernet interfaces have been assigned to USDPAA, so you cannot see any Ethernet interface in Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If your problem remains, please provide your the whole Linux booting up console log.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 May 2018 10:27:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Network-ramdisk-deployment-from-TFTP-T2080RDB-PC/m-p/767475#M2545</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2018-05-03T10:27:32Z</dc:date>
    </item>
  </channel>
</rss>