<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Series中的主题 Re: Network connection problem with T2080RDB-PC</title>
    <link>https://community.nxp.com/t5/T-Series/Network-connection-problem-with-T2080RDB-PC/m-p/765937#M2517</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Think is also general typo in that docs have "FM1@GTECn" whereas u-boot has "FM1@TGECn" :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In any case have tried both ETH2 and ETH2 connected directly to my PC and to a network switch. In neither case can not get device to work either from Linux or u-boot. From linux:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fm1-mac1 Link encap:Ethernet HWaddr 00:04:9F:05:34:46 &lt;BR /&gt; inet addr:10.1.7.36 Bcast:10.1.255.255 Mask:255.255.0.0&lt;BR /&gt; inet6 addr: fe80::204:9fff:fe05:3446/64 Scope:Link&lt;BR /&gt; UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1&lt;BR /&gt; RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt; TX packets:6 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt; collisions:0 txqueuelen:1000 &lt;BR /&gt; RX bytes:0 (0.0 B) TX bytes:508 (508.0 B)&lt;BR /&gt; Memory:fe4e0000-fe4e0fff&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fm1-mac2 Link encap:Ethernet HWaddr 00:04:9F:05:34:47 &lt;BR /&gt; inet addr:192.168.0.2 Bcast:192.168.255.255 Mask:255.255.0.0&lt;BR /&gt; inet6 addr: fe80::204:9fff:fe05:3447/64 Scope:Link&lt;BR /&gt; UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1&lt;BR /&gt; RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt; TX packets:29 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt; collisions:0 txqueuelen:1000 &lt;BR /&gt; RX bytes:0 (0.0 B) TX bytes:1530 (1.4 KiB)&lt;BR /&gt; Memory:fe4e2000-fe4e2fff &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both ports have alternating flash link/activity lights, which sort of looks like some sort of device error status?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Jan 2018 16:28:01 GMT</pubDate>
    <dc:creator>steveosselton</dc:creator>
    <dc:date>2018-01-08T16:28:01Z</dc:date>
    <item>
      <title>Network connection problem with T2080RDB-PC</title>
      <link>https://community.nxp.com/t5/T-Series/Network-connection-problem-with-T2080RDB-PC/m-p/765935#M2515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to set up a T2080RDB-PC. I can connect via console to access uboot/Linux. I have connected&lt;/P&gt;&lt;P&gt;the ETH2 port (as labelled on front of system) but cannot seen to get a network connection working from&lt;/P&gt;&lt;P&gt;either u-boot or Linux. Have verified that am trying to use the right port as the MAC address is printed on&lt;/P&gt;&lt;P&gt;the board socket, and have checked that this is what I am attempting to use from u-boot/Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In u-boot have set environment so that&amp;nbsp;&lt;A href="mailto:FM1@TGEC3"&gt;FM1@TGEC3&lt;/A&gt;&amp;nbsp;is the default ethernet device, as sen from this u-boot&lt;/P&gt;&lt;P&gt;startup snippet:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Net: Fman1: Uploading microcode version 106.4.18&lt;BR /&gt;FM1@DTSEC3, FM1@DTSEC4, FM1@TGEC1, FM1@TGEC2, FM1@TGEC3 [PRIME], FM1@TGEC4&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the user guide&amp;nbsp;&lt;A href="mailto:FM1@TGEC3"&gt;FM1@TGEC3&lt;/A&gt;&amp;nbsp;actually maps to the ETH2 labelled port, further confirmed with&lt;/P&gt;&lt;P&gt;the uboot bdinfo command that shows I am using the correct device:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ethaddr = 00:04:9F:05:34:46&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When trying to ping from uboot, I get:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ping 10.1.0.22&lt;BR /&gt;FM1@TGEC3 Waiting for PHY auto negotiation to complete................................ TIMEOUT !&lt;BR /&gt;FM1@TGEC3: No link.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ETH2 Tx/Rx lights on the panel are in a continuous alternating flash pattern.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone any idea what is wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers Steve.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jan 2018 18:56:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Network-connection-problem-with-T2080RDB-PC/m-p/765935#M2515</guid>
      <dc:creator>steveosselton</dc:creator>
      <dc:date>2018-01-04T18:56:12Z</dc:date>
    </item>
    <item>
      <title>Re: Network connection problem with T2080RDB-PC</title>
      <link>https://community.nxp.com/t5/T-Series/Network-connection-problem-with-T2080RDB-PC/m-p/765936#M2516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is a typo in the QorIQ T2080 Reference Design Board Quick Start, Table 2.&lt;/P&gt;&lt;P&gt;Corrected version is:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37134i71D21C633195547D/image-size/large?v=v2&amp;amp;px=999" title="2018-01-05_105943.jpg" alt="2018-01-05_105943.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jan 2018 04:01:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Network-connection-problem-with-T2080RDB-PC/m-p/765936#M2516</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2018-01-05T04:01:45Z</dc:date>
    </item>
    <item>
      <title>Re: Network connection problem with T2080RDB-PC</title>
      <link>https://community.nxp.com/t5/T-Series/Network-connection-problem-with-T2080RDB-PC/m-p/765937#M2517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Think is also general typo in that docs have "FM1@GTECn" whereas u-boot has "FM1@TGECn" :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In any case have tried both ETH2 and ETH2 connected directly to my PC and to a network switch. In neither case can not get device to work either from Linux or u-boot. From linux:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fm1-mac1 Link encap:Ethernet HWaddr 00:04:9F:05:34:46 &lt;BR /&gt; inet addr:10.1.7.36 Bcast:10.1.255.255 Mask:255.255.0.0&lt;BR /&gt; inet6 addr: fe80::204:9fff:fe05:3446/64 Scope:Link&lt;BR /&gt; UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1&lt;BR /&gt; RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt; TX packets:6 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt; collisions:0 txqueuelen:1000 &lt;BR /&gt; RX bytes:0 (0.0 B) TX bytes:508 (508.0 B)&lt;BR /&gt; Memory:fe4e0000-fe4e0fff&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fm1-mac2 Link encap:Ethernet HWaddr 00:04:9F:05:34:47 &lt;BR /&gt; inet addr:192.168.0.2 Bcast:192.168.255.255 Mask:255.255.0.0&lt;BR /&gt; inet6 addr: fe80::204:9fff:fe05:3447/64 Scope:Link&lt;BR /&gt; UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1&lt;BR /&gt; RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt; TX packets:29 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt; collisions:0 txqueuelen:1000 &lt;BR /&gt; RX bytes:0 (0.0 B) TX bytes:1530 (1.4 KiB)&lt;BR /&gt; Memory:fe4e2000-fe4e2fff &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both ports have alternating flash link/activity lights, which sort of looks like some sort of device error status?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jan 2018 16:28:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Network-connection-problem-with-T2080RDB-PC/m-p/765937#M2517</guid>
      <dc:creator>steveosselton</dc:creator>
      <dc:date>2018-01-08T16:28:01Z</dc:date>
    </item>
    <item>
      <title>Re: Network connection problem with T2080RDB-PC</title>
      <link>https://community.nxp.com/t5/T-Series/Network-connection-problem-with-T2080RDB-PC/m-p/765938#M2518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; &lt;SPAN style="font-size: 10.5pt; color: #666666;"&gt;In any case have tried both ETH2 and ETH2 connected directly to my PC and to a network switch.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.5pt; color: #666666;"&gt;Are ports on PC and switch 10G?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jan 2018 17:50:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Network-connection-problem-with-T2080RDB-PC/m-p/765938#M2518</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2018-01-08T17:50:42Z</dc:date>
    </item>
    <item>
      <title>Re: Network connection problem with T2080RDB-PC</title>
      <link>https://community.nxp.com/t5/T-Series/Network-connection-problem-with-T2080RDB-PC/m-p/765939#M2519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Both the ports are 1GB.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jan 2018 18:02:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Network-connection-problem-with-T2080RDB-PC/m-p/765939#M2519</guid>
      <dc:creator>steveosselton</dc:creator>
      <dc:date>2018-01-08T18:02:34Z</dc:date>
    </item>
    <item>
      <title>Re: Network connection problem with T2080RDB-PC</title>
      <link>https://community.nxp.com/t5/T-Series/Network-connection-problem-with-T2080RDB-PC/m-p/765940#M2520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is required to connect T2080 10G port to another 10G port or 1G to 1G.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jan 2018 03:09:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Network-connection-problem-with-T2080RDB-PC/m-p/765940#M2520</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2018-01-09T03:09:52Z</dc:date>
    </item>
  </channel>
</rss>