<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Series中的主题 SDK SRA source code</title>
    <link>https://community.nxp.com/t5/T-Series/SDK-SRA-source-code/m-p/751533#M2442</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear, All:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am developing the SRIO application of T2080, so I wanna refer to the SRA application code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I can not find it in SDK, where can I find it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ps:My SDK is "QorIQ Linux SDK v2.0 SOURCE", and it says:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;"10.7.16.1.2.2 SDK Installation&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;SRA is based on NXP Linux SDK. So to use SRA, make sure NXP Linux SDK is well installed."&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking forward to&amp;nbsp;your reply&amp;nbsp;and&amp;nbsp;thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Dec 2017 03:08:07 GMT</pubDate>
    <dc:creator>tapyang</dc:creator>
    <dc:date>2017-12-28T03:08:07Z</dc:date>
    <item>
      <title>SDK SRA source code</title>
      <link>https://community.nxp.com/t5/T-Series/SDK-SRA-source-code/m-p/751533#M2442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear, All:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am developing the SRIO application of T2080, so I wanna refer to the SRA application code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I can not find it in SDK, where can I find it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ps:My SDK is "QorIQ Linux SDK v2.0 SOURCE", and it says:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;"10.7.16.1.2.2 SDK Installation&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;SRA is based on NXP Linux SDK. So to use SRA, make sure NXP Linux SDK is well installed."&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking forward to&amp;nbsp;your reply&amp;nbsp;and&amp;nbsp;thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Dec 2017 03:08:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/SDK-SRA-source-code/m-p/751533#M2442</guid>
      <dc:creator>tapyang</dc:creator>
      <dc:date>2017-12-28T03:08:07Z</dc:date>
    </item>
    <item>
      <title>Re: SDK SRA source code</title>
      <link>https://community.nxp.com/t5/T-Series/SDK-SRA-source-code/m-p/751534#M2443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Look at the Chapter 9.9.16 of SDK 2.0-1703 documentation:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fsupporting-information%2FQORIQ-SDK-2.0-IC-REV0.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Dec 2017 05:14:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/SDK-SRA-source-code/m-p/751534#M2443</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2017-12-29T05:14:10Z</dc:date>
    </item>
  </channel>
</rss>