<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックIs T2080 Supported in current Linux Kernels?</title>
    <link>https://community.nxp.com/t5/T-Series/Is-T2080-Supported-in-current-Linux-Kernels/m-p/733613#M2325</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am looking to build linux-qoriq kernel 4.9 for our T2080-based custom board.&amp;nbsp; I was planning on using the Yocto recipes for t2080rdb as the base, but it appears that the 4.9 kernels do not carry &lt;STRONG&gt;corenet64_fmanv3h_smp_defconfig&lt;/STRONG&gt; any more.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I copied it from Freescale SDK 2.0, it seemed to be incompatible with the newer linux-qoriq 4.9 kernel.&amp;nbsp; The "Fman Support" in Device Drivers → Network device support → Ethernet driver support can be enabled, but "Frame Manager support" selection leads to an empty screen.&amp;nbsp;&amp;nbsp; In arch/powerpc/configs there is not any obvious t2080rdb configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a known working 4.9 kernel config for t2080rdb?&amp;nbsp; Is linux-qoriq even the right kernel variant to support T2080 and e6500 cores?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Feb 2018 18:02:12 GMT</pubDate>
    <dc:creator>vladimirboroda</dc:creator>
    <dc:date>2018-02-09T18:02:12Z</dc:date>
    <item>
      <title>Is T2080 Supported in current Linux Kernels?</title>
      <link>https://community.nxp.com/t5/T-Series/Is-T2080-Supported-in-current-Linux-Kernels/m-p/733613#M2325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am looking to build linux-qoriq kernel 4.9 for our T2080-based custom board.&amp;nbsp; I was planning on using the Yocto recipes for t2080rdb as the base, but it appears that the 4.9 kernels do not carry &lt;STRONG&gt;corenet64_fmanv3h_smp_defconfig&lt;/STRONG&gt; any more.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I copied it from Freescale SDK 2.0, it seemed to be incompatible with the newer linux-qoriq 4.9 kernel.&amp;nbsp; The "Fman Support" in Device Drivers → Network device support → Ethernet driver support can be enabled, but "Frame Manager support" selection leads to an empty screen.&amp;nbsp;&amp;nbsp; In arch/powerpc/configs there is not any obvious t2080rdb configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a known working 4.9 kernel config for t2080rdb?&amp;nbsp; Is linux-qoriq even the right kernel variant to support T2080 and e6500 cores?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Feb 2018 18:02:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Is-T2080-Supported-in-current-Linux-Kernels/m-p/733613#M2325</guid>
      <dc:creator>vladimirboroda</dc:creator>
      <dc:date>2018-02-09T18:02:12Z</dc:date>
    </item>
    <item>
      <title>Re: Is T2080 Supported in current Linux Kernels?</title>
      <link>https://community.nxp.com/t5/T-Series/Is-T2080-Supported-in-current-Linux-Kernels/m-p/733614#M2326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was able to build and run the latest mainline kernel (4.16-rc1) on the T2080. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You want to use "corenet64_smp_defconfig". Even though that file doesn't actually exist under arch/powerpc/configs, if you look in the arch/powerpc/Makefile, you'll see that the "corenet64_smp_defconfig" target pulls in a bunch of config file fragments to generate the final config file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also used the fsl/t2080rdb device tree in the mainline kernel without issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Jake Moroni&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Feb 2018 19:59:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Is-T2080-Supported-in-current-Linux-Kernels/m-p/733614#M2326</guid>
      <dc:creator>jakemoroni</dc:creator>
      <dc:date>2018-02-18T19:59:54Z</dc:date>
    </item>
    <item>
      <title>Re: Is T2080 Supported in current Linux Kernels?</title>
      <link>https://community.nxp.com/t5/T-Series/Is-T2080-Supported-in-current-Linux-Kernels/m-p/733615#M2327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Moroni,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have downloaded linux kernel (linux-fslc-4.19.x-fslc) from freescale github website, want to port in T2080RDB board similar as SDK2.0 (linux kernel4.1), please help me know the steps to follow in cross compilation and porting in T2080RDB board successfully.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have&amp;nbsp;extracted SDK2.0 kernel and toolchain&amp;nbsp; from yocto.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Amit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Nov 2018 03:07:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Is-T2080-Supported-in-current-Linux-Kernels/m-p/733615#M2327</guid>
      <dc:creator>vidyasagar</dc:creator>
      <dc:date>2018-11-16T03:07:26Z</dc:date>
    </item>
    <item>
      <title>Re: Is T2080 Supported in current Linux Kernels?</title>
      <link>https://community.nxp.com/t5/T-Series/Is-T2080-Supported-in-current-Linux-Kernels/m-p/733616#M2328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Waiting for reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Nov 2018 05:48:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Is-T2080-Supported-in-current-Linux-Kernels/m-p/733616#M2328</guid>
      <dc:creator>vidyasagar</dc:creator>
      <dc:date>2018-11-19T05:48:51Z</dc:date>
    </item>
    <item>
      <title>Re: Is T2080 Supported in current Linux Kernels?</title>
      <link>https://community.nxp.com/t5/T-Series/Is-T2080-Supported-in-current-Linux-Kernels/m-p/733617#M2329</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/ufedor"&gt;ufedor&lt;/A&gt;‌&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/khumphri"&gt;khumphri&lt;/A&gt;‌&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/Mandar"&gt;Mandar&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #212121; background-color: #ffffff; font-size: 16px;"&gt;I also encountered the same problem. When I compiled the kernel, I wanted to find a similar configuration file for T2080rdb board,So could enerybody help me.Thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jan 2019 12:32:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Is-T2080-Supported-in-current-Linux-Kernels/m-p/733617#M2329</guid>
      <dc:creator>liguofa</dc:creator>
      <dc:date>2019-01-25T12:32:56Z</dc:date>
    </item>
  </channel>
</rss>