<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックRe: Problem with IR3565B on T4240RDB board</title>
    <link>https://community.nxp.com/t5/T-Series/Problem-with-IR3565B-on-T4240RDB-board/m-p/732819#M2322</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;The &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;IR3565B Multiple Time Programming memory (MTP) is programmed in the IR3565B from the original T4240RDB board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;Use external I2C/SMBUS/PMBus programmer device for writing configuration of the IR3565B to the MTP memory. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Feb 2018 02:40:46 GMT</pubDate>
    <dc:creator>Pavel</dc:creator>
    <dc:date>2018-02-13T02:40:46Z</dc:date>
    <item>
      <title>Problem with IR3565B on T4240RDB board</title>
      <link>https://community.nxp.com/t5/T-Series/Problem-with-IR3565B-on-T4240RDB-board/m-p/732818#M2321</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see in the qoriq-tseries.pdf show the T4240RDB using IR3565BMFS01TRP to supply 1.0V and 1.5V for T4240RDB, so I bought exactly new IC IOR with partnumber IR3565BMFS01TRP, but when I solder to my custom board and original T4240RDB, in both cases, it does not work. But if I use the old IR3565B IC which is in the original T4240RDB then the power 1.0V and 1.5V is ok. My question is How to program to IR3565B?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Feb 2018 04:03:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Problem-with-IR3565B-on-T4240RDB-board/m-p/732818#M2321</guid>
      <dc:creator>tuanvutruong</dc:creator>
      <dc:date>2018-02-09T04:03:42Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with IR3565B on T4240RDB board</title>
      <link>https://community.nxp.com/t5/T-Series/Problem-with-IR3565B-on-T4240RDB-board/m-p/732819#M2322</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;The &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;IR3565B Multiple Time Programming memory (MTP) is programmed in the IR3565B from the original T4240RDB board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;Use external I2C/SMBUS/PMBus programmer device for writing configuration of the IR3565B to the MTP memory. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Feb 2018 02:40:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Problem-with-IR3565B-on-T4240RDB-board/m-p/732819#M2322</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2018-02-13T02:40:46Z</dc:date>
    </item>
  </channel>
</rss>