<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Series中的主题 T4240 endpoint problem</title>
    <link>https://community.nxp.com/t5/T-Series/T4240-endpoint-problem/m-p/732529#M2314</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a T4240 processor with PCIe1 configured as endpoint (HOST_AGT_PEX = 010).&lt;/P&gt;&lt;P&gt;The endpoint is connected to a PCIe switch. The Root Complex is a P1022.&lt;/P&gt;&lt;P&gt;I can't make any configuration accesses towards the T4240 EP, all I can see in my Lauterbach window is ????????. When I disable the controller in the DEVDISR register I read all ones.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything I need to do for the enpoint to answer configuration accesses? I have used P1022 and P4080 before and then you just have to turn the power on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Emil Viding&lt;/P&gt;&lt;P&gt;HW designer&lt;/P&gt;&lt;P&gt;Saab&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Dec 2017 06:55:29 GMT</pubDate>
    <dc:creator>emilviding</dc:creator>
    <dc:date>2017-12-19T06:55:29Z</dc:date>
    <item>
      <title>T4240 endpoint problem</title>
      <link>https://community.nxp.com/t5/T-Series/T4240-endpoint-problem/m-p/732529#M2314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a T4240 processor with PCIe1 configured as endpoint (HOST_AGT_PEX = 010).&lt;/P&gt;&lt;P&gt;The endpoint is connected to a PCIe switch. The Root Complex is a P1022.&lt;/P&gt;&lt;P&gt;I can't make any configuration accesses towards the T4240 EP, all I can see in my Lauterbach window is ????????. When I disable the controller in the DEVDISR register I read all ones.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything I need to do for the enpoint to answer configuration accesses? I have used P1022 and P4080 before and then you just have to turn the power on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Emil Viding&lt;/P&gt;&lt;P&gt;HW designer&lt;/P&gt;&lt;P&gt;Saab&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Dec 2017 06:55:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4240-endpoint-problem/m-p/732529#M2314</guid>
      <dc:creator>emilviding</dc:creator>
      <dc:date>2017-12-19T06:55:29Z</dc:date>
    </item>
    <item>
      <title>Re: T4240 endpoint problem</title>
      <link>https://community.nxp.com/t5/T-Series/T4240-endpoint-problem/m-p/732530#M2315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; Is there anything I need to do for the endpoint to answer configuration accesses?&lt;/P&gt;&lt;P&gt;Please check that CONFIG[CFG_READY] is set.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Dec 2017 09:42:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4240-endpoint-problem/m-p/732530#M2315</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2017-12-19T09:42:47Z</dc:date>
    </item>
    <item>
      <title>Re: T4240 endpoint problem</title>
      <link>https://community.nxp.com/t5/T-Series/T4240-endpoint-problem/m-p/732531#M2316</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well this is embarrassing... That solved it, thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Emil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Dec 2017 12:39:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4240-endpoint-problem/m-p/732531#M2316</guid>
      <dc:creator>emilviding</dc:creator>
      <dc:date>2017-12-19T12:39:35Z</dc:date>
    </item>
  </channel>
</rss>