<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Accessing GPIO in QorIQ u-boot in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/Accessing-GPIO-in-QorIQ-u-boot/m-p/707346#M2203</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;There is no GPIO driver in u-boot for QorIQ processors, but u-boot driver structure is relatively simple, so you can create your own GPIO driver using other GPIO drivers as reference. For example drivers please look /drivers/gpio/ folder in U-boot sources folder.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Use as example the mpc85xxx_gpio.c file.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Oct 2017 11:18:46 GMT</pubDate>
    <dc:creator>Pavel</dc:creator>
    <dc:date>2017-10-18T11:18:46Z</dc:date>
    <item>
      <title>Accessing GPIO in QorIQ u-boot</title>
      <link>https://community.nxp.com/t5/T-Series/Accessing-GPIO-in-QorIQ-u-boot/m-p/707345#M2202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To whom it may concern,&lt;/P&gt;&lt;P&gt;We're using a custom board using the T2081, derived from the T2080RDB and the T1042RDB.&lt;/P&gt;&lt;P&gt;We find ourselves needing to use a GPIO during the u-boot phase.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To that end:&lt;/P&gt;&lt;P&gt;-What do we need to include in the build?&lt;/P&gt;&lt;P&gt;-What configurations and #define are needed?&lt;/P&gt;&lt;P&gt;-What custom code do we need to generate to fill in the gaps?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help,&lt;/P&gt;&lt;P&gt;Kyle&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Oct 2017 21:02:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Accessing-GPIO-in-QorIQ-u-boot/m-p/707345#M2202</guid>
      <dc:creator>kylevonschmacht</dc:creator>
      <dc:date>2017-10-16T21:02:24Z</dc:date>
    </item>
    <item>
      <title>Re: Accessing GPIO in QorIQ u-boot</title>
      <link>https://community.nxp.com/t5/T-Series/Accessing-GPIO-in-QorIQ-u-boot/m-p/707346#M2203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;There is no GPIO driver in u-boot for QorIQ processors, but u-boot driver structure is relatively simple, so you can create your own GPIO driver using other GPIO drivers as reference. For example drivers please look /drivers/gpio/ folder in U-boot sources folder.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Use as example the mpc85xxx_gpio.c file.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Oct 2017 11:18:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Accessing-GPIO-in-QorIQ-u-boot/m-p/707346#M2203</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2017-10-18T11:18:46Z</dc:date>
    </item>
  </channel>
</rss>