<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic T2080 Routing  in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T2080-Routing/m-p/685107#M2098</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been working with the T2080RDB board and am trying to configure a bridge between two disconnected networks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After enabling the board I successfully create a bridge with the following commands:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;brctl addbr br0&lt;/P&gt;&lt;P&gt;brctl addif br0 fm1-mac10 fm1-mac3&lt;/P&gt;&lt;P&gt;ip link set fm1-mac10 up&lt;/P&gt;&lt;P&gt;ip link set fm1-mac3 up&lt;/P&gt;&lt;P&gt;ip link set br0 up&lt;/P&gt;&lt;P&gt;ip addr add 192.168.1.60/24 brd + dev br0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I now have full communication between the device connected through fm1-mac10 and fm1-mac3. I am trying to initialize this bridge un boot up automatically. I have been editing the /etc/network/interfaces file, which looks like so:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# The loopback interface&lt;BR /&gt;auto lo&lt;BR /&gt;iface lo inet loopback&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;auto br0&lt;BR /&gt;iface br0 inet static&lt;BR /&gt; address 192.168.1.60&lt;BR /&gt; netmask 255.255.255.0&lt;BR /&gt; bridge_ports fm1-mac3 fm1-mac10&lt;BR /&gt; bridge_stp off&lt;BR /&gt; bridge_fd 0&lt;BR /&gt; bridge_maxwait 0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This should, by everything ive researched online, initialize a bridge on boot up but it has not been successful thus far. I tried adding the following lines to the /etc/network/interfaces file to see if anything changed but everything remained the same on boot up:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;auto fm1-mac10&lt;BR /&gt;iface fm1-mac10 inet&amp;nbsp;manual&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;auto fm1-mac3&lt;BR /&gt;iface fm1-mac3 inet manual&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help on this matter would be much appreciated as I do not know what else to try&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Matias Lirman&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H2&gt;&lt;/H2&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Jul 2017 18:25:09 GMT</pubDate>
    <dc:creator>matiaslirman</dc:creator>
    <dc:date>2017-07-26T18:25:09Z</dc:date>
    <item>
      <title>T2080 Routing</title>
      <link>https://community.nxp.com/t5/T-Series/T2080-Routing/m-p/685107#M2098</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been working with the T2080RDB board and am trying to configure a bridge between two disconnected networks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After enabling the board I successfully create a bridge with the following commands:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;brctl addbr br0&lt;/P&gt;&lt;P&gt;brctl addif br0 fm1-mac10 fm1-mac3&lt;/P&gt;&lt;P&gt;ip link set fm1-mac10 up&lt;/P&gt;&lt;P&gt;ip link set fm1-mac3 up&lt;/P&gt;&lt;P&gt;ip link set br0 up&lt;/P&gt;&lt;P&gt;ip addr add 192.168.1.60/24 brd + dev br0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I now have full communication between the device connected through fm1-mac10 and fm1-mac3. I am trying to initialize this bridge un boot up automatically. I have been editing the /etc/network/interfaces file, which looks like so:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# The loopback interface&lt;BR /&gt;auto lo&lt;BR /&gt;iface lo inet loopback&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;auto br0&lt;BR /&gt;iface br0 inet static&lt;BR /&gt; address 192.168.1.60&lt;BR /&gt; netmask 255.255.255.0&lt;BR /&gt; bridge_ports fm1-mac3 fm1-mac10&lt;BR /&gt; bridge_stp off&lt;BR /&gt; bridge_fd 0&lt;BR /&gt; bridge_maxwait 0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This should, by everything ive researched online, initialize a bridge on boot up but it has not been successful thus far. I tried adding the following lines to the /etc/network/interfaces file to see if anything changed but everything remained the same on boot up:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;auto fm1-mac10&lt;BR /&gt;iface fm1-mac10 inet&amp;nbsp;manual&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;auto fm1-mac3&lt;BR /&gt;iface fm1-mac3 inet manual&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help on this matter would be much appreciated as I do not know what else to try&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Matias Lirman&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H2&gt;&lt;/H2&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jul 2017 18:25:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2080-Routing/m-p/685107#M2098</guid>
      <dc:creator>matiaslirman</dc:creator>
      <dc:date>2017-07-26T18:25:09Z</dc:date>
    </item>
    <item>
      <title>Re: T2080 Routing</title>
      <link>https://community.nxp.com/t5/T-Series/T2080-Routing/m-p/685108#M2099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="300960" data-username="matiaslirman" href="https://community.nxp.com/people/matiaslirman"&gt;Matias Lirman&lt;/A&gt;,&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;Please refer to the following content of /etc/network/interfaces.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;# The loopback network interface&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;auto lo br0&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;iface lo inet loopback&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;# Set up interfaces manually&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;iface &lt;SPAN style="font-size: 11.0pt;"&gt;fm1-mac3&lt;/SPAN&gt; inet manual&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;iface &lt;SPAN style="font-size: 11.0pt;"&gt;fm1-mac10&lt;/SPAN&gt; inet manual&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;# Bridge setup&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;iface br0 inet static&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; bridge_ports &lt;SPAN style="font-size: 11.0pt;"&gt;fm1-mac3 fm1-mac10&lt;/SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; address &lt;SPAN style="font-size: 11.0pt;"&gt;192.168.1.60&lt;/SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; broadcast 192.168.1.255&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; netmask 255.255.255.0&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; gateway 192.168.1.1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please rebuild package&amp;nbsp;init-ifupdown into rootfs filesystem.&lt;/P&gt;&lt;P&gt;$bitbake init-ifupdown -c cleansstate&lt;/P&gt;&lt;P&gt;$bitbake init-ifupdown -c patch&lt;/P&gt;&lt;P&gt;Go the folder build_t2080rdb/tmp/work/ppce6500-fsl-linux/init-ifupdown/1.0-r7/interfaces, please modify the file interfaces as mentioned above.&lt;/P&gt;&lt;P&gt;$bitbake init-ifupdown&lt;/P&gt;&lt;P&gt;$bitbake fsl-image-core&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 20 Aug 2017 14:16:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2080-Routing/m-p/685108#M2099</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2017-08-20T14:16:15Z</dc:date>
    </item>
  </channel>
</rss>