<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Series中的主题 Re: Maintaining persistent data through a reset using T1042</title>
    <link>https://community.nxp.com/t5/T-Series/Maintaining-persistent-data-through-a-reset-using-T1042/m-p/675660#M2051</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, the CPC ram configured as SRAM may retain data after non-power on reset, however our design team said they can not confirm this is done intentionally, this functionality is not tested and can not be guarantied by NXP. The same is applicable to SPRGs.&lt;/P&gt;&lt;P&gt;The recommended way to retain data is to use external memory, for example DDR is self-refresh mode, or some nonvolatile memory.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Jun 2017 06:43:41 GMT</pubDate>
    <dc:creator>alexander_yakov</dc:creator>
    <dc:date>2017-06-14T06:43:41Z</dc:date>
    <item>
      <title>Maintaining persistent data through a reset using T1042</title>
      <link>https://community.nxp.com/t5/T-Series/Maintaining-persistent-data-through-a-reset-using-T1042/m-p/675659#M2050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Is there a method to maintain data through a reset&amp;nbsp;(non-power on) using the e5500's internal registers or T1042's peripherals?&amp;nbsp; We are aware of configuring DDR for self-refresh mode&amp;nbsp;for this.&amp;nbsp; Can the CPC be configured as SRAM and used to store data that persists through a non-power on reset?&amp;nbsp; Can the SPRG* registers be used?&amp;nbsp; Are there any other solutions?&amp;nbsp; In other NXP processors (MPC5566), the SPRG* registers were&amp;nbsp;unchanged during a reset, but undefined during a power on condition.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jun 2017 21:56:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Maintaining-persistent-data-through-a-reset-using-T1042/m-p/675659#M2050</guid>
      <dc:creator>kurtehrhardt</dc:creator>
      <dc:date>2017-06-05T21:56:33Z</dc:date>
    </item>
    <item>
      <title>Re: Maintaining persistent data through a reset using T1042</title>
      <link>https://community.nxp.com/t5/T-Series/Maintaining-persistent-data-through-a-reset-using-T1042/m-p/675660#M2051</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, the CPC ram configured as SRAM may retain data after non-power on reset, however our design team said they can not confirm this is done intentionally, this functionality is not tested and can not be guarantied by NXP. The same is applicable to SPRGs.&lt;/P&gt;&lt;P&gt;The recommended way to retain data is to use external memory, for example DDR is self-refresh mode, or some nonvolatile memory.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jun 2017 06:43:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Maintaining-persistent-data-through-a-reset-using-T1042/m-p/675660#M2051</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2017-06-14T06:43:41Z</dc:date>
    </item>
  </channel>
</rss>