<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックRe: Why only 2GB of RAM is mapped by UBOOT in T2080 RDB when the other 2 GB is mapped</title>
    <link>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417332#M202</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;U-Boot is 32-bit and thus can only address 2 GiB of RAM (with the other half of the address space reserved for I/O).&amp;nbsp; This does not affect your ability to address all of RAM once you've booted an OS.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Sep 2015 01:45:15 GMT</pubDate>
    <dc:creator>scottwood</dc:creator>
    <dc:date>2015-09-02T01:45:15Z</dc:date>
    <item>
      <title>Why only 2GB of RAM is mapped by UBOOT in T2080 RDB when the other 2 GB is mapped</title>
      <link>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417331#M201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in sdk 1.8 I can see that only 2GB of RAM is mapped by the UBOOT , what is the reason behind it ?&lt;/P&gt;&lt;P&gt;if I MAP 4 GB what problems I will face..?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;&lt;P&gt;Manish Raturi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Sep 2015 18:22:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417331#M201</guid>
      <dc:creator>manishraturi</dc:creator>
      <dc:date>2015-09-01T18:22:38Z</dc:date>
    </item>
    <item>
      <title>Re: Why only 2GB of RAM is mapped by UBOOT in T2080 RDB when the other 2 GB is mapped</title>
      <link>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417332#M202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;U-Boot is 32-bit and thus can only address 2 GiB of RAM (with the other half of the address space reserved for I/O).&amp;nbsp; This does not affect your ability to address all of RAM once you've booted an OS.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2015 01:45:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417332#M202</guid>
      <dc:creator>scottwood</dc:creator>
      <dc:date>2015-09-02T01:45:15Z</dc:date>
    </item>
    <item>
      <title>Re: Why only 2GB of RAM is mapped by UBOOT in T2080 RDB when the other 2 GB is mapped</title>
      <link>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417333#M203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Scott,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply. Is it true that UBOOT is 32 bit because I find some documentation which says that UBOOT can be build for 36-bit as well. Please correct me on this. Also my bdinfo gives me the following result:&lt;/P&gt;&lt;P&gt;=&amp;gt; bdinfo&lt;/P&gt;&lt;P&gt;memstart&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0x00000000&lt;/P&gt;&lt;P&gt;memsize&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0x100000000&lt;/P&gt;&lt;P&gt;flashstart&amp;nbsp; = 0xE8000000&lt;/P&gt;&lt;P&gt;flashsize&amp;nbsp;&amp;nbsp; = 0x08000000&lt;/P&gt;&lt;P&gt;flashoffset = 0x00000000&lt;/P&gt;&lt;P&gt;sramstart&amp;nbsp;&amp;nbsp; = 0x00000000&lt;/P&gt;&lt;P&gt;sramsize&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0x00000000&lt;/P&gt;&lt;P&gt;immr_base&amp;nbsp;&amp;nbsp; = 0xFE000000&lt;/P&gt;&lt;P&gt;bootflags&amp;nbsp;&amp;nbsp; = 0x00000000&lt;/P&gt;&lt;P&gt;intfreq&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 1533.180 MHz&lt;/P&gt;&lt;P&gt;busfreq&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 599.940 MHz&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;addressing&amp;nbsp; = 36-bit&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;ethaddr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 00:04:9F:03:47:D4&lt;/P&gt;&lt;P&gt;IP addr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 192.168.0.3&lt;/P&gt;&lt;P&gt;baudrate&amp;nbsp;&amp;nbsp;&amp;nbsp; = 115200 bps&lt;/P&gt;&lt;P&gt;relocaddr&amp;nbsp;&amp;nbsp; = 0x7FEF0000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where I can see the addressing used is 36-bit. Why it is so when UBOOT is 32 bit..?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So mapping 4GB to kernel what all things I need to change..?&lt;/P&gt;&lt;P&gt;One thing which I am thinking is to recreate the TLB entry for DDR again in the kernel where EPN value will be 0x0000_0000 and the RPN will be 0x0_0000_0000 is my understanding correct..? What else is required we need to do inside the kernel?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;&lt;P&gt;Manish Raturi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2015 05:52:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417333#M203</guid>
      <dc:creator>manishraturi</dc:creator>
      <dc:date>2015-09-02T05:52:58Z</dc:date>
    </item>
    <item>
      <title>Re: Why only 2GB of RAM is mapped by UBOOT in T2080 RDB when the other 2 GB is mapped</title>
      <link>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417334#M204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I believe there were two main reasons for 2GB memory size. First is a historical one: this really comes from 32-bit address times. Second: 2GB memory is enough for uboot. I also believe that it will not create a problem for uboot if you map 4GB of memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your follow-up questions are not so clear, you use a term "kernel". It looks like you already ask about an OS, not uboot? Uboot will pass correct memory size to the OS (even if 2GB were initially mapped), e.g. 4GB if such a DIMM is detected on the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2015 11:35:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417334#M204</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2015-09-02T11:35:44Z</dc:date>
    </item>
    <item>
      <title>Re: Why only 2GB of RAM is mapped by UBOOT in T2080 RDB when the other 2 GB is mapped</title>
      <link>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417335#M205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bulat,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply , and sorry for my terminology , I mean OS when I say kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So you are saying if we map 2GB out of 4GB of DDR DIMM module in UBOOT and if we load the OS then OS will automatically know the 4 GB memory on board and we need not to change the memory map for the OS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My understanding is this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If we are only mapping 2GB of RAM to UBOOT and using the next 2 GB to map the other peripherals. Then when we transition from UBOOT to the OS then we need to establish different memory map in OS(different from what we have in UBOOT). Now here 4GB of the address will be taken by the DDR itself. Is it not TRUE..?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am new to UBOOT and T2080 also I am&amp;nbsp; first time making the memory map for the system having 4GB of DDR and other peripherals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;&lt;P&gt;Manish Raturi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2015 11:54:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417335#M205</guid>
      <dc:creator>manishraturi</dc:creator>
      <dc:date>2015-09-02T11:54:46Z</dc:date>
    </item>
    <item>
      <title>Re: Why only 2GB of RAM is mapped by UBOOT in T2080 RDB when the other 2 GB is mapped</title>
      <link>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417336#M206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, in our case the OS will know actual memory size, e.g. 4GB, and will set up MMU/TLB in accordance with this size. Note that uboot sets correct memory size in the DDR controller and Local Access Windows, 2GB size is restricted in the MMU only.&lt;/P&gt;&lt;P&gt;I would add that statement "mapping 2GB of RAM to UBOOT and using the next 2 GB to map the other peripherals" is not fully correct in case of the T2080. As you noticed, uboot uses 36-bit addressing, and all "other peripheral" is mapped outside of lowest 4GB memory space.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2015 12:55:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417336#M206</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2015-09-02T12:55:57Z</dc:date>
    </item>
    <item>
      <title>Re: Why only 2GB of RAM is mapped by UBOOT in T2080 RDB when the other 2 GB is mapped</title>
      <link>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417337#M207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I said that U-Boot is 32-bit, I was referring to the size of an effective (virtual) address.&amp;nbsp; "36-bit addressing" refers to the size of a physical address.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2015 16:57:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417337#M207</guid>
      <dc:creator>scottwood</dc:creator>
      <dc:date>2015-09-02T16:57:02Z</dc:date>
    </item>
    <item>
      <title>Re: Why only 2GB of RAM is mapped by UBOOT in T2080 RDB when the other 2 GB is mapped</title>
      <link>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417338#M208</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it will create a problem if you map 4 GiB -- you won't have any virtual address space left for I/O.&amp;nbsp; Yes, it is fully correct for T2080.&amp;nbsp; "Outside of lowest 4GB memory space" exists only for physical addresses, since U-Boot uses 32-bit virtual addresses.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2015 17:00:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417338#M208</guid>
      <dc:creator>scottwood</dc:creator>
      <dc:date>2015-09-02T17:00:32Z</dc:date>
    </item>
    <item>
      <title>Re: Why only 2GB of RAM is mapped by UBOOT in T2080 RDB when the other 2 GB is mapped</title>
      <link>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417339#M209</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bulat,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am summarizing my understanding in the below mail, please let me know if it is correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are making a new card using T2080 and&amp;nbsp; we have purchased the T2080 RDB board for doing some hands on. Our board will have some different interfaces with respect to reference board(T2080RDB).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So with your suggestions I have prepared a memory map for our system as shown below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;1) CS0&amp;nbsp; -&amp;gt; Boot Flash &lt;/TD&gt;&lt;TD&gt;-&amp;gt; F_E800_0000 - F_F7FF_FFFF -&amp;gt; 256 MB&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;2) CS1&amp;nbsp; -&amp;gt; Control FPGA 1 -&amp;gt; F_F800_0000 - F_F80F_FFFF -&amp;gt; 1 MB&lt;/P&gt;&lt;P&gt;3) CS2&amp;nbsp; -&amp;gt; Control Fpga 2 -&amp;gt; F_F810_0000 - F_F81F_FFFF -&amp;gt; 1 MB&lt;/P&gt;&lt;P&gt;4) CS3&amp;nbsp; -&amp;gt; Control Fpga 3 -&amp;gt; F_F820_0000 - F_F82F_FFFF -&amp;gt; 1 MB&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;5) CS4&amp;nbsp; -&amp;gt; Framer 1&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;-&amp;gt; F_F830_0000 - F_F83F_FFFF -&amp;gt; 1 MB&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;6) CS5&amp;nbsp; -&amp;gt; Framer 2&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;-&amp;gt; F_F840_0000 - F_F84F_FFFF -&amp;gt; 1 MB&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;7) CS6&amp;nbsp; -&amp;gt; spare to move boot flash when secure boot comes into picture&lt;/P&gt;&lt;P&gt;8) CS7&amp;nbsp; -&amp;gt; spare&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;9) n/a&amp;nbsp; -&amp;gt; DDR 3&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;-&amp;gt; 0_0000_0000&amp;nbsp; - 0_ffff_ffff -&amp;gt; 4 GiB&amp;nbsp; /*In boot loader (UBOOT) I will map 2 GiB only*/&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;10)n/a&amp;nbsp; -&amp;gt; CCSBAR&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;-&amp;gt; F_FE00_0000&amp;nbsp; - F_FEFF_FFFF -&amp;gt; 16 MB&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;11)n/a&amp;nbsp; -&amp;gt; PCIe1 MEM &lt;/TD&gt;&lt;TD&gt;-&amp;gt; C_0000_0000&amp;nbsp; - C_1FFF_FFFF -&amp;gt; 512 MB&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;12)n/a&amp;nbsp; -&amp;gt; PCIe2 MEM &lt;/TD&gt;&lt;TD&gt;-&amp;gt; C_2000_0000&amp;nbsp; - C_2FFF_FFFF -&amp;gt; 256 MB&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;13)n/a&amp;nbsp; -&amp;gt; PCIe 1 I/O&lt;/TD&gt;&lt;TD&gt;-&amp;gt; F_F850_0000&amp;nbsp; - F_F85F_FFFF -&amp;gt; 1 MB&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;14)n/a&amp;nbsp; -&amp;gt; PCIe 2 I/O&lt;/TD&gt;&lt;TD&gt;-&amp;gt; F_F860_0000&amp;nbsp; - F_F86F_FFFF -&amp;gt; 1 MB&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I can retain this memory map in OS. But as I need to access 4 GiB of space in kernel I will need to recreate a TLB entry for 4 GiB space.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Any other thing which I need to take care ?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also let suppose If I want to address my control FPGA 1 register which is map at this location (F_F800_0000 - F_F80F_FFFF) from kernel I can use this address F800_0000(effective address) instead of F_F800_0000(physical address) for accessing the FPGA register. &lt;STRONG&gt;Please let me know if my understanding is correct.?&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Sep 2015 13:22:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417339#M209</guid>
      <dc:creator>manishraturi</dc:creator>
      <dc:date>2015-09-03T13:22:36Z</dc:date>
    </item>
    <item>
      <title>Re: Why only 2GB of RAM is mapped by UBOOT in T2080 RDB when the other 2 GB is mapped</title>
      <link>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417340#M210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1) I think thememory map is ok. Since the total memory size of all listed devices is less than 4GB (assuming DDR3 takes 2GB in uboot), you can map all devices to 32-bit virtual memory space in uboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) Question about FPGA mapping is related to OS. Typically the user can NOT set correspondence between virtual and physical addresses on kernel level.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Sep 2015 07:52:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417340#M210</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2015-09-04T07:52:57Z</dc:date>
    </item>
    <item>
      <title>Re: Why only 2GB of RAM is mapped by UBOOT in T2080 RDB when the other 2 GB is mapped</title>
      <link>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417341#M211</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Manish,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Did you ever get to the point where the OS/Kernel/Linux saw 4G?&amp;nbsp; If so, what are the steps/configuration that you needed to do to get this to work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Dec 2018 22:37:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Why-only-2GB-of-RAM-is-mapped-by-UBOOT-in-T2080-RDB-when-the/m-p/417341#M211</guid>
      <dc:creator>evaneimer</dc:creator>
      <dc:date>2018-12-06T22:37:57Z</dc:date>
    </item>
  </channel>
</rss>