<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックRe: QCVS ACE</title>
    <link>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656114#M1919</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; Is this a failure from the discrete RAM's side or from the T4240's side?&lt;/P&gt;&lt;P&gt;There are two possible root causes of ACE bit set:&lt;BR /&gt;- Register setting is not optimized&lt;BR /&gt;- There is a HW issue&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; Who actually does the automatic-calibration?&lt;/P&gt;&lt;P&gt;DDR controller&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; Is D_INIT not being cleared BECAUSE of the ACE&lt;/P&gt;&lt;P&gt;Yes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is recommended to doublecheck:&lt;BR /&gt;a) DDR connection referring the AN3940 - Hardware and Layout Design Considerations for DDR3 SDRAM&lt;BR /&gt;b) DDR controller settings referring the AN4039 - PowerQUICC and QorIQ DDR3 settings&lt;BR /&gt;Validate the settings using the DDR Validation Tool:&lt;BR /&gt;&lt;A class="link-titled" href="http://www.nxp.com/assets/documents/data/en/user-guides/QCVS_DDR_User_Guide.pdf" title="http://www.nxp.com/assets/documents/data/en/user-guides/QCVS_DDR_User_Guide.pdf"&gt;http://www.nxp.com/assets/documents/data/en/user-guides/QCVS_DDR_User_Guide.pdf&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;c) DDR powering and noise level amplitude at the AVDD_DDR&lt;BR /&gt;d) DDR MCK frequency&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Mar 2017 02:37:45 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2017-03-16T02:37:45Z</dc:date>
    <item>
      <title>QCVS ACE</title>
      <link>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656113#M1918</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm attempting to perform board check-out on a custom board. I have the processor in a good state (it has a valid RCW) and now I'm attempting to check out RAM using the QCVS and, afterwards, push the configuration into a TCL script to initialize the processor. When I try to run the QCVS DDR Validation tool's Validation Stage, it fails on "&lt;STRONG&gt;Write-Read-Compare Run 1&lt;/STRONG&gt;" and gives the reason as: "&lt;STRONG&gt;Error configuring the target! - DDR initialization failed: D_INIT was not cleared by hardware!&lt;/STRONG&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Write-Read-Compare Run 2 then fails with the reason "ERR_DETECT register not empty, test did not run."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I look at my error capture registers, I see the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Err. capture registers:&lt;BR /&gt;0xE20, 0x00000000 0xE24, 0x00000000 0xE28, 0x00000000 0xE40, 0x00000080 &lt;BR /&gt;0xE44, 0x00000000 0xE48, 0x00000000 0xE4C, 0x00000000 0xE50, 0x00000000 &lt;BR /&gt;0xE54, 0x00000000 0xE58, 0x00010000 &amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It looks like there is an ACE being thrown. Is this a failure from the discrete RAM's side or from the T4240's side? Who actually does the automatic-calibration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is D_INIT not being cleared BECAUSE of the ACE or is the ACE being thrown because D_INIT is not cleared?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What would be causing these errors?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using discrete chips on each and every controller.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Mar 2017 23:38:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656113#M1918</guid>
      <dc:creator>jimccall</dc:creator>
      <dc:date>2017-03-15T23:38:28Z</dc:date>
    </item>
    <item>
      <title>Re: QCVS ACE</title>
      <link>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656114#M1919</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; Is this a failure from the discrete RAM's side or from the T4240's side?&lt;/P&gt;&lt;P&gt;There are two possible root causes of ACE bit set:&lt;BR /&gt;- Register setting is not optimized&lt;BR /&gt;- There is a HW issue&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; Who actually does the automatic-calibration?&lt;/P&gt;&lt;P&gt;DDR controller&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; Is D_INIT not being cleared BECAUSE of the ACE&lt;/P&gt;&lt;P&gt;Yes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is recommended to doublecheck:&lt;BR /&gt;a) DDR connection referring the AN3940 - Hardware and Layout Design Considerations for DDR3 SDRAM&lt;BR /&gt;b) DDR controller settings referring the AN4039 - PowerQUICC and QorIQ DDR3 settings&lt;BR /&gt;Validate the settings using the DDR Validation Tool:&lt;BR /&gt;&lt;A class="link-titled" href="http://www.nxp.com/assets/documents/data/en/user-guides/QCVS_DDR_User_Guide.pdf" title="http://www.nxp.com/assets/documents/data/en/user-guides/QCVS_DDR_User_Guide.pdf"&gt;http://www.nxp.com/assets/documents/data/en/user-guides/QCVS_DDR_User_Guide.pdf&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;c) DDR powering and noise level amplitude at the AVDD_DDR&lt;BR /&gt;d) DDR MCK frequency&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Mar 2017 02:37:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656114#M1919</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2017-03-16T02:37:45Z</dc:date>
    </item>
    <item>
      <title>Re: QCVS ACE</title>
      <link>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656115#M1920</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jesse, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am experiencing similar issue with aT2080based board I have developed.&lt;/P&gt;&lt;P&gt;Did you managed to solve your problem ? If yes, what was the root cause ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jun 2017 15:39:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656115#M1920</guid>
      <dc:creator>xabiven</dc:creator>
      <dc:date>2017-06-15T15:39:47Z</dc:date>
    </item>
    <item>
      <title>Re: QCVS ACE</title>
      <link>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656116#M1921</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jesse,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was wondering if you were able to figure out the issue. I am seeing a similar issue with our board based on the T1024.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;R,&lt;/P&gt;&lt;P&gt;Ram&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Aug 2017 18:36:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656116#M1921</guid>
      <dc:creator>ramkrishnan</dc:creator>
      <dc:date>2017-08-01T18:36:10Z</dc:date>
    </item>
    <item>
      <title>Re: QCVS ACE</title>
      <link>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656117#M1922</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Xabiven,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;I am face the same problem to you in a T2080 based board,i use QCVS DDRV to run it and all point response ACE ERR,have you slove it now?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Dec 2017 07:52:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656117#M1922</guid>
      <dc:creator>yixuanhao</dc:creator>
      <dc:date>2017-12-07T07:52:25Z</dc:date>
    </item>
    <item>
      <title>Re: QCVS ACE</title>
      <link>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656118#M1923</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Hello Jesse,&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;I was wondering if you were able to figure out the issue. I am seeing a similar issue with our board based on the T2080.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Dec 2017 07:57:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656118#M1923</guid>
      <dc:creator>yixuanhao</dc:creator>
      <dc:date>2017-12-07T07:57:34Z</dc:date>
    </item>
    <item>
      <title>Re: QCVS ACE</title>
      <link>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656119#M1924</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello yixuan,&lt;/P&gt;&lt;P&gt;I have solved my issue, but it was due to a PCB mistake: two control signal were inverted. So, the ACE error was justified because the DDR controller was unable to perform a correct initialization with this erroneous pinout.&lt;/P&gt;&lt;P&gt;If your hardware is correct (pinout, power supplies noise, clocks, calibration resistors, ....), the ACE error is most often due to timings errors.&lt;/P&gt;&lt;P&gt;From my own experience, the CW QCVS tool is efficient to compute operating ddr timing values.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Dec 2017 10:37:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656119#M1924</guid>
      <dc:creator>xabiven</dc:creator>
      <dc:date>2017-12-07T10:37:44Z</dc:date>
    </item>
    <item>
      <title>Re: QCVS ACE</title>
      <link>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656120#M1925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xabiven,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Thank u So much,i will check the hardware status again,mabye some wrong in hardware,becuase I have the same point with you that CW QCVS tool is&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;efficient to compute operating ddr timing values,but I configurated arguments with DDR Datasheet recommendations&lt;/SPAN&gt;&lt;SPAN&gt;&lt;SPAN style="background-color: #ffffff; color: #51626f;"&gt;&amp;nbsp;,run QCVS and&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;compute operating ALL ddr timing values,without exception,All of them is wrong(tools shows ACE ERR).&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #51626f;"&gt;&amp;nbsp; With my gratitude again for you.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Dec 2017 13:30:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656120#M1925</guid>
      <dc:creator>yixuanhao</dc:creator>
      <dc:date>2017-12-07T13:30:44Z</dc:date>
    </item>
    <item>
      <title>Re: QCVS ACE</title>
      <link>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656121#M1926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;xabiven, I'm issuing a problem quite similar to yours, could you please tell me which signals were inverted?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jan 2018 21:27:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656121#M1926</guid>
      <dc:creator>francescocaiazz</dc:creator>
      <dc:date>2018-01-16T21:27:08Z</dc:date>
    </item>
    <item>
      <title>Re: QCVS ACE</title>
      <link>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656122#M1927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Francesco,&lt;/P&gt;&lt;P&gt;This was a RAS and CAS inversion. It is not so easy to see because very similar to write, ... but so obvious when the error is located !&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 13:34:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/QCVS-ACE/m-p/656122#M1927</guid>
      <dc:creator>xabiven</dc:creator>
      <dc:date>2018-01-17T13:34:02Z</dc:date>
    </item>
  </channel>
</rss>