<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックPCIe to Nexus adapter</title>
    <link>https://community.nxp.com/t5/T-Series/PCIe-to-Nexus-adapter/m-p/638069#M1783</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are there any PCIe to Nexus connector adapters?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For advanced debugging, a Nexus / Aurora high speed debugging interface is needed. For this, some of the SerDes lanes are taken to the dedicated 70-pin connector. This is done in some boards, such as the T2080QDS-PA board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, many reference design boards&amp;nbsp;take the corresponding SerDes lanes to a PCIe connector. That is the case for the T2080RDB or the T1040RDB boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking at the schematics of the T1040RDB PCIe port and at the standard pinout of the Nexus interface, I see that almost all if not all the Nexus signals are available at the PCI-Express connector.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an adapter from the PCIe connector to the 70-pin Nexus / Aurora connector?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Apr 2017 14:35:40 GMT</pubDate>
    <dc:creator>miguelgarciacle</dc:creator>
    <dc:date>2017-04-24T14:35:40Z</dc:date>
    <item>
      <title>PCIe to Nexus adapter</title>
      <link>https://community.nxp.com/t5/T-Series/PCIe-to-Nexus-adapter/m-p/638069#M1783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are there any PCIe to Nexus connector adapters?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For advanced debugging, a Nexus / Aurora high speed debugging interface is needed. For this, some of the SerDes lanes are taken to the dedicated 70-pin connector. This is done in some boards, such as the T2080QDS-PA board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, many reference design boards&amp;nbsp;take the corresponding SerDes lanes to a PCIe connector. That is the case for the T2080RDB or the T1040RDB boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking at the schematics of the T1040RDB PCIe port and at the standard pinout of the Nexus interface, I see that almost all if not all the Nexus signals are available at the PCI-Express connector.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an adapter from the PCIe connector to the 70-pin Nexus / Aurora connector?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Apr 2017 14:35:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/PCIe-to-Nexus-adapter/m-p/638069#M1783</guid>
      <dc:creator>miguelgarciacle</dc:creator>
      <dc:date>2017-04-24T14:35:40Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe to Nexus adapter</title>
      <link>https://community.nxp.com/t5/T-Series/PCIe-to-Nexus-adapter/m-p/638070#M1784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no such adapter.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Apr 2017 15:07:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/PCIe-to-Nexus-adapter/m-p/638070#M1784</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2017-04-24T15:07:05Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe to Nexus adapter</title>
      <link>https://community.nxp.com/t5/T-Series/PCIe-to-Nexus-adapter/m-p/638071#M1785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found this question by accident and it's maybe too late for Miguel Garcia Clemente,&lt;/P&gt;&lt;P&gt;but Lauterbach provides a solution to trace over PCIe using an adapter card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Matthias&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Sep 2018 12:23:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/PCIe-to-Nexus-adapter/m-p/638071#M1785</guid>
      <dc:creator>MatthiasB</dc:creator>
      <dc:date>2018-09-28T12:23:27Z</dc:date>
    </item>
  </channel>
</rss>