<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Series中的主题 Re: T1022 Hardcoded RCW codewarrior Error</title>
    <link>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622034#M1624</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;when switch is ON, How much is voltage?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Mar 2017 13:18:09 GMT</pubDate>
    <dc:creator>mohsenhaghighat</dc:creator>
    <dc:date>2017-03-08T13:18:09Z</dc:date>
    <item>
      <title>T1022 Hardcoded RCW codewarrior Error</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622030#M1620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we design a custom board with T1022 processor and the flash is blank. So we use hardcoded RCW. we connect codewarrior TAP to jtag and try to connecting to CPU.&lt;/P&gt;&lt;P&gt;But it make a error :&lt;/P&gt;&lt;P&gt;"Error: Connect Failed.&lt;BR /&gt;Failed to correctly configure the JTAG chain(CCSProtocolPlugin)&lt;BR /&gt;Error: Connect Failed."&lt;/P&gt;&lt;P&gt;The switch setting for RCW_SRC is (010011110) , where 0 means ON.&lt;/P&gt;&lt;P&gt;what can I do about it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Mar 2017 12:14:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622030#M1620</guid>
      <dc:creator>mohsenhaghighat</dc:creator>
      <dc:date>2017-03-06T12:14:01Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 Hardcoded RCW codewarrior Error</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622031#M1621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; where 0 means ON.&lt;/P&gt;&lt;P&gt;Please provide corresponding measured levels of the RCW_SRC signals.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Mar 2017 13:07:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622031#M1621</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2017-03-06T13:07:05Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 Hardcoded RCW codewarrior Error</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622032#M1622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I measure the voltage of RCW_SRC_SIGNALs. when switch is on the voltage is 0 volt and when switch is off the is 0.7 volt.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Mar 2017 07:07:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622032#M1622</guid>
      <dc:creator>mohsenhaghighat</dc:creator>
      <dc:date>2017-03-08T07:07:15Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 Hardcoded RCW codewarrior Error</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622033#M1623</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; when switch is on the voltage is 0 volt&amp;nbsp;&lt;/P&gt;&lt;P&gt;This definitely is incorrect.&lt;/P&gt;&lt;P&gt;Please check that all power supply voltages are properly applied.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Mar 2017 08:59:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622033#M1623</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2017-03-08T08:59:23Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 Hardcoded RCW codewarrior Error</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622034#M1624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;when switch is ON, How much is voltage?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Mar 2017 13:18:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622034#M1624</guid>
      <dc:creator>mohsenhaghighat</dc:creator>
      <dc:date>2017-03-08T13:18:09Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 Hardcoded RCW codewarrior Error</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622035#M1625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The cfg_rcw_src signals have internal pull-up resistors - refer to the processor's Data Sheet, Table 1. Pinout list by bus:&lt;/P&gt;&lt;P&gt;"4. This pin is a reset configuration pin. It has a weak (~20 kΩ) internal pull-up P-FET that is enabled only when the processor is in its reset state."&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Mar 2017 17:41:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622035#M1625</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2017-03-08T17:41:36Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 Hardcoded RCW codewarrior Error</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622036#M1626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have similar problems. We designed a board with LS1020A and added pull downs, assuming pull-ups are inside the uP chip. We have a problem with IFC_AD10 when we are booting from SD card. In this case the signal should be high, but we measured 1.2 V, which looks like high, but with 1.8 V logic. Our IFC is designed with 3.3 V logic, which probably qualifies the voltage as low. The solution was to add a 4k7 pull-up.&lt;BR /&gt;Does anyone else have such a problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We use the MIC826 for a reset, which has a 200 ms period with PORESET- low.&lt;BR /&gt;I found the configuration should reside on the IFC bus for 4 clocks after PORESET- goes high.&lt;BR /&gt;This seems to be ok.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Mar 2017 23:33:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622036#M1626</guid>
      <dc:creator>dusanferbas</dc:creator>
      <dc:date>2017-03-08T23:33:17Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 Hardcoded RCW codewarrior Error</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622037#M1627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Fedor and Dusan&lt;/P&gt;&lt;P&gt;I add pull up resistors for RCW source near the switch. when siwtch is On the level of voltage is 0.2 Volt and when Switch is off the level of voltage is 1.6 Volt. In this state , some times after reset the PORESET, The HRESET signals still be low(0 volt) and some times it is be high (1.8 volt). when I connect with JTAG when RCW source set to hardcoded, I see two error&lt;/P&gt;&lt;P&gt;1 " Error measuring IR length"&amp;nbsp;&lt;/P&gt;&lt;P&gt;2 "&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Failed to correctly configure the JTAG chain&lt;/SPAN&gt;"&lt;/P&gt;&lt;P&gt;what can I do for this error?&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Mar 2017 06:33:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622037#M1627</guid>
      <dc:creator>mohsenhaghighat</dc:creator>
      <dc:date>2017-03-09T06:33:15Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 Hardcoded RCW codewarrior Error</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622038#M1628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; I add pull up resistors for RCW source near the switch.&lt;/P&gt;&lt;P&gt;This is incorrect.&lt;/P&gt;&lt;P&gt;It is required to determine why internal pull-up P-FETs do not work properly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Mar 2017 06:41:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622038#M1628</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2017-03-09T06:41:08Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 Hardcoded RCW codewarrior Error</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622039#M1629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do these pull-up P-FETs working with Vcore voltage or OVDd&amp;nbsp;voltage?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Mar 2017 07:32:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622039#M1629</guid>
      <dc:creator>mohsenhaghighat</dc:creator>
      <dc:date>2017-03-09T07:32:38Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 Hardcoded RCW codewarrior Error</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622040#M1630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With OVDD supply voltage.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Mar 2017 07:38:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622040#M1630</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2017-03-09T07:38:34Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 Hardcoded RCW codewarrior Error</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622041#M1631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I make a mistake when I meaure the RCW source voltage level. I do not reset the board when I measure these.&lt;/P&gt;&lt;P&gt;when board is not reset (HRESET is high) the level voltage of RCW_src is 0 volt (On) and 0.6 volt (off).&lt;/P&gt;&lt;P&gt;But when I reset the board with (PORESET), the voltage level of RCW_src is 0.2 volt(On) and 1.7 volt(off).&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I delete the pull up resistor near the RCW_src. Still the board is not working&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Mar 2017 11:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Hardcoded-RCW-codewarrior-Error/m-p/622041#M1631</guid>
      <dc:creator>mohsenhaghighat</dc:creator>
      <dc:date>2017-03-09T11:27:03Z</dc:date>
    </item>
  </channel>
</rss>