<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic T1040D4RDB-PA - Aurora interface? in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T1040D4RDB-PA-Aurora-interface/m-p/618953#M1586</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the reference design board for the T1040: T1040D4RDB-PA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use the Aurora debugging interface. I see that this board has not the dedicated 70-pin connector. Is there a way to configure the SerDes to direct Aurora to some high-speed interface and then use some adapter for the standard 70-pin debugging connector?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;&lt;P&gt;Miguel Garcia&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Jan 2017 14:22:38 GMT</pubDate>
    <dc:creator>miguelgarciacle</dc:creator>
    <dc:date>2017-01-16T14:22:38Z</dc:date>
    <item>
      <title>T1040D4RDB-PA - Aurora interface?</title>
      <link>https://community.nxp.com/t5/T-Series/T1040D4RDB-PA-Aurora-interface/m-p/618953#M1586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the reference design board for the T1040: T1040D4RDB-PA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use the Aurora debugging interface. I see that this board has not the dedicated 70-pin connector. Is there a way to configure the SerDes to direct Aurora to some high-speed interface and then use some adapter for the standard 70-pin debugging connector?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;&lt;P&gt;Miguel Garcia&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jan 2017 14:22:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1040D4RDB-PA-Aurora-interface/m-p/618953#M1586</guid>
      <dc:creator>miguelgarciacle</dc:creator>
      <dc:date>2017-01-16T14:22:38Z</dc:date>
    </item>
    <item>
      <title>Re: T1040D4RDB-PA - Aurora interface?</title>
      <link>https://community.nxp.com/t5/T-Series/T1040D4RDB-PA-Aurora-interface/m-p/618954#M1587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I believe that from hardware point of view it is possible to implement an adapter to be installed into PCIe x4 slot J18 and using the PCIe lane 0 as Aurora. Nevertheless it should be considered that only one SerDes protocol configures the Aurora lane and this protocol is not supported by the T1040 SDK.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jan 2017 03:12:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1040D4RDB-PA-Aurora-interface/m-p/618954#M1587</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2017-01-17T03:12:00Z</dc:date>
    </item>
  </channel>
</rss>