<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックFMAN µCode for T2081</title>
    <link>https://community.nxp.com/t5/T-Series/FMAN-%C2%B5Code-for-T2081/m-p/613289#M1503</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;which fman µcode do I have to use for the T2081? Is "QorIQ Linux SDK v2.0 PPC64E6500 IMAGE.iso/t208&lt;STRONG&gt;0&lt;/STRONG&gt;qds-64b/fsl_fman_ucode_t208&lt;STRONG&gt;0&lt;/STRONG&gt;_r1.1_108_4_5.bin" from &lt;A href="https://nxp.flexnetoperations.com/control/frse/product?entitlementId=192156747&amp;amp;lineNum=1&amp;amp;authContactId=92998637&amp;amp;authPartyId=90908867"&gt;QorIQ Linux SDK&lt;/A&gt; correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ralf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Nov 2016 11:36:00 GMT</pubDate>
    <dc:creator>ralftruebenbach</dc:creator>
    <dc:date>2016-11-22T11:36:00Z</dc:date>
    <item>
      <title>FMAN µCode for T2081</title>
      <link>https://community.nxp.com/t5/T-Series/FMAN-%C2%B5Code-for-T2081/m-p/613289#M1503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;which fman µcode do I have to use for the T2081? Is "QorIQ Linux SDK v2.0 PPC64E6500 IMAGE.iso/t208&lt;STRONG&gt;0&lt;/STRONG&gt;qds-64b/fsl_fman_ucode_t208&lt;STRONG&gt;0&lt;/STRONG&gt;_r1.1_108_4_5.bin" from &lt;A href="https://nxp.flexnetoperations.com/control/frse/product?entitlementId=192156747&amp;amp;lineNum=1&amp;amp;authContactId=92998637&amp;amp;authPartyId=90908867"&gt;QorIQ Linux SDK&lt;/A&gt; correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ralf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Nov 2016 11:36:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/FMAN-%C2%B5Code-for-T2081/m-p/613289#M1503</guid>
      <dc:creator>ralftruebenbach</dc:creator>
      <dc:date>2016-11-22T11:36:00Z</dc:date>
    </item>
    <item>
      <title>Re: FMAN µCode for T2081</title>
      <link>https://community.nxp.com/t5/T-Series/FMAN-%C2%B5Code-for-T2081/m-p/613290#M1504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;The &lt;STRONG&gt;T2080&lt;/STRONG&gt; and &lt;STRONG&gt;T2081&lt;/STRONG&gt; has the same FMAN, so customer can use the ucode for both devices. There are two T2080 microcodes – _106_ and _108_. You can look for its features in&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;A href="http://git.freescale.com/git/cgit.cgi/ppc/sdk/fm-ucode.git/tree/readme?id=fsl-sdk-v2.0"&gt;http://git.freescale.com/git/cgit.cgi/ppc/sdk/fm-ucode.git/tree/readme?id=fsl-sdk-v2.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Nov 2016 05:37:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/FMAN-%C2%B5Code-for-T2081/m-p/613290#M1504</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2016-11-24T05:37:55Z</dc:date>
    </item>
  </channel>
</rss>