<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using QorIQ SDK 2.0 to build non-Linux executables in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/Using-QorIQ-SDK-2-0-to-build-non-Linux-executables/m-p/610368#M1472</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can the &lt;SPAN&gt;QorIQ SDK v2.0 be used to build stand alone executables (non-Linux) for the QorIQ processors?&amp;nbsp; Plan to install the QorIQ SDK v2.0 on a Debian Linux distro and use the gcc toolchain to build executables.&amp;nbsp; Just want to use the gcc C/C++ toolchain with NXP tweaks for the T1042 instead of the vanilla PPC-eabi from gcc.gnu.org.&amp;nbsp; Thanks in advance for any info.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Oct 2016 21:16:07 GMT</pubDate>
    <dc:creator>kurtehrhardt</dc:creator>
    <dc:date>2016-10-28T21:16:07Z</dc:date>
    <item>
      <title>Using QorIQ SDK 2.0 to build non-Linux executables</title>
      <link>https://community.nxp.com/t5/T-Series/Using-QorIQ-SDK-2-0-to-build-non-Linux-executables/m-p/610368#M1472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can the &lt;SPAN&gt;QorIQ SDK v2.0 be used to build stand alone executables (non-Linux) for the QorIQ processors?&amp;nbsp; Plan to install the QorIQ SDK v2.0 on a Debian Linux distro and use the gcc toolchain to build executables.&amp;nbsp; Just want to use the gcc C/C++ toolchain with NXP tweaks for the T1042 instead of the vanilla PPC-eabi from gcc.gnu.org.&amp;nbsp; Thanks in advance for any info.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Oct 2016 21:16:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Using-QorIQ-SDK-2-0-to-build-non-Linux-executables/m-p/610368#M1472</guid>
      <dc:creator>kurtehrhardt</dc:creator>
      <dc:date>2016-10-28T21:16:07Z</dc:date>
    </item>
    <item>
      <title>Re: Using QorIQ SDK 2.0 to build non-Linux executables</title>
      <link>https://community.nxp.com/t5/T-Series/Using-QorIQ-SDK-2-0-to-build-non-Linux-executables/m-p/610369#M1473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using the SDK one can build bare metal applications like u-boot, Linux Kernel. But it is possible because they do not need C library and they implement C library functions they need. So in general the QorIQ SDK v2.0 be can used to build stand alone executables (non-Linux) for the QorIQ processors but you have to avoid using functions from the standard C/C++ library.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Nov 2016 04:43:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Using-QorIQ-SDK-2-0-to-build-non-Linux-executables/m-p/610369#M1473</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2016-11-01T04:43:32Z</dc:date>
    </item>
    <item>
      <title>Re: Using QorIQ SDK 2.0 to build non-Linux executables</title>
      <link>https://community.nxp.com/t5/T-Series/Using-QorIQ-SDK-2-0-to-build-non-Linux-executables/m-p/610370#M1474</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is exactly what I am looking for.&amp;nbsp; I have my own embedded kernel and do not use the C library functions in my application.&amp;nbsp; I can handle the C startup code as well.&amp;nbsp; Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Nov 2016 14:23:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Using-QorIQ-SDK-2-0-to-build-non-Linux-executables/m-p/610370#M1474</guid>
      <dc:creator>kurtehrhardt</dc:creator>
      <dc:date>2016-11-01T14:23:41Z</dc:date>
    </item>
  </channel>
</rss>