<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re:  T1024RDB booting from SD card in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T1024RDB-booting-from-SD-card/m-p/602085#M1373</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The issue is solved. &lt;/P&gt;&lt;P&gt;The problem was in img files on SD card.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Oct 2016 15:16:17 GMT</pubDate>
    <dc:creator>valentinmovsik</dc:creator>
    <dc:date>2016-10-12T15:16:17Z</dc:date>
    <item>
      <title>T1024RDB booting from SD card</title>
      <link>https://community.nxp.com/t5/T-Series/T1024RDB-booting-from-SD-card/m-p/602083#M1371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using T1024RDB board and trying to boot from SD Card. I've prepared SD card&amp;nbsp; based on this&amp;nbsp; document &lt;A class="link-titled" href="http://www.nxp.com/files/soft_dev_tools/doc/support_info/QORIQ-SDK-2.0-IC-REV0.zip?fasp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=zip&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.zip" title="http://www.nxp.com/files/soft_dev_tools/doc/support_info/QORIQ-SDK-2.0-IC-REV0.zip?fasp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=zip&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.zip"&gt;http://www.nxp.com/files/soft_dev_tools/doc/support_info/QORIQ-SDK-2.0-IC-REV0.zip?fasp=1&amp;amp;WT_TYPE=Supporting%20Informati…&lt;/A&gt;&amp;nbsp; and setted up env with the next values :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; printenv loadaddr&lt;BR /&gt;loadaddr=1000000&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;=&amp;gt; printenv fdtaddr&lt;BR /&gt;fdtaddr=2000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; printenv bootfile&lt;BR /&gt;bootfile=uImage&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;=&amp;gt; printenv fdtfile&lt;BR /&gt;fdtfile=uImage-t1024rdb.dtb&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; printenv bootcmd&lt;BR /&gt;bootcmd=setenv bootargs root=/dev/mmcblk0p2 rw rootdelay=5 console=$consoledev,$baudrate;mmcinfo;ext2load mmc 0:2 0x1000000 /boot/$bootfile;ext2load mmc 0:2 0x2000000 /boot/$fdtfile;bootm 0x1000000 - 0x2000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After I plugged in a SD, powered on the board and&amp;nbsp; tried to run from the card. I'm getting the next print-out :&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;BR /&gt;Device: FSL_SDHC&lt;BR /&gt;Manufacturer ID: 3&lt;BR /&gt;OEM: 5344&lt;BR /&gt;Name: SD16G&lt;BR /&gt;Tran Speed: 25000000&lt;BR /&gt;Rd Block Len: 512&lt;BR /&gt;SD version 3.0&lt;BR /&gt;High Capacity: Yes&lt;BR /&gt;Capacity: 14.8 GiB&lt;BR /&gt;Bus Width: 4-bit&lt;BR /&gt;Erase Group Size: 512 Bytes&lt;BR /&gt;5469444 bytes read in 526 ms (9.9 MiB/s)&lt;BR /&gt;31073 bytes read in 59 ms (513.7 KiB/s)&lt;BR /&gt;WARNING: adjusting available memory to 30000000&lt;BR /&gt;Wrong Image Format for bootm command&lt;BR /&gt;ERROR: can't get kernel image!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the print-out I can see that two files (uImage and uImage-t1024rdb.dtb)&amp;nbsp; were downloaded successfully&amp;nbsp; and sizes of downloaded files are equal to sizes what actually are on SD card. Looks fine ?! ... I don't know ...&lt;/P&gt;&lt;P&gt;But for some reason I'm getting the error message : &lt;STRONG&gt;Wrong Image Format for bootm command .&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Exactly the same uImage and uImage-t1024rdb.dtb files I'm running for TFTP and NFS deployments without any problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What am I doing wrong people ?!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Val&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Oct 2016 15:49:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1024RDB-booting-from-SD-card/m-p/602083#M1371</guid>
      <dc:creator>valentinmovsik</dc:creator>
      <dc:date>2016-10-03T15:49:15Z</dc:date>
    </item>
    <item>
      <title>Re:  T1024RDB booting from SD card</title>
      <link>https://community.nxp.com/t5/T-Series/T1024RDB-booting-from-SD-card/m-p/602084#M1372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Anybody ?!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Val&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Oct 2016 12:40:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1024RDB-booting-from-SD-card/m-p/602084#M1372</guid>
      <dc:creator>valentinmovsik</dc:creator>
      <dc:date>2016-10-04T12:40:17Z</dc:date>
    </item>
    <item>
      <title>Re:  T1024RDB booting from SD card</title>
      <link>https://community.nxp.com/t5/T-Series/T1024RDB-booting-from-SD-card/m-p/602085#M1373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The issue is solved. &lt;/P&gt;&lt;P&gt;The problem was in img files on SD card.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2016 15:16:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1024RDB-booting-from-SD-card/m-p/602085#M1373</guid>
      <dc:creator>valentinmovsik</dc:creator>
      <dc:date>2016-10-12T15:16:17Z</dc:date>
    </item>
  </channel>
</rss>