<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic T4240RDB new kernel in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T4240RDB-new-kernel/m-p/587749#M1316</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to use a new configuration file for the kernel that comes with the freescale variant of yocto 1.6 for a t4240rdb board. I have&amp;nbsp;performed the following steps:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. bitbake -c menuconfig virtual/kernel&lt;/P&gt;&lt;P&gt;--- this allows me to create the .config file as I want.&lt;/P&gt;&lt;P&gt;2. In &lt;STRONG&gt;meta-fsl-ppc/recipes-kernel/linux&lt;/STRONG&gt; I have created a file &lt;STRONG&gt;linux-qoriq-sdk_3.12.bbappend&lt;/STRONG&gt; which contains&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FILESEXTRAPATHS_prepend := "${THISDIR}/files:"&lt;/P&gt;&lt;P&gt;SRC_URI&amp;nbsp;+= "file://defconfig"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. the .config create at 1. has been copied to &lt;STRONG&gt;meta-fsl-ppc/recipes-kernel/linux/files&lt;/STRONG&gt; and renamed to &lt;STRONG&gt;defconfig&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;4. bitbake fsl-image-core&lt;/P&gt;&lt;P&gt;--- this builds everything. I assume that the new kernel will exactly be&amp;nbsp;based on my &lt;STRONG&gt;defconfig&lt;/STRONG&gt; file. Is this right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a result of 4&amp;nbsp;I see&amp;nbsp;that in the work directory&amp;nbsp;there is another&amp;nbsp;directory named &lt;STRONG&gt;linux-qoriq-sdk/3.12-r0&lt;/STRONG&gt;. There I can see my &lt;STRONG&gt;defconfig&lt;/STRONG&gt; file. However, when I go to &lt;STRONG&gt;linux-qoriq-sdk/3.12-r0&lt;/STRONG&gt;/&lt;STRONG&gt;image/usr/src/kernel &lt;/STRONG&gt;there I see a .config file that is different from the &lt;STRONG&gt;defconfig&lt;/STRONG&gt; file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This means that the resulting kernel is built according to that .config file. (I assume so). If so, what am I doing wrongly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bogdan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Sep 2016 11:54:30 GMT</pubDate>
    <dc:creator>bogdantanasa</dc:creator>
    <dc:date>2016-09-02T11:54:30Z</dc:date>
    <item>
      <title>T4240RDB new kernel</title>
      <link>https://community.nxp.com/t5/T-Series/T4240RDB-new-kernel/m-p/587749#M1316</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to use a new configuration file for the kernel that comes with the freescale variant of yocto 1.6 for a t4240rdb board. I have&amp;nbsp;performed the following steps:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. bitbake -c menuconfig virtual/kernel&lt;/P&gt;&lt;P&gt;--- this allows me to create the .config file as I want.&lt;/P&gt;&lt;P&gt;2. In &lt;STRONG&gt;meta-fsl-ppc/recipes-kernel/linux&lt;/STRONG&gt; I have created a file &lt;STRONG&gt;linux-qoriq-sdk_3.12.bbappend&lt;/STRONG&gt; which contains&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FILESEXTRAPATHS_prepend := "${THISDIR}/files:"&lt;/P&gt;&lt;P&gt;SRC_URI&amp;nbsp;+= "file://defconfig"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. the .config create at 1. has been copied to &lt;STRONG&gt;meta-fsl-ppc/recipes-kernel/linux/files&lt;/STRONG&gt; and renamed to &lt;STRONG&gt;defconfig&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;4. bitbake fsl-image-core&lt;/P&gt;&lt;P&gt;--- this builds everything. I assume that the new kernel will exactly be&amp;nbsp;based on my &lt;STRONG&gt;defconfig&lt;/STRONG&gt; file. Is this right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a result of 4&amp;nbsp;I see&amp;nbsp;that in the work directory&amp;nbsp;there is another&amp;nbsp;directory named &lt;STRONG&gt;linux-qoriq-sdk/3.12-r0&lt;/STRONG&gt;. There I can see my &lt;STRONG&gt;defconfig&lt;/STRONG&gt; file. However, when I go to &lt;STRONG&gt;linux-qoriq-sdk/3.12-r0&lt;/STRONG&gt;/&lt;STRONG&gt;image/usr/src/kernel &lt;/STRONG&gt;there I see a .config file that is different from the &lt;STRONG&gt;defconfig&lt;/STRONG&gt; file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This means that the resulting kernel is built according to that .config file. (I assume so). If so, what am I doing wrongly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bogdan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2016 11:54:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4240RDB-new-kernel/m-p/587749#M1316</guid>
      <dc:creator>bogdantanasa</dc:creator>
      <dc:date>2016-09-02T11:54:30Z</dc:date>
    </item>
  </channel>
</rss>