<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is secure boot possible only via NOR boot in T1024 processor? in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/Is-secure-boot-possible-only-via-NOR-boot-in-T1024-processor/m-p/581196#M1279</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;NXP SDK 2.0 supports secure boot for the T1024RDB board. See attached file.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Sep 2016 09:25:03 GMT</pubDate>
    <dc:creator>Pavel</dc:creator>
    <dc:date>2016-09-01T09:25:03Z</dc:date>
    <item>
      <title>Is secure boot possible only via NOR boot in T1024 processor?</title>
      <link>https://community.nxp.com/t5/T-Series/Is-secure-boot-possible-only-via-NOR-boot-in-T1024-processor/m-p/581195#M1278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;From QorIQ SDKv2.0 documentation, for T1 series it is mentioned only via NOR, secure boot is possible. &amp;nbsp;Please get this clear to me. &amp;nbsp;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Sep 2016 07:05:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Is-secure-boot-possible-only-via-NOR-boot-in-T1024-processor/m-p/581195#M1278</guid>
      <dc:creator>arumugamp</dc:creator>
      <dc:date>2016-09-01T07:05:38Z</dc:date>
    </item>
    <item>
      <title>Re: Is secure boot possible only via NOR boot in T1024 processor?</title>
      <link>https://community.nxp.com/t5/T-Series/Is-secure-boot-possible-only-via-NOR-boot-in-T1024-processor/m-p/581196#M1279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;NXP SDK 2.0 supports secure boot for the T1024RDB board. See attached file.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Sep 2016 09:25:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Is-secure-boot-possible-only-via-NOR-boot-in-T1024-processor/m-p/581196#M1279</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2016-09-01T09:25:03Z</dc:date>
    </item>
    <item>
      <title>Re: Is secure boot possible only via NOR boot in T1024 processor?</title>
      <link>https://community.nxp.com/t5/T-Series/Is-secure-boot-possible-only-via-NOR-boot-in-T1024-processor/m-p/581197#M1280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Pavel. &amp;nbsp;But whether the secure boot could be implemented from NAND in T1024?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Sep 2016 09:55:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Is-secure-boot-possible-only-via-NOR-boot-in-T1024-processor/m-p/581197#M1280</guid>
      <dc:creator>arumugamp</dc:creator>
      <dc:date>2016-09-01T09:55:12Z</dc:date>
    </item>
    <item>
      <title>Re: Is secure boot possible only via NOR boot in T1024 processor?</title>
      <link>https://community.nxp.com/t5/T-Series/Is-secure-boot-possible-only-via-NOR-boot-in-T1024-processor/m-p/581198#M1281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;SPAN class=""&gt;ARUMUGAM P,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;On T1024, secure boot could be implemented from NAND.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;But in SDK 2.0, no software support for T1024 NAND secure boot.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;You could modify RCW(PBI support) and u-boot source code by yourself, you could refer to P3041DS.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Sep 2016 08:23:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Is-secure-boot-possible-only-via-NOR-boot-in-T1024-processor/m-p/581198#M1281</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2016-09-08T08:23:24Z</dc:date>
    </item>
  </channel>
</rss>