<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic EndPoint MSI interrupt generation on T4240 in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/EndPoint-MSI-interrupt-generation-on-T4240/m-p/576092#M1258</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I have a T4240 QorIQ on a PCIe card, which configured as an EndPoint (EP) to the RootComplex (RC) on the host x86 platform. The x86 host is running with Linux CentOS and the T4240 is running with INTEGRITY OS (GreenHills). I'm trying to prototype the PCI communication between the x86 host/RC and the T4240 EP with MSI enabled. I'm&amp;nbsp;able to&amp;nbsp;generate MSI interrupt(s) from the x86 and service the interrupt(s) on the T4240. But I'm having trouble generating MSI interrupt(s) from the T4240 EP to 0x86 RC. Do you have any example that shows how to&amp;nbsp;generate MSI interrupt(s) on the T4240 QorIQ (as an EP)? &amp;nbsp;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Aug 2016 00:58:30 GMT</pubDate>
    <dc:creator>kennyle</dc:creator>
    <dc:date>2016-08-31T00:58:30Z</dc:date>
    <item>
      <title>EndPoint MSI interrupt generation on T4240</title>
      <link>https://community.nxp.com/t5/T-Series/EndPoint-MSI-interrupt-generation-on-T4240/m-p/576092#M1258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I have a T4240 QorIQ on a PCIe card, which configured as an EndPoint (EP) to the RootComplex (RC) on the host x86 platform. The x86 host is running with Linux CentOS and the T4240 is running with INTEGRITY OS (GreenHills). I'm trying to prototype the PCI communication between the x86 host/RC and the T4240 EP with MSI enabled. I'm&amp;nbsp;able to&amp;nbsp;generate MSI interrupt(s) from the x86 and service the interrupt(s) on the T4240. But I'm having trouble generating MSI interrupt(s) from the T4240 EP to 0x86 RC. Do you have any example that shows how to&amp;nbsp;generate MSI interrupt(s) on the T4240 QorIQ (as an EP)? &amp;nbsp;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2016 00:58:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/EndPoint-MSI-interrupt-generation-on-T4240/m-p/576092#M1258</guid>
      <dc:creator>kennyle</dc:creator>
      <dc:date>2016-08-31T00:58:30Z</dc:date>
    </item>
    <item>
      <title>Re: EndPoint MSI interrupt generation on T4240</title>
      <link>https://community.nxp.com/t5/T-Series/EndPoint-MSI-interrupt-generation-on-T4240/m-p/576093#M1259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Hardware and software EP MSI generation methods are described in the QorIQ T4240 Reference Manual, 19.6.2.1.2 Hardware MSI Generation and 19.6.2.1.3 Software MSI Generation.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We do not have an example in addition to the RM description.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2016 03:08:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/EndPoint-MSI-interrupt-generation-on-T4240/m-p/576093#M1259</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-09-02T03:08:55Z</dc:date>
    </item>
  </channel>
</rss>