<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Series中的主题 T1022 Example Secureboot RCW</title>
    <link>https://community.nxp.com/t5/T-Series/T1022-Example-Secureboot-RCW/m-p/550492#M1131</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Looking for an example RCW that someone has used to successfully boot SecureBoot on a T1022. I have one that I think should be working (Modified memory map, scratch registers being set, etc) but when I change the SB_EN bit = 1 I hit a machine check.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Jun 2016 15:16:47 GMT</pubDate>
    <dc:creator>tschutte</dc:creator>
    <dc:date>2016-06-20T15:16:47Z</dc:date>
    <item>
      <title>T1022 Example Secureboot RCW</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Example-Secureboot-RCW/m-p/550492#M1131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Looking for an example RCW that someone has used to successfully boot SecureBoot on a T1022. I have one that I think should be working (Modified memory map, scratch registers being set, etc) but when I change the SB_EN bit = 1 I hit a machine check.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jun 2016 15:16:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Example-Secureboot-RCW/m-p/550492#M1131</guid>
      <dc:creator>tschutte</dc:creator>
      <dc:date>2016-06-20T15:16:47Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 Example Secureboot RCW</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Example-Secureboot-RCW/m-p/550493#M1132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;T1022 is a proper subset of T1042. QorIQ SDK includes ready and verified secure boot RCWs&amp;nbsp; for T1042RDB and T1042RDB-PI. Unpack the package called 'rcw', inspect the source. Detailed instructions can be found here:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-891F9B61-E7D5-46C2-9BFA-69ACD7C4FCA6" title="https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-891F9B61-E7D5-46C2-9BFA-69ACD7C4FCA6"&gt;Submit Form&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-038CFEAB-F051-46F9-94E6-F57419C9557E" title="https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-038CFEAB-F051-46F9-94E6-F57419C9557E"&gt;Submit Form&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jun 2016 17:41:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Example-Secureboot-RCW/m-p/550493#M1132</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2016-06-20T17:41:48Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 Example Secureboot RCW</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Example-Secureboot-RCW/m-p/550494#M1133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not seeing a 'rcw' package anywhere in the SDK. Where can I download the package from?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jun 2016 18:49:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Example-Secureboot-RCW/m-p/550494#M1133</guid>
      <dc:creator>tschutte</dc:creator>
      <dc:date>2016-06-20T18:49:55Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 Example Secureboot RCW</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Example-Secureboot-RCW/m-p/550495#M1134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You do not have to download anything in addition to the SDK source DVD image. rcw package is part of the SDK:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ bitbake -s | grep rcw&lt;/P&gt;&lt;P&gt;rcw&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; :git-r0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Install the SDK and follow instructions at the links I posted above to unpack the package and inspect it's source.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jun 2016 09:51:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Example-Secureboot-RCW/m-p/550495#M1134</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2016-06-21T09:51:31Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 Example Secureboot RCW</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Example-Secureboot-RCW/m-p/550496#M1135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a way to get the RCW's without downloading the full SDK? Or could someone Just post the contents of the RCW?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jun 2016 14:19:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Example-Secureboot-RCW/m-p/550496#M1135</guid>
      <dc:creator>tschutte</dc:creator>
      <dc:date>2016-06-21T14:19:59Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 Example Secureboot RCW</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Example-Secureboot-RCW/m-p/550497#M1136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So I got RCW's but didnt see any for the T1042, are they not part of the 2.0 SDK?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jun 2016 19:01:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Example-Secureboot-RCW/m-p/550497#M1136</guid>
      <dc:creator>tschutte</dc:creator>
      <dc:date>2016-06-29T19:01:05Z</dc:date>
    </item>
  </channel>
</rss>