<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Series中的主题 How to reset ( having reset control) PCIe device connected device over T1040RDB PCIe slot through the processor ?</title>
    <link>https://community.nxp.com/t5/T-Series/How-to-reset-having-reset-control-PCIe-device-connected-device/m-p/545075#M1098</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I am using T1040 RDB evalution module and connected my PCIe card into it. Now In my debugging and driver application I need to reset the PCIe add on card.&amp;nbsp; According to the schematics of T1040RDB A11&amp;nbsp; pin of PCIe connector&amp;nbsp; is connected CPLD IO.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my PCIe device card, I have connected that PCIe RST line coming from the PCIe connector to the various devices in my PCIe card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do not know if there is&amp;nbsp; anyway to toggle that reset signal through the processor. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me kno this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:45:41 GMT</pubDate>
    <dc:creator>mvgohil</dc:creator>
    <dc:date>2016-06-15T19:45:41Z</dc:date>
    <item>
      <title>How to reset ( having reset control) PCIe device connected device over T1040RDB PCIe slot through the processor ?</title>
      <link>https://community.nxp.com/t5/T-Series/How-to-reset-having-reset-control-PCIe-device-connected-device/m-p/545075#M1098</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I am using T1040 RDB evalution module and connected my PCIe card into it. Now In my debugging and driver application I need to reset the PCIe add on card.&amp;nbsp; According to the schematics of T1040RDB A11&amp;nbsp; pin of PCIe connector&amp;nbsp; is connected CPLD IO.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my PCIe device card, I have connected that PCIe RST line coming from the PCIe connector to the various devices in my PCIe card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do not know if there is&amp;nbsp; anyway to toggle that reset signal through the processor. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me kno this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:45:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/How-to-reset-having-reset-control-PCIe-device-connected-device/m-p/545075#M1098</guid>
      <dc:creator>mvgohil</dc:creator>
      <dc:date>2016-06-15T19:45:41Z</dc:date>
    </item>
    <item>
      <title>Re: How to reset ( having reset control) PCIe device connected device over T1040RDB PCIe slot through the processor ?</title>
      <link>https://community.nxp.com/t5/T-Series/How-to-reset-having-reset-control-PCIe-device-connected-device/m-p/545076#M1099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is 8-bit soft reset register RSTCON2 implemented in the CPLD (offset = 11h, CPLD base address = 0xffdf0000). RSTCON2 bit 5 controls that reset signal&lt;BR /&gt; PEX_RST&lt;BR /&gt; 0: No reset occurs.&lt;BR /&gt; 1: Writing logic 1 produces PCIe x4 slot reset# signal, this bit can auto clear.&lt;/P&gt;&lt;P&gt;This description is from the QorIQ T1040 Reference Design Board User Guide, Rev. 0, 06/2015 available on the NXP site&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 11:59:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/How-to-reset-having-reset-control-PCIe-device-connected-device/m-p/545076#M1099</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2016-06-16T11:59:09Z</dc:date>
    </item>
  </channel>
</rss>