<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックDPAA1 Sample Code for Interfacing the Linux Network Stack with a DPAA Port.</title>
    <link>https://community.nxp.com/t5/T-Series/DPAA1-Sample-Code-for-Interfacing-the-Linux-Network-Stack-with-a/m-p/536659#M1085</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was wondering if there is any sample code out there to interface the Linux Interface stack with the the USDPAA port. I have an application wherein I switch mpls traffic using the offload and forwarding traffic directly using the FQID's and the buffer pointers. But I would like the IP traffic to be terminated in the Linux Network stack. I can do that on the ingress side using TUN/TAP interfaces but I have not been successful on the egress side in sending the traffic out. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you point me to some sample code for the Device tree and USDPAA samples to send out traffic towards a port that is DPAA enabled. I am running this application on the T1024 in a serdes 0x99 mode. I looked at the "Relationship to SDK Linux Ethernet Subsystem" in the QorIQ SDK 2.0 Documentation under the USDPAA section and I am interested in mode 3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Ram Krishnan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Jul 2016 15:38:18 GMT</pubDate>
    <dc:creator>ramkrishnan</dc:creator>
    <dc:date>2016-07-04T15:38:18Z</dc:date>
    <item>
      <title>DPAA1 Sample Code for Interfacing the Linux Network Stack with a DPAA Port.</title>
      <link>https://community.nxp.com/t5/T-Series/DPAA1-Sample-Code-for-Interfacing-the-Linux-Network-Stack-with-a/m-p/536659#M1085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was wondering if there is any sample code out there to interface the Linux Interface stack with the the USDPAA port. I have an application wherein I switch mpls traffic using the offload and forwarding traffic directly using the FQID's and the buffer pointers. But I would like the IP traffic to be terminated in the Linux Network stack. I can do that on the ingress side using TUN/TAP interfaces but I have not been successful on the egress side in sending the traffic out. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you point me to some sample code for the Device tree and USDPAA samples to send out traffic towards a port that is DPAA enabled. I am running this application on the T1024 in a serdes 0x99 mode. I looked at the "Relationship to SDK Linux Ethernet Subsystem" in the QorIQ SDK 2.0 Documentation under the USDPAA section and I am interested in mode 3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Ram Krishnan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jul 2016 15:38:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/DPAA1-Sample-Code-for-Interfacing-the-Linux-Network-Stack-with-a/m-p/536659#M1085</guid>
      <dc:creator>ramkrishnan</dc:creator>
      <dc:date>2016-07-04T15:38:18Z</dc:date>
    </item>
  </channel>
</rss>