<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 Accel offset computation using 6 orientations</title>
    <link>https://community.nxp.com/t5/Sensors/Accel-offset-computation-using-6-orientations/m-p/341866#M974</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to do an offset calibration of the MMA8451 using the six position test. According to AN4069, I should compute the offsets using the average of four 0g positions or the midpoint of the -1g and&amp;nbsp; 1g positions. Why not average all six readings?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 23:03:27 GMT</pubDate>
    <dc:creator>johnwayne23</dc:creator>
    <dc:date>2026-02-03T23:03:27Z</dc:date>
    <item>
      <title>Accel offset computation using 6 orientations</title>
      <link>https://community.nxp.com/t5/Sensors/Accel-offset-computation-using-6-orientations/m-p/341866#M974</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to do an offset calibration of the MMA8451 using the six position test. According to AN4069, I should compute the offsets using the average of four 0g positions or the midpoint of the -1g and&amp;nbsp; 1g positions. Why not average all six readings?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 23:03:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Accel-offset-computation-using-6-orientations/m-p/341866#M974</guid>
      <dc:creator>johnwayne23</dc:creator>
      <dc:date>2026-02-03T23:03:27Z</dc:date>
    </item>
  </channel>
</rss>