<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 Re: MPX5010DP 'losing' pressure</title>
    <link>https://community.nxp.com/t5/Sensors/MPX5010DP-losing-pressure/m-p/337110#M946</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Felipe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;For measuring standing water heights, the sensor leaks slightly over time, but if you are using the MPX5010DP CASE 867C-05, this is the package that leaks the least. Or case 867B-04. Those are the cases to utilize to minimize leakage over time instead of the SOP vertical port or SOP side port packages.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Further, the Tygon tubing should help. Several customers are using what amounts to similar product as a zip tie to secure the tubing. What we suggest is pick an ID (Inner diameter) slightly smaller than 4.775 (mm) for the port barb. Heat up the tubing slightly and slide this tubing on. Afterwards as it cools, it should be a strong seal. To secure it more, wire could be used, or very small zip ties. Note that some tubing also leaks slowly over time as air and water vapor can go through porous tubing material.&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Hope it helps.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Tomas&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;EM style="font-weight: normal; font-style: italic; font-size: 13px; font-family: Arial, sans-serif; color: #333333; text-align: left; text-indent: 0px;"&gt;&lt;SPAN style="font-weight: inherit; font-style: inherit; font-size: 11px; font-family: inherit; color: #3d3d3d;"&gt;&lt;EM style="font-weight: inherit; font-style: italic; font-size: 11px; font-family: inherit;"&gt;PS:&lt;SPAN class="Apple-converted-space" style="font-weight: inherit; font-style: inherit; font-size: 11px; font-family: inherit;"&gt;&lt;SPAN class="Apple-converted-space" style="font-weight: inherit; font-style: inherit; font-size: 11px; font-family: inherit;"&gt;&lt;SPAN class="Apple-converted-space"&gt; &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;SPAN style="font-weight: inherit; font-style: inherit; font-size: 11px; font-family: inherit; color: #3d3d3d;"&gt;If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.&lt;/SPAN&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Oct 2014 08:55:49 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2014-10-21T08:55:49Z</dc:date>
    <item>
      <title>MPX5010DP 'losing' pressure</title>
      <link>https://community.nxp.com/t5/Sensors/MPX5010DP-losing-pressure/m-p/337109#M945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello guys. I'm using a MPX5010DP sensor to measure the water tank level. I've tried to seal the tube on the sensor of many ways, but it still losing the pressure. Over the time, Vout don't stops decreasing. The connections are ok, the measurement starts ok. Can anyone help me? Tnx!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:24:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPX5010DP-losing-pressure/m-p/337109#M945</guid>
      <dc:creator>felipedias</dc:creator>
      <dc:date>2026-02-03T22:24:52Z</dc:date>
    </item>
    <item>
      <title>Re: MPX5010DP 'losing' pressure</title>
      <link>https://community.nxp.com/t5/Sensors/MPX5010DP-losing-pressure/m-p/337110#M946</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Felipe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;For measuring standing water heights, the sensor leaks slightly over time, but if you are using the MPX5010DP CASE 867C-05, this is the package that leaks the least. Or case 867B-04. Those are the cases to utilize to minimize leakage over time instead of the SOP vertical port or SOP side port packages.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Further, the Tygon tubing should help. Several customers are using what amounts to similar product as a zip tie to secure the tubing. What we suggest is pick an ID (Inner diameter) slightly smaller than 4.775 (mm) for the port barb. Heat up the tubing slightly and slide this tubing on. Afterwards as it cools, it should be a strong seal. To secure it more, wire could be used, or very small zip ties. Note that some tubing also leaks slowly over time as air and water vapor can go through porous tubing material.&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Hope it helps.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Tomas&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;&lt;EM style="font-weight: normal; font-style: italic; font-size: 13px; font-family: Arial, sans-serif; color: #333333; text-align: left; text-indent: 0px;"&gt;&lt;SPAN style="font-weight: inherit; font-style: inherit; font-size: 11px; font-family: inherit; color: #3d3d3d;"&gt;&lt;EM style="font-weight: inherit; font-style: italic; font-size: 11px; font-family: inherit;"&gt;PS:&lt;SPAN class="Apple-converted-space" style="font-weight: inherit; font-style: inherit; font-size: 11px; font-family: inherit;"&gt;&lt;SPAN class="Apple-converted-space" style="font-weight: inherit; font-style: inherit; font-size: 11px; font-family: inherit;"&gt;&lt;SPAN class="Apple-converted-space"&gt; &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;SPAN style="font-weight: inherit; font-style: inherit; font-size: 11px; font-family: inherit; color: #3d3d3d;"&gt;If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.&lt;/SPAN&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Oct 2014 08:55:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPX5010DP-losing-pressure/m-p/337110#M946</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2014-10-21T08:55:49Z</dc:date>
    </item>
    <item>
      <title>Re: MPX5010DP 'losing' pressure</title>
      <link>https://community.nxp.com/t5/Sensors/MPX5010DP-losing-pressure/m-p/337111#M947</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for answering.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well, i am using the &lt;SPAN style="color: #3d3d3d; font-family: Arial, sans-serif; background-color: #f6f6f6;"&gt;&lt;SPAN style="color: #3d3d3d; font-family: Arial, sans-serif;"&gt;867C-05 case, and tried to seal with silicon, and hot glue (each one at time, or one over the other). Zip ties was my firs try: unsuccessfully. And, using Tygon tubing too. The sensor is on the water tank, but completaly sealed (just the wire and the tubing leaves the sealed case). The inner pressure can make this difference?&lt;BR /&gt;&lt;BR /&gt; I've seen the "&lt;/SPAN&gt;&lt;SPAN style="font-size: 15px;"&gt;&lt;STRONG&gt;&lt;SPAN style="color: #6a737b; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Freescale pressure sensor directly exposed to car coolant during a month." &lt;/SPAN&gt;&lt;SPAN style="color: #8b8b8b; font-size: 12px;"&gt;Joshevelle&lt;/SPAN&gt; &lt;SPAN style="color: #8b8b8b; font-size: 12px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt; &lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN style="color: #3d3d3d; font-size: 12px; font-family: Arial, sans-serif;"&gt;post, and I didn't understand this: "&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;In this kind of applications, we would recommend to use Parker O-lube silicone grease or DMS-T46 or T51. This type of grease is used by most of our customer without problems". How could I use some oil on that? This oil is the media or something to held the measurement? &lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;I don't know what to do anymore :X &lt;BR /&gt;I was just about to produce in large scale to sell haha&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you again!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Oct 2014 12:49:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPX5010DP-losing-pressure/m-p/337111#M947</guid>
      <dc:creator>felipedias</dc:creator>
      <dc:date>2014-10-24T12:49:18Z</dc:date>
    </item>
  </channel>
</rss>