<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MMA9551 map multiple bits to the same GPIO pin in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/MMA9551-map-multiple-bits-to-the-same-GPIO-pin/m-p/336218#M938</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vlad,&lt;/P&gt;&lt;P&gt;Yes it is possible to do this, but you will need to write a small custom application to implement the logic. Then you can map the output of your custom application to a GPIO. Please see &lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN4129.pdf?fasp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;AN4129: Building Custom Applications on MMA9550L/MMA9551L&lt;/A&gt;. A sample custom application is also available for &lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN4129SW.zip?fpsp=1"&gt;download&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maureen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Nov 2014 15:13:26 GMT</pubDate>
    <dc:creator>maureen</dc:creator>
    <dc:date>2014-11-13T15:13:26Z</dc:date>
    <item>
      <title>MMA9551 map multiple bits to the same GPIO pin</title>
      <link>https://community.nxp.com/t5/Sensors/MMA9551-map-multiple-bits-to-the-same-GPIO-pin/m-p/336217#M937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there!&amp;nbsp; Is it possible to map a logical OR of multiple bits to the same GPIO pin?&amp;nbsp; I ask because in flash mode we can use 4 pins, but might need more bits mapped to GPIO.&amp;nbsp; For example, in the tilt application, mapping all three ANGFLG bits already leaves us with only one usable GPIO pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:18:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA9551-map-multiple-bits-to-the-same-GPIO-pin/m-p/336217#M937</guid>
      <dc:creator>vladdogaru</dc:creator>
      <dc:date>2026-02-03T21:18:33Z</dc:date>
    </item>
    <item>
      <title>Re: MMA9551 map multiple bits to the same GPIO pin</title>
      <link>https://community.nxp.com/t5/Sensors/MMA9551-map-multiple-bits-to-the-same-GPIO-pin/m-p/336218#M938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vlad,&lt;/P&gt;&lt;P&gt;Yes it is possible to do this, but you will need to write a small custom application to implement the logic. Then you can map the output of your custom application to a GPIO. Please see &lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN4129.pdf?fasp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;AN4129: Building Custom Applications on MMA9550L/MMA9551L&lt;/A&gt;. A sample custom application is also available for &lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN4129SW.zip?fpsp=1"&gt;download&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maureen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Nov 2014 15:13:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA9551-map-multiple-bits-to-the-same-GPIO-pin/m-p/336218#M938</guid>
      <dc:creator>maureen</dc:creator>
      <dc:date>2014-11-13T15:13:26Z</dc:date>
    </item>
  </channel>
</rss>