<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 MMA8652FC motion detection interrupt</title>
    <link>https://community.nxp.com/t5/Sensors/MMA8652FC-motion-detection-interrupt/m-p/335905#M935</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've been able to configure a MMA8652FC 3-Axis accelerometer to generate interrupts on free-fall events by playing with both FF_MT_CFG and FF_MT_THS registers. After this experience, I'd like the sensor to generate an interrupt when motion is detected. I'm thinking in detecting usual movements like taking an object from a table "in a natural way", but even when setting FF_MT_THS (detection threshold) to a minimum value the interrupt is only generated with fast movements. This is maybe why this functionality is called free-fall/motion detection...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I really use the MMA8652FC to detect slower movements in an interrupt-generation basis?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Daniel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2026 23:02:10 GMT</pubDate>
    <dc:creator>estratos</dc:creator>
    <dc:date>2026-02-03T23:02:10Z</dc:date>
    <item>
      <title>MMA8652FC motion detection interrupt</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8652FC-motion-detection-interrupt/m-p/335905#M935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've been able to configure a MMA8652FC 3-Axis accelerometer to generate interrupts on free-fall events by playing with both FF_MT_CFG and FF_MT_THS registers. After this experience, I'd like the sensor to generate an interrupt when motion is detected. I'm thinking in detecting usual movements like taking an object from a table "in a natural way", but even when setting FF_MT_THS (detection threshold) to a minimum value the interrupt is only generated with fast movements. This is maybe why this functionality is called free-fall/motion detection...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I really use the MMA8652FC to detect slower movements in an interrupt-generation basis?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Daniel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 23:02:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8652FC-motion-detection-interrupt/m-p/335905#M935</guid>
      <dc:creator>estratos</dc:creator>
      <dc:date>2026-02-03T23:02:10Z</dc:date>
    </item>
    <item>
      <title>Re: MMA8652FC motion detection interrupt</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8652FC-motion-detection-interrupt/m-p/335906#M936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I reply myself: pulse events can be used with low thresholds to detect simple movements.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Aug 2014 17:47:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8652FC-motion-detection-interrupt/m-p/335906#M936</guid>
      <dc:creator>estratos</dc:creator>
      <dc:date>2014-08-05T17:47:36Z</dc:date>
    </item>
  </channel>
</rss>