<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックUsing Arduino interface of MIMX RT1170 EVK for sensor connection</title>
    <link>https://community.nxp.com/t5/Sensors/Using-Arduino-interface-of-MIMX-RT1170-EVK-for-sensor-connection/m-p/2379921#M9102</link>
    <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I am interfacing ultrasonic sensor to MIMX RT1170 EVK board. For interfacing the sensor I need to use Arduino interface for GPIOs connection. I am not able to find the proper connections for ultrasonic sensor connection, because not getting power at the pins.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I gave supply to board using adapter (J43).&amp;nbsp;&lt;BR /&gt;I need reference for pins connection and are there any settings required for powering ON the arduino interface region?&lt;/P&gt;&lt;P&gt;Thank you.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 11 Jun 2026 07:09:30 GMT</pubDate>
    <dc:creator>SK02</dc:creator>
    <dc:date>2026-06-11T07:09:30Z</dc:date>
    <item>
      <title>Using Arduino interface of MIMX RT1170 EVK for sensor connection</title>
      <link>https://community.nxp.com/t5/Sensors/Using-Arduino-interface-of-MIMX-RT1170-EVK-for-sensor-connection/m-p/2379921#M9102</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I am interfacing ultrasonic sensor to MIMX RT1170 EVK board. For interfacing the sensor I need to use Arduino interface for GPIOs connection. I am not able to find the proper connections for ultrasonic sensor connection, because not getting power at the pins.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I gave supply to board using adapter (J43).&amp;nbsp;&lt;BR /&gt;I need reference for pins connection and are there any settings required for powering ON the arduino interface region?&lt;/P&gt;&lt;P&gt;Thank you.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jun 2026 07:09:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Using-Arduino-interface-of-MIMX-RT1170-EVK-for-sensor-connection/m-p/2379921#M9102</guid>
      <dc:creator>SK02</dc:creator>
      <dc:date>2026-06-11T07:09:30Z</dc:date>
    </item>
    <item>
      <title>Re: Using Arduino interface of MIMX RT1170 EVK for sensor connection</title>
      <link>https://community.nxp.com/t5/Sensors/Using-Arduino-interface-of-MIMX-RT1170-EVK-for-sensor-connection/m-p/2380495#M9103</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262693"&gt;@SK02&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;DIV&gt;
&lt;P&gt;regarding your issue, could you please verify the following power configuration?&lt;/P&gt;
&lt;P&gt;1: The adapter is connected to J43&lt;/P&gt;
&lt;P&gt;2:&amp;nbsp; The SW5 power switch is turned ON&lt;/P&gt;
&lt;P&gt;3: J38 is set to pins 1–2 to select the external 5 V input&lt;/P&gt;
&lt;P&gt;Once these settings are confirmed, the board power rails—including those supplying the Arduino interface—should be available.&lt;/P&gt;
&lt;P&gt;Please try it.&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;May&lt;/P&gt;
&lt;/DIV&gt;</description>
      <pubDate>Fri, 12 Jun 2026 02:36:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/Using-Arduino-interface-of-MIMX-RT1170-EVK-for-sensor-connection/m-p/2380495#M9103</guid>
      <dc:creator>mayliu1</dc:creator>
      <dc:date>2026-06-12T02:36:56Z</dc:date>
    </item>
  </channel>
</rss>