<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NBP8s integration with Vector system in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/NBP8s-integration-with-Vector-system/m-p/2247154#M8982</link>
    <description>Hi Tomas&lt;BR /&gt;Thanks a lot for the quick response. The configuration is exactly the same as defined in datasheet and i am following the same steps as you have outlined.&lt;BR /&gt;&lt;BR /&gt;I try to set SPIOPS and the response from the sensor is 0x0220 and it stays the same for subsequent responses.&lt;BR /&gt;i am not sure if i am missing something.&lt;BR /&gt;Any thoughts on this ?&lt;BR /&gt;&lt;BR /&gt;Best regards,'&lt;BR /&gt;Rajvishnu</description>
    <pubDate>Mon, 24 Nov 2025 09:20:46 GMT</pubDate>
    <dc:creator>goodguy94</dc:creator>
    <dc:date>2025-11-24T09:20:46Z</dc:date>
    <item>
      <title>NBP8s integration with Vector system</title>
      <link>https://community.nxp.com/t5/Sensors/NBP8s-integration-with-Vector-system/m-p/2246790#M8980</link>
      <description>&lt;P&gt;Hello evreyone ,&lt;BR /&gt;&lt;BR /&gt;I am trying to integrate NBP8s pressure sensor with vector system. VT2710 sensor module has SPI interface.&lt;BR /&gt;&lt;BR /&gt;Has anyone tried this integration before ? Would love to know your suggestions. I am not able to get proper and valid response from the sensor.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;CAPL script i wrote :&lt;/P&gt;&lt;P&gt;/*@!Encoding:1252*/&lt;/P&gt;&lt;P&gt;variables&lt;BR /&gt;{&lt;BR /&gt;/* IO buffers, timers */&lt;BR /&gt;byte txBuffer[2];&lt;BR /&gt;msTimer tMain, tSpi, tDelay;&lt;/P&gt;&lt;P&gt;/* Main state machine */&lt;BR /&gt;int mainState = 0;&lt;BR /&gt;word curFrame;&lt;BR /&gt;int intAsserted, b_INTF;&lt;BR /&gt;int s4, s3, s2, s1, s0;&lt;/P&gt;&lt;P&gt;/* Micro-FSM for SPI transaction */&lt;BR /&gt;enum Spiop {OP_NONE = 0, OP_RD=1, OP_WR=2};&lt;BR /&gt;enum Spisub {IDLE=0, TX1=10, RX1=11, TX2=12, RX2=13};&lt;BR /&gt;int tr_op , spiSub;&lt;/P&gt;&lt;P&gt;word tr_addr = 0;&lt;BR /&gt;byte tr_wdata = 0;&lt;BR /&gt;byte tr_rdata = 0;&lt;BR /&gt;int tr_retry = 0; // bounded retry count (faults)&lt;BR /&gt;int needDummy = 1; // after WAKE/CS glitch or any detected fault&lt;/P&gt;&lt;P&gt;/* SPI response */&lt;BR /&gt;byte misoHi = 0, misoLo = 0;&lt;BR /&gt;word spiResp = 0;&lt;/P&gt;&lt;P&gt;/* Cached registers (live mirror) */&lt;BR /&gt;byte regSPIOPS = 0;&lt;BR /&gt;byte spiops_base = 0;&lt;BR /&gt;int spiops_base_valid = 0;&lt;/P&gt;&lt;P&gt;/* INT edge auto-detect */&lt;BR /&gt;int lastIntLevel = -1;&lt;BR /&gt;int Idle;&lt;BR /&gt;int active_IntPol = 0; // bit 5 of INTTRIG&lt;BR /&gt;int intLevel = 0;&lt;BR /&gt;int USE_READY_GATE = 1; // 0 - off (default) , 1 - on (real HW)&lt;/P&gt;&lt;P&gt;/* device asserts READY when it s safe to transact. */&lt;BR /&gt;int startupWaitDone = 0;&lt;/P&gt;&lt;P&gt;/* Optional: last decoded flags */&lt;BR /&gt;byte status, data;&lt;BR /&gt;word msb, lsb, msb_addr, lsb_addr;&lt;/P&gt;&lt;P&gt;/* Register Addresses */&lt;BR /&gt;word ADDR_SPIOPS = 0x0038; // [2]=CORE_TR_HOLD, [1:0]=FLASH_RANGE ; [7:3] reserved&lt;/P&gt;&lt;P&gt;/* Firmware/HW derivative/version windows (via SPIOPS) */&lt;BR /&gt;word ADDR_FW_DERIV = 0x0805; // valid when SPIOPS FLASH_RANGE == 00 (0x04)&lt;BR /&gt;word ADDR_FW_VER = 0x0804;&lt;BR /&gt;word ADDR_HW_DERIV = 0x1542; // valid when SPIOPS FLASH_RANGE == 11 (0x07)&lt;BR /&gt;word ADDR_HW_VER = 0x1543;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* SPI frame builder&lt;BR /&gt;p1 covers bits b15..b9, p0 covers b8..b2, both even parity. */&lt;BR /&gt;/* Build a 16-bit SPI frame per NBP8S protocol:&lt;BR /&gt;- bit15: R/W (1=write, 0=read)&lt;BR /&gt;- bits14..2: address / data field&lt;BR /&gt;- bits1..0: parity bits (even parity on bits15..9 and bits8..2) */&lt;/P&gt;&lt;P&gt;word makeNbp8sFrame(int rw, word addr_or_data)&lt;BR /&gt;{&lt;BR /&gt;word f = 0;&lt;BR /&gt;int group1, group2, p1, p0;&lt;/P&gt;&lt;P&gt;if (spiSub == TX1) {&lt;BR /&gt;/* TX1: Address frame 13-bit address */&lt;BR /&gt;f = ((rw &amp;amp; 1) &amp;lt;&amp;lt; 15) | ((addr_or_data &amp;amp; 0x1FFF) &amp;lt;&amp;lt; 2);&lt;/P&gt;&lt;P&gt;} else {&lt;BR /&gt;/* TX2: Data frame or dummy 8-bit data in bits9..2 */&lt;BR /&gt;f = ((rw &amp;amp; 1) &amp;lt;&amp;lt; 15) | ((addr_or_data &amp;amp; 0xFF) &amp;lt;&amp;lt; 2);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;write("[makeFrame] RAW Frame (no parity) = 0x%04X", f);&lt;/P&gt;&lt;P&gt;/* --- Inline parity logic (same as computeParity, no countBits) --- */&lt;BR /&gt;group1 = (f &amp;gt;&amp;gt; 9) &amp;amp; 0x7F; // bits 15..9&lt;BR /&gt;group2 = (f &amp;gt;&amp;gt; 2) &amp;amp; 0x7F; // bits 8..2&lt;/P&gt;&lt;P&gt;// count ones manually&lt;BR /&gt;p1 = 0; p0 = 0;&lt;BR /&gt;while (group1) { if (group1 &amp;amp; 1) p1++; group1 &amp;gt;&amp;gt;= 1; }&lt;BR /&gt;while (group2) { if (group2 &amp;amp; 1) p0++; group2 &amp;gt;&amp;gt;= 1; }&lt;/P&gt;&lt;P&gt;p1 = (p1 &amp;amp; 1) ; // even parity for group1&lt;BR /&gt;p0 = (p0 &amp;amp; 1) ; // even parity for group2&lt;/P&gt;&lt;P&gt;f &amp;amp;= 0xFFFC; // clear bits1..0&lt;BR /&gt;f |= ((p1 &amp;lt;&amp;lt; 1) | p0); // set parity bits&lt;/P&gt;&lt;P&gt;write("[makeFrame] Final frame = 0x%04X", f);&lt;BR /&gt;return f;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* Status &amp;amp; fault logging */&lt;BR /&gt;void logSpiStatus(word r)&lt;BR /&gt;{&lt;BR /&gt;s4 = (r &amp;gt;&amp;gt; 14) &amp;amp; 1;&lt;BR /&gt;s3 = (r &amp;gt;&amp;gt; 13) &amp;amp; 1;&lt;BR /&gt;s2 = (r &amp;gt;&amp;gt; 12) &amp;amp; 1;&lt;BR /&gt;s1 = (r &amp;gt;&amp;gt; 11) &amp;amp; 1;&lt;BR /&gt;s0 = (r &amp;gt;&amp;gt; 10) &amp;amp; 1;&lt;/P&gt;&lt;P&gt;status = (r &amp;gt;&amp;gt; 10) &amp;amp; 0x1F;&lt;BR /&gt;data = (r &amp;gt;&amp;gt; 2) &amp;amp; 0xFF;&lt;/P&gt;&lt;P&gt;write("[SPI Status Bits] s4=%d s3=%d s2=%d s1=%d s0=%d | Full Response=0x%04X", s4, s3, s2, s1, s0, r);&lt;BR /&gt;write("[SPI Decoded] Status=0x%02X Data=0x%02X", status, data);&lt;/P&gt;&lt;P&gt;if (s4) write("Fault: Reserved fault (undefined)");&lt;BR /&gt;if (s3) write("Fault: Ignored command or invalid previous read");&lt;BR /&gt;if (s2) write("Fault: Clock error");&lt;BR /&gt;if (s1) write("Fault: Parity error");&lt;BR /&gt;if (s0) write("Fault: Bus contention or illegal access");&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/* (s4..s0 any non-zero indicates an issue). */&lt;BR /&gt;int hasFault(word r)&lt;BR /&gt;{&lt;BR /&gt;return (((r &amp;gt;&amp;gt; 14) &amp;amp; 1) || ((r &amp;gt;&amp;gt; 13) &amp;amp; 1) || ((r &amp;gt;&amp;gt; 12) &amp;amp; 1) || ((r &amp;gt;&amp;gt; 11) &amp;amp; 1) || ((r &amp;gt;&amp;gt; 10) &amp;amp; 1));&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* Queue a 16-bit frame on MOSI (CS low is driven here) */&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;void sendFrame(word frame16)&lt;BR /&gt;{&lt;BR /&gt;txBuffer[0] = (byte)(frame16 &amp;gt;&amp;gt; 8);&lt;BR /&gt;txBuffer[1] = (byte)(frame16 &amp;amp; 0xFF);&lt;BR /&gt;sensorQueueMosiData("SENSOR::SPI::Master_Port::NBP_Sensor", txBuffer, 16);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* High-level: schedule a READ/WRITE op */&lt;/P&gt;&lt;P&gt;void spiReadByte(word addr)&lt;BR /&gt;{&lt;BR /&gt;tr_addr = addr;&lt;BR /&gt;tr_op = OP_RD;&lt;BR /&gt;tr_retry= 0;&lt;BR /&gt;spiSub = TX1;&lt;BR /&gt;setTimer(tSpi, 1);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;void spiWriteByte(word addr, byte data)&lt;BR /&gt;{&lt;BR /&gt;tr_addr = addr;&lt;BR /&gt;tr_wdata = data;&lt;BR /&gt;tr_op = OP_WR;&lt;BR /&gt;tr_retry= 0;&lt;BR /&gt;spiSub = TX1;&lt;BR /&gt;setTimer(tSpi, 1);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/* SPI Micro-FSM */&lt;BR /&gt;on timer tSpi&lt;BR /&gt;{&lt;BR /&gt;switch (spiSub)&lt;BR /&gt;{&lt;/P&gt;&lt;P&gt;/* TX1 */&lt;BR /&gt;case TX1:&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/42252"&gt;@VTS&lt;/a&gt;::VT2710_1_DIO_Ch2::DigitalOutput6 = 0 ; // CS low&lt;BR /&gt;&lt;BR /&gt;if (USE_READY_GATE &amp;amp;&amp;amp; (tr_addr != ADDR_SPIOPS))&lt;BR /&gt;{&lt;BR /&gt;intAsserted = (active_IntPol ? (intLevel == 1) : (intLevel == 0));&lt;BR /&gt;if( b_INTF &amp;amp;&amp;amp; !intAsserted)&lt;BR /&gt;{&lt;BR /&gt;write("[SPI] Waiting for READY before first TX1 - Sensor initiated");&lt;BR /&gt;setTimer(tSpi, 1);&lt;BR /&gt;break;&lt;BR /&gt;}&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;curFrame = needDummy ? makeNbp8sFrame(0, 0x0000): makeNbp8sFrame((tr_op == OP_WR) ? 1 : 0, tr_addr);&lt;/P&gt;&lt;P&gt;write("[TX1] Master --&amp;gt; Sensor: Frame = 0x%04X (R/W=%d Addr=0x%04X)",curFrame, (curFrame &amp;gt;&amp;gt; 15) &amp;amp; 1, (curFrame &amp;gt;&amp;gt; 2) &amp;amp; 0x1FFF);&lt;BR /&gt;sendFrame(curFrame);&lt;BR /&gt;spiSub = RX1;&lt;BR /&gt;setTimer(tSpi, 1);&lt;BR /&gt;break;&lt;/P&gt;&lt;P&gt;/* RX1 (R0 after TX1) */&lt;BR /&gt;case RX1:&lt;BR /&gt;misoHi = &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/149080"&gt;@sensor&lt;/a&gt;::SPI::Master_Port::NBP_Sensor::Frame1.MISO_Signals.MISO_High_byte;&lt;BR /&gt;misoLo = &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/149080"&gt;@sensor&lt;/a&gt;::SPI::Master_Port::NBP_Sensor::Frame1.MISO_Signals.MISO_Low_byte;&lt;BR /&gt;spiResp = ((word)misoHi &amp;lt;&amp;lt; &lt;LI-EMOJI id="lia_smiling-face-with-sunglasses" title=":smiling_face_with_sunglasses:"&gt;&lt;/LI-EMOJI&gt; | misoLo;&lt;BR /&gt;write("[RX1] Sensor --&amp;gt; Master: Response = 0x%04X (Status=0x%02X Data=0x%02X)",spiResp, (spiResp &amp;gt;&amp;gt; 10) &amp;amp; 0x1F, (spiResp &amp;gt;&amp;gt; 2) &amp;amp; 0xFF);&lt;BR /&gt;if (needDummy) {&lt;BR /&gt;needDummy = 0;&lt;BR /&gt;spiSub = TX1;&lt;BR /&gt;setTimer(tSpi, 1);&lt;BR /&gt;break;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;// correct fault handling&lt;BR /&gt;logSpiStatus(spiResp);&lt;BR /&gt;if(tr_addr != ADDR_SPIOPS)&lt;BR /&gt;{&lt;BR /&gt;s4 = (spiResp &amp;gt;&amp;gt; 14) &amp;amp; 1;&lt;BR /&gt;s3 = (spiResp &amp;gt;&amp;gt; 13) &amp;amp; 1;&lt;BR /&gt;s2 = (spiResp &amp;gt;&amp;gt; 12) &amp;amp; 1;&lt;BR /&gt;s1 = (spiResp &amp;gt;&amp;gt; 11) &amp;amp; 1;&lt;BR /&gt;s0 = (spiResp &amp;gt;&amp;gt; 10) &amp;amp; 1;&lt;/P&gt;&lt;P&gt;if (s2) { // Clock fault&lt;BR /&gt;if (tr_retry &amp;lt; 4) {&lt;BR /&gt;write("[SPI] Clock fault: dummy+retry");&lt;BR /&gt;needDummy = 1; tr_retry++;&lt;BR /&gt;spiSub = TX1; setTimer(tSpi, 5);&lt;BR /&gt;break;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;tr_op = OP_NONE;&lt;BR /&gt;spiSub = IDLE;&lt;BR /&gt;break;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;if (s3 || s4) {&lt;BR /&gt;write("[SPI] Fatal fault (Reserved/Previous read/write) error, aborting transfer");&lt;/P&gt;&lt;P&gt;tr_op = OP_NONE;&lt;BR /&gt;spiSub = IDLE;&lt;BR /&gt;break;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;if (s1 || s0) {&lt;BR /&gt;if (tr_retry &amp;lt; 4) {&lt;BR /&gt;write("[SPI] SPI fault (s1/s0) : dummy+retry");&lt;BR /&gt;needDummy = 1;&lt;BR /&gt;tr_retry++;&lt;BR /&gt;spiSub = TX1;&lt;BR /&gt;setTimer(tSpi, 1);&lt;BR /&gt;break;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;tr_op = OP_NONE;&lt;BR /&gt;spiSub = IDLE;&lt;BR /&gt;break;&lt;BR /&gt;}&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;if (tr_op == OP_WR) {&lt;BR /&gt;curFrame = makeNbp8sFrame(1, tr_wdata);&lt;BR /&gt;write("[TX2] Master --&amp;gt; Sensor: Data Frame = 0x%04X", curFrame);&lt;BR /&gt;sendFrame(curFrame);&lt;BR /&gt;spiSub = RX2;&lt;BR /&gt;setTimer(tSpi, 5);&lt;BR /&gt;break;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* For READs send dummy frame */&lt;BR /&gt;else if (tr_op == OP_RD) {&lt;BR /&gt;curFrame = makeNbp8sFrame(0, 0x0000);&lt;BR /&gt;write("[TX2] Master --&amp;gt; Sensor: Dummy Frame = 0x%04X", curFrame);&lt;BR /&gt;sendFrame(curFrame);&lt;BR /&gt;spiSub = RX2;&lt;BR /&gt;setTimer(tSpi, 1);&lt;BR /&gt;break;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* TX2 */&lt;BR /&gt;case TX2:&lt;BR /&gt;spiSub = RX2;&lt;BR /&gt;setTimer(tSpi, 1);&lt;BR /&gt;break;&lt;/P&gt;&lt;P&gt;/* RX2 (R1: DATA for READ, STATUS for WRITE) */&lt;BR /&gt;case RX2:&lt;BR /&gt;&lt;BR /&gt;misoHi = &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/149080"&gt;@sensor&lt;/a&gt;::SPI::Master_Port::NBP_Sensor::Frame1.MISO_Signals.MISO_High_byte;&lt;BR /&gt;misoLo = &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/149080"&gt;@sensor&lt;/a&gt;::SPI::Master_Port::NBP_Sensor::Frame1.MISO_Signals.MISO_Low_byte;&lt;BR /&gt;spiResp = ((word)misoHi &amp;lt;&amp;lt; &lt;LI-EMOJI id="lia_smiling-face-with-sunglasses" title=":smiling_face_with_sunglasses:"&gt;&lt;/LI-EMOJI&gt; | misoLo;&lt;BR /&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/42252"&gt;@VTS&lt;/a&gt;::VT2710_1_DIO_Ch2::DigitalOutput6 = 1 ; // CS high&lt;BR /&gt;setTimer(tDelay, 10);&lt;BR /&gt;write("[RX2] Sensor --&amp;gt; Master: Response = 0x%04X (Status=0x%02X Data=0x%02X)",spiResp, (spiResp &amp;gt;&amp;gt; 10) &amp;amp; 0x1F, (spiResp &amp;gt;&amp;gt; 2) &amp;amp; 0xFF);&lt;/P&gt;&lt;P&gt;logSpiStatus(spiResp); // correct fault handling */&lt;BR /&gt;if(tr_addr != ADDR_SPIOPS)&lt;BR /&gt;{&lt;BR /&gt;s4 = (spiResp &amp;gt;&amp;gt; 14) &amp;amp; 1;&lt;BR /&gt;s3 = (spiResp &amp;gt;&amp;gt; 13) &amp;amp; 1;&lt;BR /&gt;s2 = (spiResp &amp;gt;&amp;gt; 12) &amp;amp; 1;&lt;BR /&gt;s1 = (spiResp &amp;gt;&amp;gt; 11) &amp;amp; 1;&lt;BR /&gt;s0 = (spiResp &amp;gt;&amp;gt; 10) &amp;amp; 1;&lt;/P&gt;&lt;P&gt;if (s2) { // Clock fault&lt;BR /&gt;if (tr_retry &amp;lt; 4) {&lt;BR /&gt;write("[SPI] Clock fault: dummy+retry");&lt;BR /&gt;needDummy = 1;&lt;BR /&gt;tr_retry++;&lt;BR /&gt;spiSub = TX1;&lt;BR /&gt;setTimer(tSpi, 1);&lt;BR /&gt;break;&lt;BR /&gt;}&lt;BR /&gt;tr_op = OP_NONE;&lt;BR /&gt;spiSub = IDLE;&lt;BR /&gt;break;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;if (s3 || s4) {&lt;BR /&gt;write("[SPI] Fatal fault (parity/contend), aborting transfer");&lt;BR /&gt;tr_op = OP_NONE;&lt;BR /&gt;spiSub = IDLE;&lt;BR /&gt;break;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;if (s1 || s0) {&lt;BR /&gt;if (tr_retry &amp;lt; 4) {&lt;BR /&gt;write("[SPI] SPI fault (s1/s0) : dummy+retry");&lt;BR /&gt;needDummy = 1;&lt;BR /&gt;tr_retry++;&lt;BR /&gt;spiSub = TX1;&lt;BR /&gt;setTimer(tSpi, 1);&lt;BR /&gt;break;&lt;BR /&gt;}&lt;BR /&gt;tr_op = OP_NONE;&lt;BR /&gt;spiSub = IDLE;&lt;BR /&gt;break;&lt;BR /&gt;}&lt;BR /&gt;}&lt;BR /&gt;if (tr_op == OP_RD)&lt;BR /&gt;tr_rdata = (spiResp &amp;gt;&amp;gt; 2) &amp;amp; 0xFF;&lt;/P&gt;&lt;P&gt;tr_op = OP_NONE;&lt;BR /&gt;spiSub = IDLE;&lt;BR /&gt;setTimer(tDelay, 1);&lt;BR /&gt;break;&lt;BR /&gt;}&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* Utility */&lt;BR /&gt;int spiBusy() { return (tr_op != OP_NONE) || (spiSub != IDLE); }&lt;/P&gt;&lt;P&gt;/* Start */&lt;BR /&gt;on start&lt;BR /&gt;{&lt;BR /&gt;write("NBP8s Evaluation");&lt;BR /&gt;setTimer(tDelay,38);&lt;/P&gt;&lt;P&gt;needDummy = 1; /* first transfer dummy after WAKE/CS glitch */&lt;BR /&gt;mainState = 0;&lt;BR /&gt;tr_op = OP_NONE;&lt;BR /&gt;spiSub = IDLE;&lt;BR /&gt;startupWaitDone = 1;&lt;BR /&gt;setTimer(tMain, 35);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* tDelay yields back to main */&lt;BR /&gt;on timer tDelay&lt;BR /&gt;{&lt;BR /&gt;setTimer(tMain, 5);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* Main FSM */&lt;BR /&gt;on timer tMain&lt;BR /&gt;{&lt;BR /&gt;setTimer(tMain, 1);&lt;BR /&gt;&lt;BR /&gt;/* State machine */&lt;BR /&gt;switch (mainState)&lt;BR /&gt;{&lt;BR /&gt;/* SPIOPS handshake */&lt;BR /&gt;case 0:&lt;BR /&gt;if (spiBusy()) break;&lt;BR /&gt;// If a dummy is pending (e.g. after reset/fault), consume it&lt;BR /&gt;write("SPIOPS - Dummy frame to clear start up");&lt;/P&gt;&lt;P&gt;// &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/42252"&gt;@VTS&lt;/a&gt;::VT2710_1_DIO_Ch2::DigitalOutput6 = 0; // CS low&lt;BR /&gt;// setTimer(tDelay, 2);&lt;BR /&gt;// &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/42252"&gt;@VTS&lt;/a&gt;::VT2710_1_DIO_Ch2::DigitalOutput6 = 1; // CS high&lt;BR /&gt;// setTimer(tDelay, 5);&lt;BR /&gt;&lt;BR /&gt;spiReadByte(0x0000); // dummy frame (ignored by device)&lt;BR /&gt;setTimer(tDelay,5);&lt;/P&gt;&lt;P&gt;needDummy = 0;&lt;BR /&gt;setTimer(tDelay,5);&lt;BR /&gt;mainState = 1;&lt;BR /&gt;break;&lt;/P&gt;&lt;P&gt;case 1:&lt;BR /&gt;if (spiBusy()) break;&lt;BR /&gt;write("SPIOPS - SENSOR Ready , proceeding to write");&lt;BR /&gt;spiWriteByte(ADDR_SPIOPS, 0x04); // write SPIOPS = 0x04&lt;BR /&gt;setTimer(tDelay,5);&lt;BR /&gt;mainState = 2;&lt;BR /&gt;break;&lt;/P&gt;&lt;P&gt;case 2:&lt;BR /&gt;if (spiBusy()) break;&lt;BR /&gt;spiReadByte(ADDR_SPIOPS); // read back SPIOPS&lt;BR /&gt;setTimer(tDelay, 5);&lt;BR /&gt;mainState = 3;&lt;BR /&gt;break;&lt;/P&gt;&lt;P&gt;case 3:&lt;BR /&gt;if (spiBusy()) break;&lt;BR /&gt;mainState = 4;&lt;BR /&gt;break;&lt;/P&gt;&lt;P&gt;case 4:&lt;BR /&gt;if (spiBusy()) break;&lt;/P&gt;&lt;P&gt;// Use tr_rdata (captured byte) instead of spiResp bits&lt;BR /&gt;regSPIOPS = (byte)(tr_rdata &amp;amp; 0x07);&lt;/P&gt;&lt;P&gt;// If HOLD active and range 00 -&amp;gt; SPIOPS must be 0x04&lt;BR /&gt;if (regSPIOPS == 0x04) {&lt;BR /&gt;write("SPIOPS: SET OK (0x%02X)", regSPIOPS);&lt;BR /&gt;mainState = 10; // go to FW/HW read&lt;BR /&gt;}&lt;BR /&gt;else {&lt;BR /&gt;write("SPIOPS NOT READY (SPIOPS = 0x%02X) --&amp;gt; retrying", regSPIOPS);&lt;BR /&gt;needDummy = 1;&lt;BR /&gt;setTimer(tDelay,5);&lt;BR /&gt;mainState = 1 ;&lt;BR /&gt;}&lt;BR /&gt;break;&lt;/P&gt;&lt;P&gt;/* FW / HW READ SEQUENCE */&lt;BR /&gt;case 10:&lt;BR /&gt;if (spiBusy()) break;&lt;BR /&gt;write("SPIOPS already set to 0x04 --&amp;gt; Firmware window active");&lt;BR /&gt;write("Reading FW_DERIV (0x0805)...");&lt;BR /&gt;spiReadByte(ADDR_FW_DERIV);&lt;BR /&gt;setTimer(tDelay, 5);&lt;BR /&gt;mainState = 11;&lt;BR /&gt;break;&lt;/P&gt;&lt;P&gt;case 11:&lt;BR /&gt;if (spiBusy()) break;&lt;BR /&gt;write("FW_DERIV = 0x%02X", tr_rdata);&lt;BR /&gt;write("Reading FW_VER (0x0804)...");&lt;BR /&gt;spiReadByte(ADDR_FW_VER);&lt;BR /&gt;setTimer(tDelay, 5);&lt;BR /&gt;mainState = 12;&lt;BR /&gt;break;&lt;/P&gt;&lt;P&gt;case 12:&lt;BR /&gt;if (spiBusy()) break;&lt;BR /&gt;write("FW_VER = 0x%02X", tr_rdata);&lt;BR /&gt;setTimer(tDelay, 5);&lt;BR /&gt;mainState = 13;&lt;BR /&gt;break;&lt;/P&gt;&lt;P&gt;case 13:&lt;BR /&gt;if (spiBusy()) break;&lt;BR /&gt;write("Clearing SPIOPS (0x0038) to release NBP8s CPU");&lt;BR /&gt;spiWriteByte(ADDR_SPIOPS, 0x00);&lt;BR /&gt;setTimer(tDelay, 5);&lt;BR /&gt;mainState = 14;&lt;BR /&gt;break;&lt;BR /&gt;&lt;BR /&gt;case 14:&lt;BR /&gt;if (spiBusy()) break;&lt;BR /&gt;write("FW read complete");&lt;BR /&gt;mainState = 99;&lt;BR /&gt;break;&lt;/P&gt;&lt;P&gt;case 99:&lt;BR /&gt;// Idle / stop&lt;BR /&gt;break;&lt;BR /&gt;}}&lt;/P&gt;&lt;P&gt;any suggestions and feedback would be helpful for further progress.&lt;BR /&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 20:53:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/NBP8s-integration-with-Vector-system/m-p/2246790#M8980</guid>
      <dc:creator>goodguy94</dc:creator>
      <dc:date>2026-02-03T20:53:27Z</dc:date>
    </item>
    <item>
      <title>Re: NBP8s integration with Vector system</title>
      <link>https://community.nxp.com/t5/Sensors/NBP8s-integration-with-Vector-system/m-p/2246835#M8981</link>
      <description>&lt;P&gt;Hello&amp;nbsp;Rajvishnu,&lt;/P&gt;
&lt;P&gt;The NBP8 sensor uses SPI Mode 0 (CPOL=0, CPHA=0) with 16-bit frames and even parity on two groups of bits. Ensure your Vector VT2710 SPI settings match this.&amp;nbsp;After WAKEUP or any CS_B glitch, the first SPI command is ignored due to a clock fault -&amp;gt; send a dummy frame first to clear the error.&amp;nbsp;Always wait for the READY pin to assert before starting SPI transfers. This indicates the sensor is ready and its CPU is halted.&amp;nbsp;Check that CS_B stays low for all 16 clock cycles per frame and that parity bits are correct.&amp;nbsp;Handle fault bits (s4..s0) properly. If any are set, retry with a dummy frame. s3 (ignored command) also requires a retry.&amp;nbsp;Clear the SPIOPS register at the end of the session to resume normal sensor operation.&amp;nbsp;These steps usually resolve invalid responses during integration.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Mon, 24 Nov 2025 08:04:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/NBP8s-integration-with-Vector-system/m-p/2246835#M8981</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2025-11-24T08:04:44Z</dc:date>
    </item>
    <item>
      <title>Re: NBP8s integration with Vector system</title>
      <link>https://community.nxp.com/t5/Sensors/NBP8s-integration-with-Vector-system/m-p/2247154#M8982</link>
      <description>Hi Tomas&lt;BR /&gt;Thanks a lot for the quick response. The configuration is exactly the same as defined in datasheet and i am following the same steps as you have outlined.&lt;BR /&gt;&lt;BR /&gt;I try to set SPIOPS and the response from the sensor is 0x0220 and it stays the same for subsequent responses.&lt;BR /&gt;i am not sure if i am missing something.&lt;BR /&gt;Any thoughts on this ?&lt;BR /&gt;&lt;BR /&gt;Best regards,'&lt;BR /&gt;Rajvishnu</description>
      <pubDate>Mon, 24 Nov 2025 09:20:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/NBP8s-integration-with-Vector-system/m-p/2247154#M8982</guid>
      <dc:creator>goodguy94</dc:creator>
      <dc:date>2025-11-24T09:20:46Z</dc:date>
    </item>
  </channel>
</rss>