<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 PCF85053A Bootable CPU RTC with two I2C buses</title>
    <link>https://community.nxp.com/t5/Sensors/PCF85053A-Bootable-CPU-RTC-with-two-I2C-buses/m-p/2177465#M8956</link>
    <description>&lt;P&gt;Hi all,&lt;BR /&gt;I am using PCF85053a rtc in our project,&lt;BR /&gt;one control bit TWO, have power to control the time write access from secondary i2c,&lt;BR /&gt;when removing cr2032 control bit TWO reg move to zero,&lt;BR /&gt;do this reg move back zero when power cut happen in rtc or only after removing cr2032 battery, attached the datasheet ...&lt;BR /&gt;when primary system taking control over rtc , it makes control bit TWO as 1 and it should never go back until or unless cr2032 is not removed and added, but i am observing very suspicious behavior with the control bit TWO reg, why sometimes it moves back 0&lt;/P&gt;</description>
    <pubDate>Mon, 29 Sep 2025 12:09:50 GMT</pubDate>
    <dc:creator>ninja_hathori</dc:creator>
    <dc:date>2025-09-29T12:09:50Z</dc:date>
    <item>
      <title>PCF85053A Bootable CPU RTC with two I2C buses</title>
      <link>https://community.nxp.com/t5/Sensors/PCF85053A-Bootable-CPU-RTC-with-two-I2C-buses/m-p/2177465#M8956</link>
      <description>&lt;P&gt;Hi all,&lt;BR /&gt;I am using PCF85053a rtc in our project,&lt;BR /&gt;one control bit TWO, have power to control the time write access from secondary i2c,&lt;BR /&gt;when removing cr2032 control bit TWO reg move to zero,&lt;BR /&gt;do this reg move back zero when power cut happen in rtc or only after removing cr2032 battery, attached the datasheet ...&lt;BR /&gt;when primary system taking control over rtc , it makes control bit TWO as 1 and it should never go back until or unless cr2032 is not removed and added, but i am observing very suspicious behavior with the control bit TWO reg, why sometimes it moves back 0&lt;/P&gt;</description>
      <pubDate>Mon, 29 Sep 2025 12:09:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/PCF85053A-Bootable-CPU-RTC-with-two-I2C-buses/m-p/2177465#M8956</guid>
      <dc:creator>ninja_hathori</dc:creator>
      <dc:date>2025-09-29T12:09:50Z</dc:date>
    </item>
    <item>
      <title>Re: PCF85053A Bootable CPU RTC with two I2C buses</title>
      <link>https://community.nxp.com/t5/Sensors/PCF85053A-Bootable-CPU-RTC-with-two-I2C-buses/m-p/2177675#M8957</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Could you please share your schematic?&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;It’s not entirely clear to me. Please note that when the RTC switches to battery mode, the VDD power domain is disabled. This means the I²C interface is ignored, the CLK output is disabled, and the pin goes into high impedance (Hi-Z).&lt;BR /&gt;Thanks to the battery, the RTC continues keeping time, but communication is not possible until VDD rises above the threshold again.&lt;BR /&gt;Regarding your question: Does the TWO register reset to 0 (default) only when the CR2032 battery is removed, even if VDD is still present?&lt;/P&gt;
&lt;P&gt;Regards.&lt;/P&gt;</description>
      <pubDate>Mon, 29 Sep 2025 19:12:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/PCF85053A-Bootable-CPU-RTC-with-two-I2C-buses/m-p/2177675#M8957</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2025-09-29T19:12:19Z</dc:date>
    </item>
    <item>
      <title>Re: PCF85053A Bootable CPU RTC with two I2C buses</title>
      <link>https://community.nxp.com/t5/Sensors/PCF85053A-Bootable-CPU-RTC-with-two-I2C-buses/m-p/2178104#M8958</link>
      <description>&lt;P&gt;Hi Erika,&amp;nbsp;&lt;BR /&gt;Thanks for the response, I am asking about the behaviour of the TWO reg in control bit, highlighted in the attachment,&amp;nbsp;&lt;BR /&gt;when primary i2c set the time, it takes ownership of rtc module and make TWO bit 1,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;my question is when this TWO bits come to default state zero,&amp;nbsp;&lt;BR /&gt;case 1: when rtc coin cell cr2032 is removed or&amp;nbsp;&lt;BR /&gt;case 2: when rtc power is turn off,&lt;BR /&gt;&lt;BR /&gt;my observation, when I am removing coin cell cr2032 it comes back to zero,&amp;nbsp;&lt;BR /&gt;but sometimes it comes back to zero, with no reason, which allow secondary i2c to set time, we not want this ...&lt;/P&gt;</description>
      <pubDate>Tue, 30 Sep 2025 10:02:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/PCF85053A-Bootable-CPU-RTC-with-two-I2C-buses/m-p/2178104#M8958</guid>
      <dc:creator>ninja_hathori</dc:creator>
      <dc:date>2025-09-30T10:02:55Z</dc:date>
    </item>
    <item>
      <title>Re: PCF85053A Bootable CPU RTC with two I2C buses</title>
      <link>https://community.nxp.com/t5/Sensors/PCF85053A-Bootable-CPU-RTC-with-two-I2C-buses/m-p/2182075#M8962</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi Erika,&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for the response, I am asking about the behaviour of the TWO reg in control bit, highlighted in the attachment,&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;when primary i2c set the time, it takes ownership of rtc module and make TWO bit 1,&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;my question is when this TWO bits come to default state zero,&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;case 1: when rtc coin cell cr2032 is removed or&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;case 2: when rtc power is turn off,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;my observation, when I am removing coin cell cr2032 it comes back to zero,&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;but sometimes it comes back to zero, with no reason, which allow secondary i2c to set time, we not want this ...&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Oct 2025 17:54:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/PCF85053A-Bootable-CPU-RTC-with-two-I2C-buses/m-p/2182075#M8962</guid>
      <dc:creator>ninja_hathori</dc:creator>
      <dc:date>2025-10-08T17:54:04Z</dc:date>
    </item>
  </channel>
</rss>