<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 Re: MMA8451Q FIFO Interrupt... getting extra interrupts without FIFO flag</title>
    <link>https://community.nxp.com/t5/Sensors/MMA8451Q-FIFO-Interrupt-getting-extra-interrupts-without-FIFO/m-p/2137451#M8909</link>
    <description>&lt;P&gt;Thanks&amp;nbsp;@ JosefKozen.&lt;/P&gt;&lt;P&gt;I have in fact tried all of those things.&lt;/P&gt;&lt;P&gt;Accomplishing #1 while still gaining (and printing) some diagnostics is a like a quantum physics problem... you disturb the system by observing it.&amp;nbsp; If you don't "observe" it with the diagnostics, it might be working correctly but with&amp;nbsp; "observing" it, you don't know.&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;Schrödinger&lt;/SPAN&gt; lives...&lt;/P&gt;&lt;P&gt;I am really trying not to leave any time slices unsampled.&amp;nbsp; I am playing with how I allocate the tasks between cores and the time slice priorities in FreeRTOS to see if I can "get around" to checking the interrupt more promptly.&amp;nbsp; That might be my biggest problem.&lt;/P&gt;&lt;P&gt;I know see that the MMA 8451Q is going out of production so will need to change chips for production.&amp;nbsp; &amp;nbsp;I need to maintain 14-bit resolution for my application.&amp;nbsp; I found some non-NXP accelerometer chips with 14-bit resolution at 2g AND 512 sample FIFOs.&amp;nbsp; &amp;nbsp;A larger FIFO would allow me to grab my 500ms worth of samples in a single (long) I2C fetch.&amp;nbsp; That would dramatically improve my timing issues.&amp;nbsp; Does NXP offer such a chip?&amp;nbsp; (even a 256 sample FIFO, or possibly a 128 sample FIFO, would do the trick)&lt;/P&gt;&lt;P&gt;Thanks again!&lt;/P&gt;</description>
    <pubDate>Mon, 21 Jul 2025 12:45:00 GMT</pubDate>
    <dc:creator>peteDDD</dc:creator>
    <dc:date>2025-07-21T12:45:00Z</dc:date>
    <item>
      <title>MMA8451Q FIFO Interrupt... getting extra interrupts without FIFO flag</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8451Q-FIFO-Interrupt-getting-extra-interrupts-without-FIFO/m-p/2136636#M8906</link>
      <description>&lt;P&gt;I have been working for months on a motion sensing project using the MMA8451Q and now realize that my FIFO full (watermark) interrupts and generating an extra interrupt before the FIFO watermark is achieved (FIFO full).&amp;nbsp; It seems to me that the interrupt is being re-asserted immediately after I check the INT_SOURCE register (0x0C) or after I check the FIFO_STATUS register (0x00).&amp;nbsp; But since I should check the INT_SOURCE register to make sure I have the current interrupt and must check the FIFO_STATUS register to know if the number of samples in the FIFO is correct, how can I avoid getting these "extra" interrupts.&lt;/P&gt;&lt;P&gt;Let me clarify further with a highly instrumented and commented version of my software.&lt;/P&gt;&lt;P&gt;First, the configuration...&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;FIFO FULL interrupt with watermark at 32 samples&lt;/LI&gt;&lt;LI&gt;Range: 2G, 14-bit&lt;/LI&gt;&lt;LI&gt;200hz sample rate, low-noise off, fast read off, active mode&lt;/LI&gt;&lt;/UL&gt;&lt;DIV&gt;&lt;DIV&gt;Set up interrupt for ESP32-S3&lt;/DIV&gt;&lt;/DIV&gt;&lt;LI-CODE lang="cpp"&gt;    pinMode(mmaInt1, INPUT_PULLUP);
    attachInterrupt(mmaInt1, handleInterrupt, FALLING);&lt;/LI-CODE&gt;&lt;DIV&gt;Incidentally, yes, I have tried RISING as well...)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Then configure the MMA8451Q&lt;/DIV&gt;&lt;LI-CODE lang="cpp"&gt; writeRegister8(MMA8451_REG_CTRL_REG1, 0x00);

  // Configure for 2G range (maximum sensitivity)
  writeRegister8(MMA8451_REG_XYZ_DATA_CFG, MMA8451_RANGE_2_G);  // setting to 2G sets res to 14-bit

  // Enable FIFO interrupt on INT1 pin
  writeRegister8(MMA8451_REG_CTRL_REG4, MMA8451_INT_EN_FIFO); // Enable FIFO interrupt  
  writeRegister8(MMA8451_REG_CTRL_REG5, MMA8451_INT_CFG_FIFO_INT1); // Route FIFO to INT1

  // Configure FIFO after interrupts
  // Fill mode (stop when full)
  writeRegister8(MMA8451_F_SETUP, MMA8451_FIFI_MODE_FILL_BUFFER | Jconfig.FIFO_WATERMARK); // 0x80 for fill mode (FMODE = 11), 0x20 for watermark at 32

  // Set for highest precision:
  // - ignore auto-wake frequency field
  // - 400z data rate (0b011) for 80ms of data  MMA8451_DATARATE_400_HZ
  // - Low-Noise off  MMA8451_LNOISE_OFF 
  // - Normal read mode    MMA8451_F_READ_OFF = 0b00
  // - Active mode   MMA8451_ACTIVE = 0b01
  writeRegister8(MMA8451_REG_CTRL_REG1, MMA8451_DATARATE_200_HZ | MMA8451_LNOISE_OFF | MMA8451_F_READ_OFF | MMA8451_ACTIVE);  // Changed from 0x19 to 0x15 for 400Hz

  // Add a small delay to let the device stabilize
  delay(10);&lt;/LI-CODE&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Now, I set a flag when I catch the interrupt&lt;/DIV&gt;&lt;LI-CODE lang="cpp"&gt;volatile bool movementInterrupt = false;
void IRAM_ATTR handleInterrupt() {
    // Only set a flag - no I2C communication in ISR!
    portENTER_CRITICAL_ISR(&amp;amp;mux);
    movementInterrupt = true;
    portEXIT_CRITICAL_ISR(&amp;amp;mux);
}&lt;/LI-CODE&gt;&lt;DIV&gt;and I look for the interrupt in my state machine&lt;/DIV&gt;&lt;LI-CODE lang="markup"&gt;bool checkForMovementAndReadFIFO() {
    static const char* TAG = "checkForMovementAndReadFIFO";
   // if (movementInterrupt &amp;gt; 0) {
    checkForMovementAndReadFIFO_startTime = millis();
    if (movementInterrupt) {

        portENTER_CRITICAL(&amp;amp;mux);
        movementInterrupt = false;
        portEXIT_CRITICAL(&amp;amp;mux);
...
        ESP_LOGD(TAG, "\n\n");
        ESP_LOGD(TAG, "Interrupt!");

         // According to datasheet... the FIFO interrupt is automatically cleared when you read the F_STATUS register (which we're doing in getFIFOStatus()
        uint8_t Int_SourceSystem = mma.getIntSourceReg();
        ESP_LOGD(TAG, "***Int_SourceSystem: 0x%02X", Int_SourceSystem);

       // Read interrupt status registers
        uint8_t fifoStatus = mma.getFIFOStatus();
        ESP_LOGD(TAG, "FIFO Status: 0x%02X", fifoStatus);
        ESP_LOGD(TAG, "  Overflow: %d", (fifoStatus &amp;amp; 0x80) ? 1 : 0);
        ESP_LOGD(TAG, "  Watermark: %d", (fifoStatus &amp;amp; 0x40) ? 1 : 0);
        ESP_LOGD(TAG, "  Sample Count: %d", fifoStatus &amp;amp; 0x3F);


        // Check if FIFO watermark caused the interrupt
        if (fifoStatus &amp;amp; 0x40) // Check F_WMRK_FLAG bit  if set, FIFO watermark event detected. FIFO sample count is equal to watermark value.
        {
            ESP_LOGD(TAG, "Valid FIFO interrupt");
            // Read in 32 14-bit raw values
          bool errorcode = (i2c_dev-&amp;gt;write_then_read(targetRegister, 1, FIFObuffer, use14bit ? BYTES_IN_14_BIT_FIFO : BYTES_IN_8_BIT_FIFO));  // this converts to (i2c_dev-&amp;gt;write_then_read(targetRegister, 1, FIFObuffer,6)
...
// NOW, THE FIFO FULL STATUS SHOULD BE CLEARED AS SOON AS WE READ THE FIRST ITEM IN THE FIFO BUFFER (per the datasheet)
// then my math on the data
// check is we have accumulated &amp;gt; 500ms worth of samples
  }
 else {
            if (fifoStatus == 0x00) // check for no FIFO watermark or overflow
            {
                ESP_LOGD(TAG, "no FIFO watermark or overflow event");
            }
            else {
                ESP_LOGD(TAG, "Invalid interrupt: %d\n", Int_SourceSystem);
                ESP_LOGD(TAG, "Unexpected FIFO status: 0x%02X\n", fifoStatus);
            }
            ESP_LOGD(TAG, "checkForMovementAndReadFIFO elapsed time: %dms", millis() - checkForMovementAndReadFIFO_startTime);
            return false;
        }
    } // if (movementInterrupt &amp;gt; 0)
    ESP_LOGD(TAG, "checkForMovementAndReadFIFO elapsed time: %dms", millis() - checkForMovementAndReadFIFO_startTime);
    return false;
}&lt;/LI-CODE&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;And now the output...&amp;nbsp; I have added comments to the output which are preceded with "&amp;gt;&amp;gt;"&lt;/DIV&gt;&lt;LI-CODE lang="cpp"&gt;D (41928) checkForMovementAndReadFIFO: [MEMS_Support.cpp:282] checkForMovementAndReadFIFO():    &amp;gt;&amp;gt; WE CHECK FOR INTERRUPT FLAG 


D (41928) checkForMovementAndReadFIFO: [MEMS_Support.cpp:283] checkForMovementAndReadFIFO(): Interrupt!  &amp;gt;&amp;gt; AND WE FIND IT
D (41939) checkForMovementAndReadFIFO: [MEMS_Support.cpp:287] checkForMovementAndReadFIFO(): ***Int_SourceSystem: 0x40   &amp;gt;&amp;gt; IT IS A FIFO FULL INTERRUPT 
D (41949) checkForMovementAndReadFIFO: [MEMS_Support.cpp:291] checkForMovementAndReadFIFO(): FIFO Status: 0xE0
D (41960) checkForMovementAndReadFIFO: [MEMS_Support.cpp:292] checkForMovementAndReadFIFO():   Overflow: 1
D (41970) checkForMovementAndReadFIFO: [MEMS_Support.cpp:293] checkForMovementAndReadFIFO():   Watermark: 1 &amp;gt;&amp;gt; THE WATERMARK BIT **IS** SET
D (41980) checkForMovementAndReadFIFO: [MEMS_Support.cpp:294] checkForMovementAndReadFIFO():   Sample Count: 32  &amp;gt;&amp;gt; AND INDEED, THE FIFO SAMPLE COUNT IS CORRECT AT 32
D (41991) checkForMovementAndReadFIFO: [MEMS_Support.cpp:300] checkForMovementAndReadFIFO(): Valid FIFO interrupt
D (42006) checkForMovementAndReadFIFO: [MEMS_Support.cpp:303] checkForMovementAndReadFIFO(): FIFO read successful &amp;gt;&amp;gt; ALL DATA FROM FIFO RETRIEVED AND PROCESSED
D (42006) checkForMovementAndReadFIFO: [MEMS_Support.cpp:357] checkForMovementAndReadFIFO(): checkForMovementAndReadFIFO elapsed time: 78ms  &amp;gt;&amp;gt; DONE WITH PLENTY OF TIME TO SPARE
D (42029) checkForMovementAndReadFIFO: [MEMS_Support.cpp:282] checkForMovementAndReadFIFO(): &amp;gt;&amp;gt; NEXT CHECK FOR INTERRUPT FLAG (23MS LATER)


D (42029) checkForMovementAndReadFIFO: [MEMS_Support.cpp:283] checkForMovementAndReadFIFO(): Interrupt! &amp;gt;&amp;gt; AND WE FIND IT
D (42040) checkForMovementAndReadFIFO: [MEMS_Support.cpp:287] checkForMovementAndReadFIFO(): ***Int_SourceSystem: 0x00 &amp;gt;&amp;gt; BUT THE FIFO FULL FLAG IS **NOT** SET
D (42050) checkForMovementAndReadFIFO: [MEMS_Support.cpp:291] checkForMovementAndReadFIFO(): FIFO Status: 0x0A
D (42061) checkForMovementAndReadFIFO: [MEMS_Support.cpp:292] checkForMovementAndReadFIFO():   Overflow: 0
D (42071) checkForMovementAndReadFIFO: [MEMS_Support.cpp:293] checkForMovementAndReadFIFO():   Watermark: 0  &amp;gt;&amp;gt; THE WATERMARK BIT **IS NOT** SET
D (42081) checkForMovementAndReadFIFO: [MEMS_Support.cpp:294] checkForMovementAndReadFIFO():   Sample Count: 10 &amp;gt;&amp;gt; AND INDEED, THE FIFO IS NOT FULL
D (42091) checkForMovementAndReadFIFO: [MEMS_Support.cpp:350] checkForMovementAndReadFIFO(): Invalid interrupt: 0

D (42102) checkForMovementAndReadFIFO: [MEMS_Support.cpp:351] checkForMovementAndReadFIFO(): Unexpected FIFO status: 0x0A

D (42112) checkForMovementAndReadFIFO: [MEMS_Support.cpp:353] checkForMovementAndReadFIFO(): checkForMovementAndReadFIFO elapsed time: 83ms
D (42124) checkForMovementAndReadFIFO: [MEMS_Support.cpp:357] checkForMovementAndReadFIFO(): checkForMovementAndReadFIFO elapsed time: 0ms &amp;gt;&amp;gt; WE CHECK FOR THE INTERRUPT FLAG...AND DON'T FIND ONE
D (42136) checkForMovementAndReadFIFO: [MEMS_Support.cpp:357] checkForMovementAndReadFIFO(): checkForMovementAndReadFIFO elapsed time: 0ms &amp;gt;&amp;gt; WE CHECK FOR THE INTERRUPT FLAG...AND DON'T FIND ONE
D (42148) checkForMovementAndReadFIFO: [MEMS_Support.cpp:357] checkForMovementAndReadFIFO(): checkForMovementAndReadFIFO elapsed time: 0ms &amp;gt;&amp;gt; WE CHECK FOR THE INTERRUPT FLAG...AND DON'T FIND ONE
D (42160) checkForMovementAndReadFIFO: [MEMS_Support.cpp:282] checkForMovementAndReadFIFO(): &amp;gt;&amp;gt; NEXT CHECK FOR INTERRUPT FLAG


D (42170) checkForMovementAndReadFIFO: [MEMS_Support.cpp:283] checkForMovementAndReadFIFO(): Interrupt! &amp;gt;&amp;gt; AND WE FIND IT
D (42171) checkForMovementAndReadFIFO: [MEMS_Support.cpp:287] checkForMovementAndReadFIFO(): ***Int_SourceSystem: 0x40 &amp;gt;&amp;gt; IT IS A FIFO FULL INTERRUPT 
D (42181) checkForMovementAndReadFIFO: [MEMS_Support.cpp:291] checkForMovementAndReadFIFO(): FIFO Status: 0xE0
D (42191) checkForMovementAndReadFIFO: [MEMS_Support.cpp:292] checkForMovementAndReadFIFO():   Overflow: 1
D (42202) checkForMovementAndReadFIFO: [MEMS_Support.cpp:293] checkForMovementAndReadFIFO():   Watermark: 1 &amp;gt;&amp;gt; THE WATERMARK BIT **IS** SET
D (42212) checkForMovementAndReadFIFO: [MEMS_Support.cpp:294] checkForMovementAndReadFIFO():   Sample Count: 32 &amp;gt;&amp;gt; AND INDEED, THE FIFO SAMPLE COUNT IS CORRECT AT 32

D (42222) checkForMovementAndReadFIFO: [MEMS_Support.cpp:300] checkForMovementAndReadFIFO(): Valid FIFO interrupt
D (42237) checkForMovementAndReadFIFO: [MEMS_Support.cpp:303] checkForMovementAndReadFIFO(): FIFO read successful &amp;gt;&amp;gt; ALL DATA FROM FIFO RETRIEVED AND PROCESSED
D (42248) checkForMovementAndReadFIFO: [MEMS_Support.cpp:357] checkForMovementAndReadFIFO(): checkForMovementAndReadFIFO elapsed time: 88ms
D (42260) checkForMovementAndReadFIFO: [MEMS_Support.cpp:282] checkForMovementAndReadFIFO(): &amp;gt;&amp;gt; NEXT CHECK FOR INTERRUPT FLAG


D (42260) checkForMovementAndReadFIFO: [MEMS_Support.cpp:283] checkForMovementAndReadFIFO(): Interrupt! &amp;gt;&amp;gt;****AND THE PATTERN REPEATS....****
D (42271) checkForMovementAndReadFIFO: [MEMS_Support.cpp:287] checkForMovementAndReadFIFO(): ***Int_SourceSystem: 0x00
D (42281) checkForMovementAndReadFIFO: [MEMS_Support.cpp:291] checkForMovementAndReadFIFO(): FIFO Status: 0x09
D (42291) checkForMovementAndReadFIFO: [MEMS_Support.cpp:292] checkForMovementAndReadFIFO():   Overflow: 0
D (42302) checkForMovementAndReadFIFO: [MEMS_Support.cpp:293] checkForMovementAndReadFIFO():   Watermark: 0
D (42312) checkForMovementAndReadFIFO: [MEMS_Support.cpp:294] checkForMovementAndReadFIFO():   Sample Count: 9
D (42322) checkForMovementAndReadFIFO: [MEMS_Support.cpp:350] checkForMovementAndReadFIFO(): Invalid interrupt: 0

D (42333) checkForMovementAndReadFIFO: [MEMS_Support.cpp:351] checkForMovementAndReadFIFO(): Unexpected FIFO status: 0x09

D (42343) checkForMovementAndReadFIFO: [MEMS_Support.cpp:353] checkForMovementAndReadFIFO(): checkForMovementAndReadFIFO elapsed time: 83ms
D (42355) checkForMovementAndReadFIFO: [MEMS_Support.cpp:357] checkForMovementAndReadFIFO(): checkForMovementAndReadFIFO elapsed time: 0ms
D (42367) checkForMovementAndReadFIFO: [MEMS_Support.cpp:357] checkForMovementAndReadFIFO(): checkForMovementAndReadFIFO elapsed time: 0ms
D (42379) checkForMovementAndReadFIFO: [MEMS_Support.cpp:357] checkForMovementAndReadFIFO(): checkForMovementAndReadFIFO elapsed time: 0ms&lt;/LI-CODE&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;So you can see a pattern of one correct FIFO FULL interrupt followed by an "extra" and "false" interrupt in which the FIFO is not actually full. And this repeats over and over.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;It seems I need to be able to check the interrupt and fifo status but somehow not let the interrupt be reasserted before I read the FIFO data.&amp;nbsp; Other than turning off the MMA8451Q interrupt and then restarting it after the read, is there another way to accomplish this checking and reading of the *full* FIFO without having the interrupt re-asserted?&amp;nbsp; Is there a "normal" way to do this that I am just not getting?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Many thanks!&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Tue, 03 Feb 2026 20:59:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8451Q-FIFO-Interrupt-getting-extra-interrupts-without-FIFO/m-p/2136636#M8906</guid>
      <dc:creator>peteDDD</dc:creator>
      <dc:date>2026-02-03T20:59:51Z</dc:date>
    </item>
    <item>
      <title>Re: MMA8451Q FIFO Interrupt... getting extra interrupts without FIFO flag</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8451Q-FIFO-Interrupt-getting-extra-interrupts-without-FIFO/m-p/2137100#M8908</link>
      <description>&lt;P&gt;Dear Pete,&lt;/P&gt;
&lt;P&gt;you're encountering a common issue with the&amp;nbsp;MMA8451Q FIFO interrupt behavior, where an&amp;nbsp;extra interrupt&amp;nbsp;is triggered even though the FIFO watermark condition is no longer valid.&lt;/P&gt;
&lt;P&gt;Here are a few strategies to try:&lt;/P&gt;
&lt;P&gt;1. Make sure you&amp;nbsp;read the FIFO buffer immediately&amp;nbsp;after confirming the interrupt source and before any other I2C operations. This ensures the FIFO interrupt flag is cleared as early as possible.&lt;/P&gt;
&lt;P&gt;&lt;!--ScriptorStartFragment--&gt;&lt;/P&gt;
&lt;DIV class="scriptor-paragraph"&gt;uint8_t intSource = mma.getIntSourceReg();&lt;/DIV&gt;
&lt;DIV class="scriptor-paragraph"&gt;if (intSource &amp;amp; 0x40) {&lt;/DIV&gt;
&lt;DIV class="scriptor-paragraph"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint8_t fifoStatus = mma.getFIFOStatus();&lt;/DIV&gt;
&lt;DIV class="scriptor-paragraph"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (fifoStatus &amp;amp; 0x40) {&lt;/DIV&gt;
&lt;DIV class="scriptor-paragraph"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Immediately read FIFO here&lt;/DIV&gt;
&lt;DIV class="scriptor-paragraph"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/DIV&gt;
&lt;DIV class="scriptor-paragraph"&gt;}&lt;/DIV&gt;
&lt;P&gt;&lt;LI-WRAPPER&gt;&lt;!--ScriptorEndFragment--&gt;&lt;/LI-WRAPPER&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2.&amp;nbsp;Mask Interrupt During Processing&lt;/P&gt;
&lt;P&gt;Temporarily&amp;nbsp;disable the FIFO interrupt&amp;nbsp;in&amp;nbsp;&lt;CODE&gt;CTRL_REG4&lt;/CODE&gt;&amp;nbsp;or&amp;nbsp;mask it&amp;nbsp;in&amp;nbsp;&lt;CODE&gt;CTRL_REG5&lt;/CODE&gt;&amp;nbsp;during processing, then re-enable it after reading the FIFO:&lt;/P&gt;
&lt;P&gt;&lt;!--ScriptorStartFragment--&gt;&lt;/P&gt;
&lt;DIV class="scriptor-paragraph"&gt;// Disable FIFO interrupt&lt;/DIV&gt;
&lt;DIV class="scriptor-paragraph"&gt;writeRegister8(MMA8451_REG_CTRL_REG4, 0x00);&lt;/DIV&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV class="scriptor-paragraph"&gt;// Read FIFO...&lt;/DIV&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV class="scriptor-paragraph"&gt;// Re-enable FIFO interrupt&lt;/DIV&gt;
&lt;DIV class="scriptor-paragraph"&gt;writeRegister8(MMA8451_REG_CTRL_REG4, MMA8451_INT_EN_FIFO);&lt;/DIV&gt;
&lt;P&gt;&lt;LI-WRAPPER&gt;&lt;!--ScriptorEndFragment--&gt;&lt;/LI-WRAPPER&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;3.&amp;nbsp;Use FIFO in Circular Mode Instead of Fill Mode&lt;/P&gt;
&lt;P&gt;In&amp;nbsp;Circular Mode, the FIFO continues to collect data and overwrite old samples. This can help avoid the "stuck" interrupt condition that sometimes occurs in Fill Mode.&lt;/P&gt;
&lt;P&gt;&lt;!--ScriptorStartFragment--&gt;&lt;/P&gt;
&lt;DIV class="scriptor-paragraph"&gt;writeRegister8(MMA8451_F_SETUP, 0xC0 | watermark); // FMODE = 10 (circular)&lt;/DIV&gt;
&lt;P&gt;&lt;LI-WRAPPER&gt;&lt;!--ScriptorEndFragment--&gt;&lt;/LI-WRAPPER&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;4.&amp;nbsp;Debounce or Delay Interrupt Handling&lt;/P&gt;
&lt;P&gt;Add a&amp;nbsp;short delay&amp;nbsp;(e.g., 5–10 ms) before re-enabling the interrupt or checking the FIFO again. This gives the sensor time to stabilize and avoids catching a transient state.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jul 2025 06:52:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8451Q-FIFO-Interrupt-getting-extra-interrupts-without-FIFO/m-p/2137100#M8908</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2025-07-21T06:52:06Z</dc:date>
    </item>
    <item>
      <title>Re: MMA8451Q FIFO Interrupt... getting extra interrupts without FIFO flag</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8451Q-FIFO-Interrupt-getting-extra-interrupts-without-FIFO/m-p/2137451#M8909</link>
      <description>&lt;P&gt;Thanks&amp;nbsp;@ JosefKozen.&lt;/P&gt;&lt;P&gt;I have in fact tried all of those things.&lt;/P&gt;&lt;P&gt;Accomplishing #1 while still gaining (and printing) some diagnostics is a like a quantum physics problem... you disturb the system by observing it.&amp;nbsp; If you don't "observe" it with the diagnostics, it might be working correctly but with&amp;nbsp; "observing" it, you don't know.&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;Schrödinger&lt;/SPAN&gt; lives...&lt;/P&gt;&lt;P&gt;I am really trying not to leave any time slices unsampled.&amp;nbsp; I am playing with how I allocate the tasks between cores and the time slice priorities in FreeRTOS to see if I can "get around" to checking the interrupt more promptly.&amp;nbsp; That might be my biggest problem.&lt;/P&gt;&lt;P&gt;I know see that the MMA 8451Q is going out of production so will need to change chips for production.&amp;nbsp; &amp;nbsp;I need to maintain 14-bit resolution for my application.&amp;nbsp; I found some non-NXP accelerometer chips with 14-bit resolution at 2g AND 512 sample FIFOs.&amp;nbsp; &amp;nbsp;A larger FIFO would allow me to grab my 500ms worth of samples in a single (long) I2C fetch.&amp;nbsp; That would dramatically improve my timing issues.&amp;nbsp; Does NXP offer such a chip?&amp;nbsp; (even a 256 sample FIFO, or possibly a 128 sample FIFO, would do the trick)&lt;/P&gt;&lt;P&gt;Thanks again!&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jul 2025 12:45:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8451Q-FIFO-Interrupt-getting-extra-interrupts-without-FIFO/m-p/2137451#M8909</guid>
      <dc:creator>peteDDD</dc:creator>
      <dc:date>2025-07-21T12:45:00Z</dc:date>
    </item>
    <item>
      <title>Re: MMA8451Q FIFO Interrupt... getting extra interrupts without FIFO flag</title>
      <link>https://community.nxp.com/t5/Sensors/MMA8451Q-FIFO-Interrupt-getting-extra-interrupts-without-FIFO/m-p/2137922#M8910</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Dear Pete,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;As of the latest available information,&amp;nbsp;NXP does not currently offer a direct replacement for the MMA8451Q&amp;nbsp;with both:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;14-bit resolution at ±2g, and&lt;/LI&gt;
&lt;LI&gt;a FIFO buffer of 128 samples or more.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;However, here are a few NXP accelerometers that come close and might be worth evaluating:&lt;/P&gt;
&lt;H3&gt;&lt;A href="https://www.nxp.com/products/FXLS8974CF#documentation" target="_self"&gt;&amp;nbsp;FXLS8974CF&lt;/A&gt;&lt;/H3&gt;
&lt;UL&gt;
&lt;LI&gt;Resolution: 14-bit&lt;/LI&gt;
&lt;LI&gt;Range: ±2g to ±16g&lt;/LI&gt;
&lt;LI&gt;FIFO: 32 samples&lt;/LI&gt;
&lt;LI&gt;Interface: I²C/SPI&lt;/LI&gt;
&lt;LI&gt;Power: Ultra-low power&lt;/LI&gt;
&lt;LI&gt;Notes: Designed for industrial and consumer applications. FIFO is smaller than your target, but otherwise a solid performer.&lt;/LI&gt;
&lt;/UL&gt;
&lt;H3&gt;&lt;A href="https://www.nxp.com/products/sensors/accelerometers/2g-4g-8g-16g-low-power-12-bit-digital-accelerometer:FXLS8964AF#documentation" target="_self"&gt;FXLS8964AF&lt;/A&gt;&lt;/H3&gt;
&lt;UL&gt;
&lt;LI&gt;Resolution: 14-bit&lt;/LI&gt;
&lt;LI&gt;Range: ±2g to ±16g&lt;/LI&gt;
&lt;LI&gt;FIFO: 32 samples&lt;/LI&gt;
&lt;LI&gt;Interface: I²C/SPI&lt;/LI&gt;
&lt;LI&gt;Notes: Similar to FXLS8974CF, with slightly different packaging and power profiles.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Tue, 22 Jul 2025 04:02:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MMA8451Q-FIFO-Interrupt-getting-extra-interrupts-without-FIFO/m-p/2137922#M8910</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2025-07-22T04:02:55Z</dc:date>
    </item>
  </channel>
</rss>