<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: TPMS (Tire Pressure Monitoring System)</title>
    <link>https://community.nxp.com/t5/Sensors/TPMS-Tire-Pressure-Monitoring-System/m-p/2131647#M8894</link>
    <description>I get it. Thank you.&lt;BR /&gt;I had one more question but you didn't see that probably. No problem.&lt;BR /&gt;"Do you have evaluation board for NTM88 series?" Because at the beginning I chose FXTH87 but these sensors are not manufactured anymore. FXTH87 just has a evaluation board but no manufactured chips I think. It means it is not sustainable. So, If I draw a schematic what is your suggest to me?&lt;BR /&gt;Do I draw a schematic from FXTH87 or NTM88?&lt;BR /&gt;&lt;BR /&gt;</description>
    <pubDate>Thu, 10 Jul 2025 10:50:46 GMT</pubDate>
    <dc:creator>sadur</dc:creator>
    <dc:date>2025-07-10T10:50:46Z</dc:date>
    <item>
      <title>TPMS (Tire Pressure Monitoring System)</title>
      <link>https://community.nxp.com/t5/Sensors/TPMS-Tire-Pressure-Monitoring-System/m-p/2131446#M8892</link>
      <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I'm currently working on "Tire Pressure Monitoring System". I did some search and found NTM88 series which is&amp;nbsp; perfect. This sensor has range of 90kPa-1518kPa. That mean is also 13psi-220psi. But I need to measure high pressure. Is there any chance that you have high range TPMS over 1600kPa. At least 300-350psi maybe.&lt;/P&gt;&lt;P&gt;And also I need to evaluation board &lt;LI-EMOJI id="lia_grinning-face-with-smiling-eyes" title=":grinning_face_with_smiling_eyes:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;I have one more question:&lt;/P&gt;&lt;P&gt;Do you have evaluation board for NTM88 series.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 23:40:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/TPMS-Tire-Pressure-Monitoring-System/m-p/2131446#M8892</guid>
      <dc:creator>sadur</dc:creator>
      <dc:date>2026-02-03T23:40:34Z</dc:date>
    </item>
    <item>
      <title>Re: TPMS (Tire Pressure Monitoring System)</title>
      <link>https://community.nxp.com/t5/Sensors/TPMS-Tire-Pressure-Monitoring-System/m-p/2131569#M8893</link>
      <description>&lt;P&gt;Hello Salih,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP’s TPMS solutions.&lt;/P&gt;
&lt;P&gt;At this time, we do not offer TPMS sensors that support pressure ranges beyond 1518 kPa (220 psi). The NTM88K series is our highest-range TPMS solution, with an operating pressure range up to 1518 kPa.&lt;/P&gt;
&lt;P&gt;For applications requiring higher pressure monitoring (such as 300 to 350 psi), you may need to explore specialized or industrial-grade TPMS solutions from other vendors.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jul 2025 08:41:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/TPMS-Tire-Pressure-Monitoring-System/m-p/2131569#M8893</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2025-07-10T08:41:42Z</dc:date>
    </item>
    <item>
      <title>Re: TPMS (Tire Pressure Monitoring System)</title>
      <link>https://community.nxp.com/t5/Sensors/TPMS-Tire-Pressure-Monitoring-System/m-p/2131647#M8894</link>
      <description>I get it. Thank you.&lt;BR /&gt;I had one more question but you didn't see that probably. No problem.&lt;BR /&gt;"Do you have evaluation board for NTM88 series?" Because at the beginning I chose FXTH87 but these sensors are not manufactured anymore. FXTH87 just has a evaluation board but no manufactured chips I think. It means it is not sustainable. So, If I draw a schematic what is your suggest to me?&lt;BR /&gt;Do I draw a schematic from FXTH87 or NTM88?&lt;BR /&gt;&lt;BR /&gt;</description>
      <pubDate>Thu, 10 Jul 2025 10:50:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/TPMS-Tire-Pressure-Monitoring-System/m-p/2131647#M8894</guid>
      <dc:creator>sadur</dc:creator>
      <dc:date>2025-07-10T10:50:46Z</dc:date>
    </item>
    <item>
      <title>Re: TPMS (Tire Pressure Monitoring System)</title>
      <link>https://community.nxp.com/t5/Sensors/TPMS-Tire-Pressure-Monitoring-System/m-p/2132252#M8895</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello Salih,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;NTM88 series TPMS evaluation boards are not sold via NXP website or distributors. They are provided free of charge by NXP TPMS Application team.&amp;nbsp;In order to ask for the EVB, please create a standard support ticket with the following information included:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;- Brief description of your application, estimated volume and start of production.&lt;BR /&gt;- Desired pressure (930kPa, 1100kPa or 1518kPa) and desired frequency.&lt;BR /&gt;- Name, address and phone number of the person who will receive the evaluation board + VAT number of the company.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BRs, Tomas&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jul 2025 06:41:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/TPMS-Tire-Pressure-Monitoring-System/m-p/2132252#M8895</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2025-07-11T06:41:21Z</dc:date>
    </item>
  </channel>
</rss>