<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 Re: MPL3115A2 Temperature Compensated</title>
    <link>https://community.nxp.com/t5/Sensors/MPL3115A2-Temperature-Compensated/m-p/2112670#M8848</link>
    <description>&lt;P&gt;Hello Adrian,&lt;/P&gt;
&lt;P&gt;Yes, the MPL3115A2 handles temperature effects on altitude internally through built-in compensation mechanisms. It includes an on-chip temperature sensor that is used internally to compensate pressure readings. This compensation ensures that the pressure values used for altitude calculations are temperature-corrected.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
    <pubDate>Mon, 09 Jun 2025 08:01:38 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2025-06-09T08:01:38Z</dc:date>
    <item>
      <title>MPL3115A2 Temperature Compensated</title>
      <link>https://community.nxp.com/t5/Sensors/MPL3115A2-Temperature-Compensated/m-p/2112292#M8845</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the MPL3115A2 - I2C Barometric Pressure/Altitude/Temperature Sensor &lt;/SPAN&gt;&lt;SPAN&gt;and was wondering if anyone knows, specifically, how temperature affects the altitude calculation. Under section 5.2.4 - Span, the documentation says, "The MPL3115A2 uses internal temperature compensation to remove drift."&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If anyone knows, I would greatly appreciate an answer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Adrin&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:10:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL3115A2-Temperature-Compensated/m-p/2112292#M8845</guid>
      <dc:creator>LabOrders</dc:creator>
      <dc:date>2026-02-03T21:10:54Z</dc:date>
    </item>
    <item>
      <title>Re: MPL3115A2 Temperature Compensated</title>
      <link>https://community.nxp.com/t5/Sensors/MPL3115A2-Temperature-Compensated/m-p/2112670#M8848</link>
      <description>&lt;P&gt;Hello Adrian,&lt;/P&gt;
&lt;P&gt;Yes, the MPL3115A2 handles temperature effects on altitude internally through built-in compensation mechanisms. It includes an on-chip temperature sensor that is used internally to compensate pressure readings. This compensation ensures that the pressure values used for altitude calculations are temperature-corrected.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Mon, 09 Jun 2025 08:01:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL3115A2-Temperature-Compensated/m-p/2112670#M8848</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2025-06-09T08:01:38Z</dc:date>
    </item>
    <item>
      <title>Re: MPL3115A2 Temperature Compensated</title>
      <link>https://community.nxp.com/t5/Sensors/MPL3115A2-Temperature-Compensated/m-p/2128204#M8885</link>
      <description>&lt;P&gt;Hello, is it possible to get the exact formula used for compensating pressure with temperature?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Adrin&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jul 2025 16:12:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPL3115A2-Temperature-Compensated/m-p/2128204#M8885</guid>
      <dc:creator>LabOrders</dc:creator>
      <dc:date>2025-07-03T16:12:03Z</dc:date>
    </item>
  </channel>
</rss>