<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>SensorsのトピックRe: FXPS7115DS4T1</title>
    <link>https://community.nxp.com/t5/Sensors/FXPS7115DS4T1/m-p/2067713#M8761</link>
    <description>&lt;P&gt;Dear Richard,&lt;/P&gt;
&lt;P&gt;unfortunately I didn't find the&amp;nbsp;FXPS7115D SPI messages (perhaps somebody else will share them) in older cases, but I have found a description for CRC calculation from an application engineer. Please see below.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;In order to build CRC checksum on the SPI command, you can take ”8-bit crc” fields as either ‘0000 0000’ or ‘1111 1111’ to complete the total 32-bit command. Calculate 8-bit CRC using the default polynomial on the 32-bit command and then replace calculated 8-bit CRC value in the ”8-bit crc” fields before sending the command. If the calculated CRC does not match the transmitted CRC, the command is ignored and the device responds with the SPI error response.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;I have also found FXPS7xxx SW examples. Please find it attached.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
    <pubDate>Tue, 25 Mar 2025 12:44:02 GMT</pubDate>
    <dc:creator>JozefKozon</dc:creator>
    <dc:date>2025-03-25T12:44:02Z</dc:date>
    <item>
      <title>FXPS7115DS4T1</title>
      <link>https://community.nxp.com/t5/Sensors/FXPS7115DS4T1/m-p/2067681#M8760</link>
      <description>&lt;P&gt;Can anyone share SPI messages with calculated CRC. To start and read pressure and temperature?&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:11:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXPS7115DS4T1/m-p/2067681#M8760</guid>
      <dc:creator>Fast</dc:creator>
      <dc:date>2026-02-03T21:11:46Z</dc:date>
    </item>
    <item>
      <title>Re: FXPS7115DS4T1</title>
      <link>https://community.nxp.com/t5/Sensors/FXPS7115DS4T1/m-p/2067713#M8761</link>
      <description>&lt;P&gt;Dear Richard,&lt;/P&gt;
&lt;P&gt;unfortunately I didn't find the&amp;nbsp;FXPS7115D SPI messages (perhaps somebody else will share them) in older cases, but I have found a description for CRC calculation from an application engineer. Please see below.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;In order to build CRC checksum on the SPI command, you can take ”8-bit crc” fields as either ‘0000 0000’ or ‘1111 1111’ to complete the total 32-bit command. Calculate 8-bit CRC using the default polynomial on the 32-bit command and then replace calculated 8-bit CRC value in the ”8-bit crc” fields before sending the command. If the calculated CRC does not match the transmitted CRC, the command is ignored and the device responds with the SPI error response.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;I have also found FXPS7xxx SW examples. Please find it attached.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Tue, 25 Mar 2025 12:44:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXPS7115DS4T1/m-p/2067713#M8761</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2025-03-25T12:44:02Z</dc:date>
    </item>
    <item>
      <title>Re: FXPS7115DS4T1</title>
      <link>https://community.nxp.com/t5/Sensors/FXPS7115DS4T1/m-p/2067733#M8762</link>
      <description>&lt;P&gt;Thank you Jozef, I have looked at that but I do not need CRC and it is desperately slow to live calculate. I will attempt to use online tool to calculate CRC. Surely someone has a real example, not a code example? Perhaps it will get supported with&amp;nbsp;SPIGen.exe, which is very useful tool.&lt;/P&gt;</description>
      <pubDate>Tue, 25 Mar 2025 12:56:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXPS7115DS4T1/m-p/2067733#M8762</guid>
      <dc:creator>Fast</dc:creator>
      <dc:date>2025-03-25T12:56:10Z</dc:date>
    </item>
    <item>
      <title>Re: FXPS7115DS4T1</title>
      <link>https://community.nxp.com/t5/Sensors/FXPS7115DS4T1/m-p/2072803#M8766</link>
      <description>&lt;P&gt;No examples only code. I'll look at the Infineon and ST offerings&lt;/P&gt;</description>
      <pubDate>Wed, 02 Apr 2025 10:49:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/FXPS7115DS4T1/m-p/2072803#M8766</guid>
      <dc:creator>Fast</dc:creator>
      <dc:date>2025-04-02T10:49:13Z</dc:date>
    </item>
  </channel>
</rss>