<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPX5010 vs MPX2010 in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/MPX5010-vs-MPX2010/m-p/327510#M863</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jason Haedt,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Answering to your questions:&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;It is a very similar sensor with the difference (that you already noticed) that the MPX5010 is on-chip amplified, but both have the same pressure range and general functionality.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;It is actually very simple to interface the MPX5010 since it’s already amplified, temperature compensated and calibrated, so the only think you need to add are just a few capacitors (as seen on Figure 3 of the datasheet) and the signal goes directly to your mcu’s ADC.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Click &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MPXx5010&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab"&gt;here&lt;/A&gt; to find all the documentation available for the MPX5010.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose Reyes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Feb 2015 14:34:28 GMT</pubDate>
    <dc:creator>reyes</dc:creator>
    <dc:date>2015-02-26T14:34:28Z</dc:date>
    <item>
      <title>MPX5010 vs MPX2010</title>
      <link>https://community.nxp.com/t5/Sensors/MPX5010-vs-MPX2010/m-p/327509#M862</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Freescale,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I currently use MPX2010 in a dual port configuration.&amp;nbsp; I am looking to move to the MPX5010 with the integrated amplifier but had a few questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.) Is the sensor the same in the MPX2010 and the MPX5010?&lt;/P&gt;&lt;P&gt;2.) Are there any application recommendations for interfacing to the MPX5010?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sincerely,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jason&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2026 22:22:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPX5010-vs-MPX2010/m-p/327509#M862</guid>
      <dc:creator>jasonhaedt</dc:creator>
      <dc:date>2026-02-03T22:22:30Z</dc:date>
    </item>
    <item>
      <title>Re: MPX5010 vs MPX2010</title>
      <link>https://community.nxp.com/t5/Sensors/MPX5010-vs-MPX2010/m-p/327510#M863</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jason Haedt,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Answering to your questions:&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;It is a very similar sensor with the difference (that you already noticed) that the MPX5010 is on-chip amplified, but both have the same pressure range and general functionality.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;It is actually very simple to interface the MPX5010 since it’s already amplified, temperature compensated and calibrated, so the only think you need to add are just a few capacitors (as seen on Figure 3 of the datasheet) and the signal goes directly to your mcu’s ADC.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Click &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MPXx5010&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab"&gt;here&lt;/A&gt; to find all the documentation available for the MPX5010.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose Reyes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Feb 2015 14:34:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPX5010-vs-MPX2010/m-p/327510#M863</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2015-02-26T14:34:28Z</dc:date>
    </item>
  </channel>
</rss>