<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPXV5010DP under electric field problem in Sensors</title>
    <link>https://community.nxp.com/t5/Sensors/MPXV5010DP-under-electric-field-problem/m-p/1978947#M8531</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have&amp;nbsp;MPXV5010DP assembled on board.&lt;/P&gt;&lt;P&gt;During electric field 50V/m, at several frequencies, projected on it ( from distance of 1 meter), the sensor started to output failed analog signals ( it should be 0).&lt;/P&gt;&lt;P&gt;Do you know about this type of phenomena? any suggestion how to eliminate it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;AE&lt;/P&gt;</description>
    <pubDate>Tue, 03 Feb 2026 21:30:08 GMT</pubDate>
    <dc:creator>AEb2</dc:creator>
    <dc:date>2026-02-03T21:30:08Z</dc:date>
    <item>
      <title>MPXV5010DP under electric field problem</title>
      <link>https://community.nxp.com/t5/Sensors/MPXV5010DP-under-electric-field-problem/m-p/1978947#M8531</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have&amp;nbsp;MPXV5010DP assembled on board.&lt;/P&gt;&lt;P&gt;During electric field 50V/m, at several frequencies, projected on it ( from distance of 1 meter), the sensor started to output failed analog signals ( it should be 0).&lt;/P&gt;&lt;P&gt;Do you know about this type of phenomena? any suggestion how to eliminate it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;AE&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:30:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPXV5010DP-under-electric-field-problem/m-p/1978947#M8531</guid>
      <dc:creator>AEb2</dc:creator>
      <dc:date>2026-02-03T21:30:08Z</dc:date>
    </item>
    <item>
      <title>Re: MPXV5010DP under electric field problem</title>
      <link>https://community.nxp.com/t5/Sensors/MPXV5010DP-under-electric-field-problem/m-p/1979172#M8532</link>
      <description>&lt;P&gt;Hello Aharon,&lt;/P&gt;
&lt;P&gt;Strong electric fields can induce unwanted noise or disturbances in sensitive analog circuits, resulting in erroneous sensor outputs.&lt;/P&gt;
&lt;P&gt;Here are some suggestions to mitigate this effect:&lt;/P&gt;
&lt;P&gt;Surround the sensor and associated circuitry with a conductive enclosure or shield. Make sure the shield is properly grounded to prevent electric fields from penetrating and affecting the sensor.&lt;/P&gt;
&lt;P&gt;Ensure that the sensor and the surrounding electronics have a good ground connection.&amp;nbsp;Keep the signal traces as short as possible. Use ground planes to provide shielding and better grounding.&lt;/P&gt;
&lt;P&gt;Place decoupling capacitors near the power supply pins of the sensor to stabilize the power and reduce noise sensitivity.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Unfortunately it is difficult to diagnose without more data, but I believe that implementing some of these suggestions can help mitigate the effects of EMI and stabilize the sensor output under electric field exposure.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BRs, Tomas&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Oct 2024 10:50:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPXV5010DP-under-electric-field-problem/m-p/1979172#M8532</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-10-22T10:50:10Z</dc:date>
    </item>
  </channel>
</rss>