<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Sensors中的主题 MPXV2010DP Designreview</title>
    <link>https://community.nxp.com/t5/Sensors/MPXV2010DP-Designreview/m-p/1951682#M8470</link>
    <description>&lt;P&gt;Hello Folks,&lt;/P&gt;&lt;P&gt;i would like to use 3 MPXV2010DP differential pressure sensors&lt;/P&gt;&lt;P&gt;I wanna use them to messure pressures up to 10kPa, which seems fine like the datasheet.&lt;/P&gt;&lt;P&gt;Now it is that the MPXV2010DP is giving out 0-25mV. To use this i want to amplify the Outputvoltage x 200, so i have a range from 0-5V, so i can read it out from an ADC.&lt;/P&gt;&lt;P&gt;For this i am using an operational amplifier as non-inverting amplifier.&lt;/P&gt;&lt;P&gt;Now it would be nice if you can check my schematic to see, if i am right or not.. &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt; Its my first time working with them and before i order my PCB i can change things before..&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="Screenshot 2024-09-11 071319.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/298443iE8E1397C99FFFA77/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot 2024-09-11 071319.png" alt="Screenshot 2024-09-11 071319.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
    <pubDate>Tue, 03 Feb 2026 21:24:23 GMT</pubDate>
    <dc:creator>BTLede</dc:creator>
    <dc:date>2026-02-03T21:24:23Z</dc:date>
    <item>
      <title>MPXV2010DP Designreview</title>
      <link>https://community.nxp.com/t5/Sensors/MPXV2010DP-Designreview/m-p/1951682#M8470</link>
      <description>&lt;P&gt;Hello Folks,&lt;/P&gt;&lt;P&gt;i would like to use 3 MPXV2010DP differential pressure sensors&lt;/P&gt;&lt;P&gt;I wanna use them to messure pressures up to 10kPa, which seems fine like the datasheet.&lt;/P&gt;&lt;P&gt;Now it is that the MPXV2010DP is giving out 0-25mV. To use this i want to amplify the Outputvoltage x 200, so i have a range from 0-5V, so i can read it out from an ADC.&lt;/P&gt;&lt;P&gt;For this i am using an operational amplifier as non-inverting amplifier.&lt;/P&gt;&lt;P&gt;Now it would be nice if you can check my schematic to see, if i am right or not.. &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt; Its my first time working with them and before i order my PCB i can change things before..&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="Screenshot 2024-09-11 071319.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/298443iE8E1397C99FFFA77/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot 2024-09-11 071319.png" alt="Screenshot 2024-09-11 071319.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 21:24:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPXV2010DP-Designreview/m-p/1951682#M8470</guid>
      <dc:creator>BTLede</dc:creator>
      <dc:date>2026-02-03T21:24:23Z</dc:date>
    </item>
    <item>
      <title>Re: MPXV2010DP Designreview</title>
      <link>https://community.nxp.com/t5/Sensors/MPXV2010DP-Designreview/m-p/1951849#M8473</link>
      <description>&lt;P&gt;Hello Thomas,&lt;/P&gt;
&lt;P&gt;First of all, all 4 pins of the MPX2010DP needs to be connected as below:&lt;/P&gt;
&lt;P&gt;Pin 1: GND&lt;BR /&gt;Pin 2: Positive Output Voltage&lt;BR /&gt;Pin 3: Voltage Supply (10V recommended)&lt;BR /&gt;Pin 4: Negative Output Voltage&lt;/P&gt;
&lt;P data-unlink="true"&gt;The output of this sensor is differential and temperature compensated, which means that the sensor gives you a differential output in the range of millivolts (0-25mV). This differential output needs to be converted to a single ended output using an instrumentation amplifier (differential input amplifier).&amp;nbsp;&lt;SPAN&gt;You can find some information about that e.g. in our old&amp;nbsp;&lt;/SPAN&gt;AN1318 (attached)&lt;SPAN&gt;, but my recommendation would be using a single chip solution such as the INA122 instrumentation amplifier.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P data-unlink="true"&gt;&lt;SPAN&gt;Alternatively, you can&amp;nbsp;&lt;/SPAN&gt;use an integrated pressure sensor &lt;A href="https://www.nxp.com/part/MPX5010DP" target="_self"&gt;MPX5010DP&lt;/A&gt; instead, it is already internally compensated, calibrated and amplified, so you do not need many external components other than few capacitors (as can be seen in Figure 11 of the &lt;A href="https://www.nxp.com/docs/en/data-sheet/MPX5010.pdf" target="_self"&gt;MPX5010 datasheet&lt;/A&gt;) and the output is already given in the range of 0 to 5V, so it is much more easier to use than the MPX2010DP pressure sensor.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;
&lt;P data-unlink="true"&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 07:55:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPXV2010DP-Designreview/m-p/1951849#M8473</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-09-11T07:55:28Z</dc:date>
    </item>
    <item>
      <title>Re: MPXV2010DP Designreview</title>
      <link>https://community.nxp.com/t5/Sensors/MPXV2010DP-Designreview/m-p/1951873#M8474</link>
      <description>&lt;P&gt;Hello Tomas!&lt;/P&gt;&lt;P&gt;thank you so much..&lt;/P&gt;&lt;P&gt;Yes, it seems like the MPX2010DP has an + and - output.. i started the design with an MPX5010DP and also created the footprint for it, and then i thought i could use the MPX2010DP since it has better tolerances.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But as you asume, it would be better to just use the MPX5010DP. But here i would need your help again:&lt;BR /&gt;When i use the MPX5010DP, i can delete the operational amplifier and give the signals directly into the ADC? That would be really really easy.. since i only need those 3 sensors.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 08:21:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPXV2010DP-Designreview/m-p/1951873#M8474</guid>
      <dc:creator>BTLede</dc:creator>
      <dc:date>2024-09-11T08:21:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPXV2010DP Designreview</title>
      <link>https://community.nxp.com/t5/Sensors/MPXV2010DP-Designreview/m-p/1951985#M8476</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello Thomas,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Yes, when using the MPX5010DP with a single ended and internally amplified output, there is no need for the external&amp;nbsp;operational amplifier. The output voltage is typically in the range of 0.2V to 4.7V and can usually be directly connected to the ADC input.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BRs, Tomas&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 10:03:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Sensors/MPXV2010DP-Designreview/m-p/1951985#M8476</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-09-11T10:03:09Z</dc:date>
    </item>
  </channel>
</rss>